ST7 Programming Error
Company  
ST Home | Microcontrollers

Index  »  ST7  »  ST7 Programming Error
     
   ST7 Programming Error
 Moderated by :   »  Jatin  -  laubey  -  Setler

Author
beginning argument    ( Replies received: 4 )
oc.james.fowkes   Posted 23-05-2008 at 12:41   



Registered on :
05-06-2008

Messages : 3

 OFF-Line

Hello,

I am using an ST72F60E1 device, trying to program through an RLINK USB programmer.


I've actually had this working before, but coming back to it after a few months and now I'm getting this error:

"Error : Cannot communicate with the device ! Option Bytes are Enabled on the device.
Check the ICC cable connection and check all the needed pin connections on the ICP connector."

I've double- and triple-checked the ICC connections, and I'm sure they're correct. I'm using a 12MHz crystal on the board, which is producing a steady clock. The application power supply is 5v from the USB bus.

What are the possible sources of this error? It must be something simple...



 Profile   Quote  
silicon.ray   Posted 26-05-2008 at 10:17   



Registered on :
05-06-2008

Messages : 5

 OFF-Line

Hi

You can try to change booten bits set to load from external (1,1,1).Then erase flash and set booten to load from flash (0,0,0).

r,A



 Profile   Quote  
oc.james.fowkes   Posted 27-05-2008 at 10:53   



Registered on :
05-06-2008

Messages : 3

 OFF-Line

OK, how do I do that? I am using ST7 Visual Programmer.



 Profile   Quote  
sjo   Posted 27-05-2008 at 15:38   



Registered on :
09-16-2002

From UK

Messages : 620

 OFF-Line

Afraid you don't, silicon.ray is confusing your device with the strxx family.

Normally just check your have the latest version of Visual Programmer

Could also try checking the reset line for to much capacitance.
Are the ICC line shared with your application?

Cheers
sjo



 Profile   www   Quote  
oc.james.fowkes   Posted 21-08-2008 at 18:27   



Registered on :
05-06-2008

Messages : 3

 OFF-Line

I am using the latest version of ST7VP/ST7VD, the reset line has no capacitance (that was a problem before), and the ICCDATA/ICCCLK are not shared by the application.

Having tried the RLINK with another board and MCU, that's not working either, so maybe I've somehow damaged the programmer...



 Profile   Quote  
On Top

Search in the forums
 
Jump To