PRESS RELEASE

STMicroelectronics Introduces the Market’s Smallest 3-Axis Analog Gyroscope

Innovative sensors from the market leader drive the adoption of advanced motion user interfaces in all kinds of consumer applications

L3G462A

Geveva, March 24, 2011 -

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications and the leading supplier of MEMS for consumer and portable applications 1 has extended its motion-sensor portfolio with the market’s smallest 3-axis analog-output gyroscope. Housed inside an ultra-small 4x4x1mm3 package, ST’s newest gyroscope combines superior performance and reliability with smart power management and design flexibility, advancing adoption of high-precision gesture control and intuitive user interfaces in mobile phones, tablets, game controllers and other consumer devices.

All of ST’s MEMS gyroscopes employ an industry-unique concept of a single sensing structure for motion measurement along all three orthogonal axes 2 . This innovative design approach eliminates all interference between the axes, significantly increasing accuracy and reliability in a wide range of consumer and industrial applications. The Company has introduced more than 40 gyroscopes over past two years and boosted its market share in gyroscopes for consumer and mobile applications from less than 1% in 2009 to 30% in 2010.

ST’s L3G462A gyroscope provides accurate angular-rate detection with a separate output for each of the three axes. The full scale of ±625dps accurately measures gestures and movements of different types and speeds, enabling applications from navigation to motion-activated user interface and gaming. The analog interface ensures very fast response with low latency and offers flexibility in external filtering capabilities and fine-tuning of key parameters to the individual application requirements.

The gyroscope’s extremely compact design eliminates the layout and placement issues common with existing bulkier solutions, without penalty in performance or reliability. The unparalleled stability over temperature (±0.04dps/°C) and sensitivity (±0.017%/°C) significantly improves measurement accuracy and the low noise level (0.017dps/√Hz) guarantees high precision in movement and gesture recognition.

ST’s newest 3-axis analog-output gyroscope can operate with any supply voltage in the range of 2.4 to 3.6V and the power-down and sleep-to-wake modes contribute to the reduction in power consumption of the entire system.

Volume production is scheduled for the end of Q3 2011 and the unit price is $3.5 in quantities of 1000 pieces.

For further information on ST’s complete MEMS portfolio go to www.st.com/mems 

Editors’ Notes
ST has shipped over 1.2 billion MEMS sensors to date and its dedicated 8-inch MEMS fabrication line, which was among the first in the world, currently produces more than 1.5 million devices a day.

The MEMS consumer market grew 27% in 2010 to US$1.6 billion and similar growth is expected in the next years, with revenues topping US$3.7 billion by 2014, according to iSuppli. The continued demands from consumer and mobile applications dominate the growth and these fields are expected to become the biggest MEMS segment by 2014.

About STMicroelectronics
STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2010, the Company’s net revenues were $10.35 billion. Further information on ST can be found at www.st.com.

Click here for the high-resolution photo

1  iSuppli: H2 2010 Consumer and Mobile MEMS Market Tracker, January 2011
2 There are three main types of angular motion: yaw is rotation around the vertical axis; roll is rotation around the front-to-back axis and pitch is the rotation around the side-to-side axis.