Highly integrated SoC takes multimedia in new directions – delivers extensive support for 2D/3D input formats and display resolutions, while reducing system bill-of-materials

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications and a world leader in developing and delivering System-on-Chip (SoC) ICs, today announced a new highly integrated SoC family with unique integration of comprehensive video and audio inputs, advanced video quality and expanded functionality. The new SoCs have been designed for multi-function premium monitors, public displays, All-in-One PCs and high-performance notebooks.
The first three members of the new multi-media monitor SoC family, STDP9320, STDP9210 and STDP7320, combine a DisplayPort 1.2 receiver and transmitter and a High-Definition Multimedia Interface (HDMI) 1.4 receiver. In addition, the STDP9320 and STDP9210 sustain 120Hz 3D Full High-Definition (FHD), very high-resolution WQXGA* and WQHD* display panels, while the STDP7320 supports 60Hz FHD WUXGA* display panels. The new products include first-of-their-kind features, such as multi-stream, multi-monitor daisy chain support, patented active video window detection, simple end-user accessible firmware updating, and ST’s industry-leading Faroudja® imaging technology.
The DisplayPort 1.2 receiver/transmitter enables wider bandwidth data – up to 21.6 Gbps – and multi-stream transmission through a single cable for ‘daisy chain’ and ‘tile’ display monitor applications. The HDMI 1.4 receiver supports all mandatory 3D input formats defined by the HDMI 1.4 specifications. Monitor firmware upgrading is made easy for consumers with the patented EZ-FUN (Easy Firmware Upgrade Network) feature, accessed via a simplified On-Screen Display (OSD) menu.
The SoC family provides additional digital-video and audio connectivity, such as dual Digital Visual Interface (DVI), analog component, TTL and SPDIF/I2S inputs. Panel interface options are Quad Low-Voltage Differential Signaling (LVDS) and Internal DisplayPort (iDP) or Embedded DisplayPort (eDP) formats.
The new SoCs integrate features for advanced image quality and usability not typically found in this category of product, including:
Availability
The STDP9320 and STDP9210 (WQXGA and WQHD/ 120Hz FHD) in 521-ball BGA packages are now sampling to early adapter customers. The STDP7320 (WUXGA / 60Hz FHD) will be available for sampling in a 345-ball BGA package in Q4 2011.
Click here for the high-resolution photo
About STMicroelectronics
STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2010, the Company’s net revenues were $10.35 billion. Further information on ST can be found at www.st.com.
• WQXGA (Wide Quad eXtended Graphics Array display resolution of 2560 x 1600 pixels)
• WQHD (Wide Quad High Definition display resolution of 2560 x 1440 pixels)
• WUXGA (Widescreen Ultra eXtended Graphic Array display resolution of 1920 x 1200 pixels)
Faroudja is a registered trademark of STMicroelectronics