ST Life.augmented

新闻稿

New Miniaturization Record by STMicroelectronics Makes More Room for Mobile Functionality

Mandatory over-voltage protection now available in smallest industry-standard surface-mount package
Geneva /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications and the world’s largest supplier of Transient Voltage Suppression (TVS) protection components, has introduced the world’s smallest TVS diode for protecting sensitive electronics in consumer products and handhelds.

 

As the first such device to be offered in the industry’s smallest standard surface-mount outline of 0.45 x 0.2mm, the ESDAVLC6-1BV2 is one size smaller than today’s 0.6 x 0.3mm devices.

The value of the space saving to designers can be seen by comparing with other chip sizes used in smartphones and tablets. “A complete motion-sensing IC for features such as indoor navigation and advanced user interface, such as ST’s LSM303D, measures just 3 x 3mm, while some power chips are as small as 2 x 2mm,” explains Eric Paris, Product Marketing Director, ASD & IPAD Division, STMicroelectronics. “Trimming 0.2mm or 0.1mm from each TVS can simplify placing components and routing connections, especially if the design contains several such devices.”

The ESDAVLC6-1BV2 TVS diode fully satisfies the protection requirements specified in the international standard IEC 61000-4-2. Although other types of electrostatic-discharge (ESD) protectors, such as varistors, are available in the same size, these generally do not protect as effectively. ST’s new ESDAVLC6-1BV2 has a clamping voltage half that of the nearest competing varistor in the same size package, offering greater safety for the internal components. Although useful in many applications, varistors also age, providing progressively less protection with each ESD event clamped.

 

Major features of ESDAVLC6-1BV2:
• Bidirectional operation; single part number fulfils multiple roles on pc-board
• Bandwidth: 1GHz
• Line capacitance: 7.5pF
• Breakdown voltage 6V
• Ultra-thin 0.2mm package height

The ESDAVLC6-1BV2 is in mass production now, and samples are also available. Prices start at $0.10 for orders of 1,000 pieces. If your company has higher volume requirements, please contact your local ST representative.

Click here for the high-resolution photo

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power and automotive products and embedded processing solutions. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.
In 2012, the Company’s net revenues were $8.49 billion. Further information on ST can be found at www.st.com.