ST Life.augmented

Press Release

STMicroelectronics Enables More Precise Motion Recognition by Combining Linear and Angular Motion Sensing in a Single Device

Geneva /

MEMS motion sensors add an intuitive man-machine interface to mobile phones, portable multimedia players, game controllers, personal navigation systems and remote input devices, creating interaction by linking the user’s wrist, arm, and hand movements to applications, navigation within and between menus, the movement of characters in a game and much more.

Robust and resistant to mechanical stress, the module leverages the same micromachining technology process that ST has already successfully applied to more than 600 million motion sensors sold in the market. The device boasts excellent stability over a wide operating temperature range (from -40°C to 85°C) and a negligible level of output noise.

ST’s low-power motion-sensing module combines a user-selectable full-scale acceleration range of ±2g/±4g/±8g with the industry’s widest angular-rate detection from 30 to 6000 dps along the pitch and yaw axes. The gyroscope element provides two separate outputs for each axis at the same time: an unamplified output value for high accuracy of slow motion and a 4x amplification to detect and measure very fast gestures and movements.

Addressing power constraints in battery-operated portable devices, ST’s new MEMS module includes power-down and sleep modes and it can operate with any supply voltage in the range of 2.7 to 3.6V. The device comes with built-in self-test capability that allows the customer to verify the functioning of both sensors after the assembly, without the need to move the board during testing.

“ST meets the market demand for cost-effective integration of multiple motion sensors in a single module,” said Sam Guilaume, CEO, Movea, the industry leader in motion-sensing controllers. “With ST’s new MEMS modules, and our complementary SmartMotion™ technology, we will provide unequalled motion-based solutions for user interfaces in remote controls, game pads, smartphones and other consumer devices.”

“The only company with high-volume production of gyroscopes and accelerometers for consumer applications, ST now makes another significant step in MEMS consumerization by introducing the market’s first multiple-axis sensing device in a single package,” said Benedetto Vigna, General Manager of STMicroelectronics’ MEMS, Sensors and High Performance Analog division. “Our customers will benefit from the industry-unique combination of superior performance, compelling price points, and large-scale production capacity at ST’s dedicated 8-inch MEMS fab.”

Samples of ST’s LSM320HAY30 multi-axis motion sensor module are available now, with mass production scheduled for Q1 2010. Unit pricing is $3.3 for quantities over 50,000 pieces.

For further information on ST’s complete MEMS portfolio, go to: www.st.com/mems.

About Movea
Movea is the global leader in developing and delivering technology, patents, and complete solutions for human motion sensing applications in consumer electronics, healthcare and sports markets.

Created in March 2007 by a team of industry leading researchers and executive managers, Movea SA was founded out of the French research institute CEA-Léti and is headquartered in Grenoble, France. Movea represents the commercialization of decades of intellectual property, research and development at CEA-Léti’s world renowned Minatec innovation campus, focused primarily on human motion sensing for healthcare and sports applications. In December 2007, Movea acquired Gyration, the pioneer since 1989 in consumer motion products, in order to further position itself as the global leader in motion-sensing solutions for consumer electronics. 

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2008, the Company's net revenues were $9.84 billion. Further information on ST can be found at www.st.com.
Information last updated Jun 2009