ST Life.augmented

Press Release

New Battery “Fuel Gauge” IC from STMicroelectronics Gives Reliable Runtimes for Mobile Users

Innovative state-of-charge calculator maintains accurate fuel gauging with battery age and usage
Geneva /
STMicroelectronics (NYSE: STM), a global semiconductor leader supplying customers across the spectrum of electronics applications and a leading manufacturer of standard ICs, has unveiled its latest battery fuel-gauging device featuring patented innovations that improve long-term accuracy. This tiny chip, the STC3115, can be used in high-volume handheld electronics, and has already been selected by Samsung for some of its recent smartphones. Battery charge indicators – or fuel gauges - have become essential for managing devices such as smartphones, laptops or digital cameras. Accurate “time-remaining” predictions enhance the user’s experience, and can be critical in certain types of portable electronics such as medical devices. Even so, many of today’s fuel-gauging electronics are susceptible to errors caused by battery aging, reduced charging efficiency, leakage, variations in system power demand, and temperature effects.
To enhance fuel-gauging accuracy, ST has combined several important advances in its latest adaptive fuel-gauge IC, the STC3115. Until now, leading devices have used Coulomb counting to monitor energy entering and leaving the battery, and periodic voltage-mode state-of-charge measurements to adjust the Coulomb counter for accuracy. The STC3115 uses both sets of measurements continuously, with OptimGauge™, an adaptive algorithm that tracks the state of charge and corrects the battery model.

The STC3115 further enhances accuracy by measuring true initial battery open-circuit voltage and preventing measurement disruptions when connecting the charger or launching an app. The charging inhibitor is a patented feature that significantly improves accuracy. Aging and temperature compensation are built in, and the voltage measurement accuracy is 0.25%.

Additional value-added features of the new IC include a low-power mode that reduces operating current to only 45µA while continuing to monitor the battery, and a 2µA standby mode. An Under-Voltage Lockout (UVLO) filter prevents short-term fluctuations in battery voltage from causing unwanted system resets. In addition, the STC3115 saves bill-of-materials costs by operating directly from the battery voltage without requiring its own voltage regulator.

Key features of STC3115:
• The OptimGauge algorithm, which adjusts the battery charge/discharge model over the battery’s life
• Industry-standard I2C connection to application processor
• Programmable with different battery profiles at manufacture, for flexibility
• Monitors batteries up to 4.5V
• Monitors multi-cell packs when used with TS941ILT low-power buffer
• Dedicated “battery-present” input simplifies battery replacement
• Dedicated alarm output, activated if battery voltage falls below threshold level

The STC3115 is in full production in a 1.4 x 2.0mm chip-scale package, priced from $.95 in quantities of 1,000 pieces. If your company has high-volume requirements please contact your local ST sales office.

Click here for the high-resolution photo

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power and automotive products and embedded processing solutions. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.
In 2012, the Company’s net revenues were $8.49 billion. Further information on ST can be found at www.st.com.