RoHS / ECOPACK
STMicroelectronics is fully committed to Environmental protection within its Sustainable Excellence program. It has been a pioneer in environmental protection since 1992 and kept such issues at the forefront of its management. ST has adopted the most stringent Environment, Health & Safety regulations worldwide and strictly applies these rules to all its sites / organizations. Read more into the following chapters:
Lead-free Quality and Reliability
STMicroelectronics devices are requalified to ensure their resistance to new soldering temperatures requested by PC board mounting with Tin-Silver-Copper alloys : melting temperature of 217°C instead of 183°C for SnPb eutectic alloy.Materials Declaration
STMicroelectronics’ banned, exempted and declarable substances list is regularly reviewed to include regulations and customer requirements and to insure that our suppliers are in line with our rules regarding the use of chemicals and hazardous substances.Lead-free Solutions
The Ecopack working group has selected 3 technologies (NiPdAu, Pure Sn and SnAgCu Ball) to match the different technical and quality requirements and cover the full spectrum of packages. The Conversion program applies both to internal and subcontractor production lines.