/**
  @page TriangularDitherMethod AN2668 TriangularDitherMethod Readme File
  
  @verbatim
  ******************** (C) COPYRIGHT 2009 STMicroelectronics *******************
  * @file TriangularDitherMethod/readme.txt 
  * @author   MCD Application Team
  * @version  V2.0.0
  * @date     04/27/2009
  * @brief    Description of the AN2668 Application note's triangular dither firmware.
  ******************************************************************************
  * THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS
  * WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE
  * TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY
  * DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING
  * FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE
  * CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.
  ******************************************************************************
   @endverbatim
      
@par Description

This firmware gives the STM32L ADC oversampling using triangular dither. This method 
consists on adding a triangular signal to the input signal and sampling it with 
a rate of 1s. 
The timer TIM2 is used to generate the input signal sampling frequency. 
The STM32L ADC clock is configured to 16Mhz and the channel 5 is converted (PA.05).
The triangular dither is generated using the Timer TIM3. 
After OSR DMA transfer from the ADC data register to a buffer in RAM, the new 
sample is computed. 

When uncommenting the Thermal_Noise_Measure, the ADC thermal noise can be 
determined.

When uncommenting the line #define Oversampling_Test, the oversampled data is 
displayed on the hyperterminal and can be captured in a file for the evaluation.
results.
The Hyperterminal configuration is 115.2KB and 8-bit data with 1 stop bit on USART2.

@par Directory contents 
  
  - inc: containing the user header files  
      - TriangularDitherMethod/inc/stm32l1xx_conf.h  Library Configuration files
      - TriangularDitherMethod/inc/stm32l1xx_it.h    Interrupt handlers header files
      - TriangularDitherMethod/inc/oversampling.h    Oversampling header file
    
  - src: containg the user source files  
      - TriangularDitherMethod/src/oversampling.c    Oversampling source file 
      - TriangularDitherMethod/src/stm32l1xx_it.c    Interrupt handlers
      - TriangularDitherMethod/src/main.c            Main program

@par Hardware and Software environment 

    - This example runs on STM32L1xx High-Density, STM32L1xx Medium-Density
      Devices.
            
    - This example has been tested with STMicroelectronics STM32L152-EVAL  
      evaluations board and can be easily tailored to any other supported device
      and development board.

    - Connect the input signal to be converted on ADC Channel 5: PA.05
     
    - Connect a RC signal on the TIM3 output channel
      
    - Use a hardware network to add the input signal and the traingular signal 
      generated by the Timer TIM3. 

    - Set JP13 to 3.3V position.
      
         
@par How to use it? 

In order to load the Oversampling Triagular Dither Method code, you have do the following:

 - EWARM: 
    - Open the Triangular_Dither.eww workspace
    - In the workspace toolbar select the project config:
        - STM32L152-EVAL: to configure the project for STM32L Medium-density devices
    - Rebuild all files: Project->Rebuild all
    - Load project image: Project->Debug
    - Run program: Debug->Go(F5)

 - RIDE: 
    - Open the Triangular_Dither.rprj project
    - In the configuration toolbar(Project->properties) select the project config:
        - STM32L152-EVAL: to configure the project for STM32L Medium-density devices
    - Rebuild all files: Project->build project
    - Load project image: Debug->start(ctrl+D)
    - Run program: Debug->Run(ctrl+F9)

 - MDK-ARM: 
    - Open the Triangular_Dither.uvproj project
    - In the build toolbar select the project config:
        - STM32L152-EVAL: to configure the project for STM32L Medium-density devices
    - Rebuild all files: Project->Rebuild all target files
    - Load project image: Debug->Start/Stop Debug Session
    - Run program: Debug->Run (F5)

 - TrueSTUDO:
    - Open the TrueSTUDIO toolchain.
    - Click on File->Switch Workspace->Other and browse to TrueSTUDIO workspace directory.
    - Click on File->Import, select General->'Existing Projects into Workspace' and then click "Next". 
    - Browse to the TrueSTUDIO workspace directory, select the project:
        - STM32L152-EVAL: to configure the project for STM32L Medium-density devices
    - Rebuild all project files: Select the project in the "Project explorer" 
      window then click on Project->build project menu.
    - Run program: Run->Debug (F11)

 - TASKING:
    - Open TASKING toolchain.
    - Click on File->Import, select General->'Existing Projects into Workspace' 
      and then click "Next". 
    - Browse to  TASKING workspace directory and select the project: 
      - STM32L152-EVAL: to configure the project for STM32L Medium-density devices
     - Rebuild all project files: Select the project in the "Project explorer" 
      window then click on Project->build project menu.
    - Run program: Select the project in the "Project explorer" window then click 
      Run->Debug (F11)
     

@note
 - Medium-density devices are STM32L1xx microcontrollers where
   the Flash memory density ranges between 64 and 128 Kbytes.
 - High-density devices are STM32L1xx microcontrollers where
   the Flash memory density ranges between 256 and 512 Kbytes. 

 * <h2><center>&copy; COPYRIGHT 2013 STMicroelectronics</center></h2>
 */