Contents
- What's
New in AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling" V3.0.0
- What's
New in AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling" V2.0.0
- What
is AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling"?
- AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling" update History
- License
What's New in AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling" V3.0.0?
The AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling"
V3.0.0 is an update of V2.0.0
that makes the application note compliant with the STM32L low power family microcontrollers.
What's New in AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling" V2.0.0?
The AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling"
V2.0.0 is an update of V1.0.0
that makes the application note compliant with the Cortex™
microcontroller software interface standard (CMSIS).
What
is AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling"?
The AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling"
gives two methods to improve ADC resolution. These techniques are based
on the same principle: oversampling the input signal with the maximum 1
MHz ADC capability and decimating the input signal to enhance its
resolution.
The method and the firmware given within this
application note apply to both Medium- and High-density STM32F10xxx
products and STM32L1xxxx products. Some specific hints are given at the end of the application
note to take advantage of the Medium- and High-density STM32F103xx
performance line devices and of the High-density STM32F101xx access
line devices.
This application note is split into two main parts:
the first one describes how oversampling increases the ADC-specified
resolution while the second describes the guidelines to implement the
different methods available and gives the firmware flowchart of their
implementation on the STM32F101xx, STM32F103xx and STM32L1xxxx devices.
The AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling" is full CMSIS compliant.

AN2668 "Improving STM32F10xxx and STM32L1xxxx ADC resolution by oversampling" update History
V3.0.0
- 03/19/2013
- AN2668
V3.0.0 updated to support STM32L1xxxx
microcontrollers
- added STM32L1xx
Standard Peripherals Library (StdPeriph_Lib) V1.1.1
- exaples ported to support STM32L1xxxx
microcontrollers
- AN2668
V3.0.0 updated to support more toolchains
- EWARM, MDK-ARM, RIDE, TASKING, TrueSTUDIO
V2.0.0
- 04/27/2009
- AN2668
V2.0.0 updated with STM32F10x
Standard Peripherals Library (StdPeriph_Lib)
V3.0.0
- AN2668 V2.0.0 is full
CMSIS compliant
- STM32F10x
Standard Peripherals Library Structure is updated.
- AN2668 Package
Architecture is enhanced
For
more details, please refer to AN2953 "How to migrate from the
STM32F10xxx firmware library V2.0.3 to the STM32F10xxx standard
peripheral library V3.0.0".
V1.0.0
- 09/08/2008
- Updated with STM32F10x FWLib V2.0.1
- Add Project with RIDE and HITOP, EWARM toolchains
V0.1 - 01/25/2008
License
The
enclosed firmware and all the related documentation are not covered by
a License Agreement, if you need such License you can contact your
local STMicroelectronics office.
THE
PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS
WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO
SAVE TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR
ANY DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY
CLAIMS ARISING FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY
CUSTOMERS OF THE CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH
THEIR PRODUCTS.
For
Complete on STM32(CORTEX M3) 32-Bit Microcontrollers
visit www.st.com/STM32
|