AN1051 APPLICATION NOTE TSM102 : A DUAL LI-ION BATTERY CHARGER USING AN ST SILICON TRIPLET
by A. BAILLY, D. CABROL, J. CAMIOLO S. LAFFONT, R. LIOU
This application note explains how to use the VIPER20, the ST62 Controller and the TSM102A in an SMPS-type battery charger which features : Dual Li-Ion Battery charging with Constant Current/Constant Voltage Battery type recognition (4.1V or 4.2V and different capacities) Precision Voltage Control Temperature and Failing Battery protection End of Charge detection
. . . . .
1 - DEVICES PRESENTATION The VIPER20 integrates on the same chip a PWM circuit together with a high voltage avalanche rugged vertical MOSFET (600V, 0.5A) which make it ideal for primary side control of battery chargers or power supplies featuring up to 20W output. Moreover, this device allows stand-by mode operation without additional components. The ST62T25C is a low cost 28 pins 8-bit Microcontroller available in Mask ROM, FastROM and OTP versions. It features an A/D converter with up to 16 channels, 20 I/O pins of which 4 have High Current capability. An integrated Static Reset circuitry, Oscillator Safe Guard, 3 to 6 V power supply range and high ESD tolerance make the device well suited for noisy environment. The TSM102A integrated circuit includes two Operational Amplifiers (type LM358), two Comparators (type LM393) and one adjustable precision Voltage Reference (type TL1431 : 2.5V to 36V, 0.4% or 1%). TSM102A can sustain up to 36V power supply voltage. Figure 1 : ST62T25C, TSM102A and VIPER20 Pin
Vdd TIMER OSCin OSCout NMI PC7 PC6 PC5 PC4 TEST !RESET PB7 PB6 PB5 1 2 3 Vss PA0 PA1
28 27 26
20mA
ST62T25C
4 5 6 7 8 9 10 11 12 13 14
25 24 23 22 21 20 19 18 17 16 15
PA2 PA3 PA4 PA5 PA6 PA7 PB0 PB1 PB2 PB3 PB4
1 2 3
TSM102
16 15 14
PowerSO-10
OSC Vdd NC NC COMP
6 7 8 9 10 5
Pentawatt-HV
DRAIN
VIPER20
SOURCE SOURCE NC
V+ CC
5 6 7
COMP
COMP
VCC
12 11 10
VIPER20
4 3 2 1
1
5
2
4
3
SOURCE SOURCE
OSC
Vref
Cathode
DIP28 - SO28
SOURCE
DRAIN
Vdd
February 1999
COMP
1/9
AN1051 - APPLICATION NOTE
2 - APPLICATION CONTEXT AND PRINCIPLE OF OPERATION The Li-Ion Battery Rechargeable battery using Lithium have high voltage, big capacity and light weight, yielding an extraordinary energy density, more than twice the one of the NiCd. The maximum load current is not as high as for the NiCd, but is still sufficient for many applications such as cellular phone and camcorder. To improve lifetime and keep the battery in safe operating conditions, some protection circuitry is always added inside the battery pack that can disconnect the electrochemical cell from the external connectors. This protection circuitry is designed to trigger in case of overcurrent (both when charging and discharging), overvoltage (when charging) and undervoltage (when discharging). The cell temperature is also monitored. Charging Principle The charging principle of the Lithium-Ion batteries is very different from the Nickel type. Figure 2 shows the different stages in the charging process. Time values are only indicative and depend on battery type and speed of charge. Figure 2 : Li-Ion Charging Scheme
I V Cell voltage rises to voltabe limit
Maximum cell voltage is reached Occasional topping charge is applied if battery voltage drops
15
30
45
CONSTANT CURRENT CHARGE
60 75 90 105 120 135 150 165 180 minutes of charge 1h CONSTANT NO TRICKLE 2h
VOLTAGE CHARGE 70% charged Charge current starts to drop as the battery gets saturated. CHARGING 100% charged The Li-ion battery cannot absorb over-charge. Trickle charge would be harmfull.
Maximum charge current is applied until the set voltage limit is reached.
During Stage 1, the battery is charged at constant current. The battery voltage is slowly increasing from original voltage up to the maximum cell voltage, which depends on the battery electrode technology (4.2V/cell for coke electrode, 4.1V/cell for graphite electrode). Should this maximum voltage be exceeded and the battery could suffer significant damage and the protection circuitry may trigger. Thus during Stage 2 a constant voltage charge is applied. Battery chargers manufacturers recommend a highly precise voltage supervision of 0.05 V/cell. The current is slowly decreasing as the battery gets closer to full capacity. End of charge can be detected by the charge current getting lower than a fixed threshold value (usually one fifth to one tenth of the constant current charge value). The dual Li-Ion Batteries charger : In this application which requires ever increasing performances in more and more reduced space, the silicon triplet VIPER20, ST62T25C and TSM102A provides an attractive solution in terms of performance, cost efficiency and versatility.
2/9
AN1051 - APPLICATION NOTE
Figure 3a and 3b show the primary and the secondary sides of the battery charger (SMPS type, primary and secondary sides) where the VIPER20, the ST62T25C and TSM102A are combined to ensure safe charging of two Li-Ion battery cells in parallel (main and spare batteries). The Viper20 ensures with a very low component count the energy transfer from the off-line primary side to the secondary side thanks to its PWM ability ( with externally adjustable frequency of operation) and integrated high voltage avalanche-rugged vertical MOSFET. The ST62T25C Controller is used to : · recognize the Li-Ion battery type (4.1V or 4.2V and capacity) · manage the charging of the two different cells in parallel thanks to the proper command of two power switches · prevent the battery charging in case of overtemperature or undertemperature · drive adequate LEDs for convenient visual information The TSM102A can ensure all analog interfacing between the batteries and the P by · controlling current and voltage with adequate feedback via the optocoupler to the primary side · offering highly precise voltage reference for all measurements · amplifying the current signal through the sense resistor to be monitored by the Controller · providing a low cost solution for 5V power supply of the MCU Figure 3a : Primary Side of Battery Charger
3/9
AN1051 - APPLICATION NOTE
In detail : a - The Primary Side : The VIPER20 stands as a PWM circuit with integrated Power MOSFET after the Rectifying-Filtering stage (F01 fuse, R03 NTC, L02 and C04 filtering coil and capacitor, D03 diode bridge and C03 front bulk capacitor). R01 and D01 ensure the correct supplying of the VIPer20 device during normal operation thanks to the auxiliary winding of the transformer. C05 is in charge of filtering this output, and provides also the needed energy at start up thanks to the integrated start up current source of the VIPer20 device. The PWM function is determined by R02, D06 (frequency of operation) and the collector and emmitor of the photocoupler (linear width modulation). The couple R04, C07 is a compensation network. b - The Secondary side : Figure 3b : Secondary Side of Battery Charger
4/9
AN1051 - APPLICATION NOTE
POWER SUPPLY : Both ST62T25C and TSM102A are supplied by a regulated 5V line. This line is regulated from the SMPS Auxiliary output thanks to an NPN bipolar transistor (Q1) polarized via its base by the integrated adjustable precision Voltage reference of the TSM102A (R2, R3). The base of Q1 is pulled up by R1 to ensure proper start up conditions and also to limit the current through the Voltage Reference during regulation mode. This 5V regulation circuitry is smoothened by the input and output capacitors C1 and C2. VOLTAGE AND CURRENT REGULATION : The two comparators of TSM102A are used to regulate the voltage and the charging current of the batteries. The first comparator compares the precise 2.5V Reference voltage with a part of the SMPS Main Output (resistor bridge R4, R6) and the second comparator compares the voltage drop through the sense resistor R0 with a part of the regulated 5V line (resistor bridge R11, R12). The feedback to the primary side is achieved thanks to the pair of ORing diodes (D1, D2) which pulls linearly the photocoupler (PH1) down via the resistor R8. Compensation loops (R9, C3 and R10, C4) and output capacitors (Co1 and Co2) are added to stabilize the voltage and current regulations. BATTERY TYPE DETECTION AND CHARGE PARAMETERS ADJUSTMENT : Pins C/F and V/F of the battery packs are used to provide charging voltage (V/F) and charging current (C/F) information to the charger. Resistors R30, R31, R35 and R36 are used to make resistor bridges with internal battery pack resistors, which connect V/F and C/F pins to the battery pack ground pin as shown on figure 4. Figure 4 : Battery Pack Internal Schematics and Principle of Detection
5V + V/F
+ to MCU A/D
+
C/F
MCU Gnd -
Table 1 : BATTERY VOLTAGE DETECTION FROM V/F
V/F Resistor 10k 5% 4.7k 5% other V/F Voltage 2.375~2.625 3.29~3.51 other 8 bit A/D Result 117~138 163~183 other Detected Battery Voltage 4.1V 4.2V no battery
Table 2 : BATTERY CURRENT DETECTION FROM C/F
C/F Resistor 3.3 ~ 4.7k 5% 2.4k 5% 1.1k 5% other C/F Voltage 2.375~2.625 3.29~3.51 4.02~4.17 other 8 bit A/D Result 119~136 165~181 203~205 other Detected Battery Voltage 400mA 800mA 1300mA no battery
5/9
AN1051 - APPLICATION NOTE
The Controller is using A/D converters inputs PA6, PA7, PB2 and PB3 to measure respectively the voltages on battery pack pins V/F1, C/F1, V/F2 and C/F2. Depending on these voltages the Controller will switch various Open Drain pins to adjust the Voltage and Current regulation loops to the requirements of the battery currently in charge. Thus depending on the V/F pin voltage, the resistor R7 can be connected in parallel with R6 through PC4 which is configured in Open Drain mode. This will modify the resistor bridge R4, R6, and will set the voltage regulation to 4.1V or 4.2V in respect with the battery type. The detection of the battery voltage is summarized in Table 1. The 5% tolerance of the resistors, as well as the 2 LSB accuracy of the Analog to Digital Converter are taken into account for the calculation. In a similar way, and depending on the C/F pin voltage, the charge current is set to match the requirements of the battery. PC5, PC6 and PC7, configured in Open Drain mode, command the PNP transistors Q2 (PC5), Q3 (PC6) and Q4 (PC7). When Q2, Q3 or Q4 (or the three at the same time) are on, the current control value is modified according to the resistor bridge (R11, R12) modification (R14, R15, R16 in parallel with R11). The detection of the battery charge current is summarized in Table 2. CURRENT FEEDBACK TO THE CONTROLLER : One Operational Amplifier of the TSM102A is used to zoom the current that flows through the sense resistor R0 (amplification loop R17, R19) so that this current information can be readable by the Controller. The Controller acquires the data though PB7 configured as and A/D input. 2 SLOTS CHARGING FLOW : In this specific application the first slot (A) is made to receive a complete handy phone while the second one (B) is made to accommodate a spare battery. Thus the user can charge both his phone + battery and a replacement battery. To ensure efficient charging of both batteries cells (which are connected in parallel), the Controller commands two low Rdson P-channel MOSFETs alternatively (Q5 and Q6 with PB4 and PB5). If only one of the slot receives a battery (either A or B) the charger will perform a standard charge of that battery by switching on the corresponding MOSFET. When the charger receives both the phone + battery (A) and the spare battery (B), the A slot has the priority. Q5 will be turned on first and until A battery is full, B will be in Wait for Charge state, and Q6 will be off. Only when A is full will B be charged (Q5 off, Q6 on). As the phone in slot A may be on, and thus its battery may discharge as B is on charge, the voltage of A slot is continuously monitored. If a significant drop is detected, then the charger will enter an alternate charging mode where both batteries are charged on a time sharing basis, so as to always keep the phone battery in full condition. USER INTERFACING : The Controller drives directly 2 bicolor LEDs (one for each battery) through PA0, PA1, PA2, PA3. The meaning of the different signals in given in Table 3. Table 3 : USER INTERFACE LEDs
State No battery Charging Full Wait for charge Battery fail Over/Under temperature Green Off Off On On Blink On Red Off On Off On Blink On Bicolor Result Off Red Green Orange Orange Blink Orange Remark each slot each slot each slot B slot only each slot only when charging
6/9
AN1051 - APPLICATION NOTE
PROTECTION/SAFETY FEATURES : The Controller is checking the charging process in several ways so as to make sure that the battery is kept into safe operating conditions. Temperature is measured via resistor bridge R21 and R22 (where R22 is an NTC) and PB6 configured in A/D input. According to Li-Ion manufacturers information the cells should be charged only when the temperature is between 0 and 45 C. Thus when the temperature reaches outside this safe operating range, the charging process is kept in standby (charge timings held, Power MOSFETs off thus stopping the charge current, and user is warned of this condition by corresponding LED turning orange). When the temperature is back to normal, charging process is resumed. The 0 and 45 degrees threshold level have a programmable software hysteresis to prevent the charger from oscillating form Temperature protection to Normal mode. Open battery condition is detected using current measurement through PB7. If no current is flowing for more than a programmable current establishment delay after the charge has started the battery will be rejected, the charge terminated and the user warned of this condition by the corresponding LED blinking orange. Bad voltage battery condition : the Controller is continuously monitoring the voltage of the batteries. According to the battery manufacturers specifications, and depending on the voltage, the actions of the charger are summarized in Table 4.
. . . .
Table 4 : CHARGER STATE AS A FUNCTION OF BATTERY VOLTAGE
Voltage 0 - 1.5V 1.5 - 2.7V 2.7 - 4.1/4.2V 4.4V and over Very low Normal Overvoltage State Pack protection circuitry active Action Trickle charge Trickle charge Standard charge Stop charge Condition V > 1.5V within 1 second V > 2.7V within 30 minutes V > 3.9V when battery is full -
The Condition Column shows what the result of the action must be for the charger to proceed with the charging. In case this condition is not fulfilled, the battery will be rejected, the charge terminated and the user warned of this condition by the corresponding LED blinking orange. FULL BATTERY DETECTION : This is made either by detecting a low current flowing through the battery or by an overtime condition (maximum time after standard charge has been started). A minimum voltage of 3.9 volt must be reached at that time or the battery will be rejected, and the user warned of this condition by the corresponding LED blinking orange. 3 - CALCULATION OF THE ELEMENTS All the components values have been chosen for a two-Lithium-Ion batteries charge application: PWM Frequency and Maximum swithching ratio of the VIPER20 : R02 > 1.2k Fsw = 2.3 Dmax / (R02 x C06)
Dmax = 1 - 550 / (R02 - 150) recommended Dmax values are : 100kHz : Dmax > 80% 200kHz : Dmax > 70% R02 = 4.7k C06 = 4.7nF Dmax = 87.9% Fsw = 91.5kHz 5V line power supply for TSM102A & ST62T25C : Vout = Vref ( 1 + R2 / R3 ) R2 = R3 = 10k C1 = C2 = 10F R1 = 1.5k Voltage Control : Vbatt = 4.100V Vref = Vbatt x R6 / ( R6 + R4 ) With R6 = 100k, R4 = 64k
.
7/9
AN1051 - APPLICATION NOTE
If the battery is a 4.2V type, then, the resistor R7 will be connected in parallel to the resistor R6 by means of the Controller (PC4) : Vbatt = 4.200V Vref = Vbatt x (R6 // R7) / [ (R6 // R7) + R4 ] where Rlim2 = R11 // R14 Rlim2 = 4.957k Therefore, R14 = 9.83k Third current limitation : Ilim3 = 800mA Vlim3 = R0 x Ilim3 = 160mV = Vcc x R12 / (R12 + Rlim3) where Rlim3 = R11 // R15 Rlim3 = 2.438k Therefore, R15 = 3.22k Fourth current limitation : Ilim4 = 1.3A Vlim4 = R0 x Ilim4 = 260mV = Vcc x R12 / (R12 + Rlim4) where Rlim4 = R11 // R16 Rlim4 = 1.469k Therefore, R16 = 1.72k
. . . .
. .
Vref = Vbatt x [ R7 x R6 / ( R6 + R7) ] / [ R7 x R6 / ( R6 + R7) + R4 ] R7 = 1.6M Current Control : Lowest current limitation : Ilim1 = 200mA, with sense resistor R0 = 0.2 Vlim1 = R0 x Ilim1 = 40mV = Vcc x R12 / (R12 + R11)
with R11 = 10k, R12 = 80.6 Second current limitation : Ilim2 = 400mA Vlim2 = R0 x Ilim2 = 80mV = Vcc x R12 / (R12 + Rlim2)
OTHER COMPONENTS : All other components values are indicated on the schematics Notes : When plugged in the sockets, the two batteries can have very different charge states (ie one is fully charged and the other, almost empty). If no precaution is taken, and as long as the two batteries voltages differ from more than 0.6V, a dramatic current flow can appear between the charged battery towards the empty battery through the intrisic diodes of the power MOSFETS. This current is not regulated and may either damage the MOSFETS, or trigger the over current protection system of the battery pack itself and block the charging of the battery. The schottky diodes D7, D8, the diode D6 and the PNP transistors Q7, Q8 solve this problem : · no current can flow through the intrinsic diodes of the MOSFETS thanks to the schottky diodes · the voltage regulation is picked directly on the battery packs for increased precision thanks to the PNP bipolar transistors used as low power analog switches
. . . . .
8/9
· the diode D6 prevents the voltage regulation from loosing its reference when the two Power MOSFETS are OFF. The current control values must be chosen in accordance with the elements of the primary side. The global performances of the battery charger are highly dependent on the adequation of the primary and the secondary elements. R13 and R18 are the equivalent resistors seen from the opamp and from the comparator (R13 = R11//R12, R18 = R17//R19) C7 to C13 capacitors are optional filtering capacitors which ensure proper stabilization of the analog values imposed to each of the corresponding A/D converters of the Controller. Transistors Q9 and Q10 are inserted to ensure good start up conditions (open collector until the C is correctly supplied). An improvement to the integrated Voltage Reference's line stability is shown on figure 5. The LED D' (used as a visual "charger is ON" signal) polarized by the resistor R' feeds the PNP bipolar transistor Q' with a quasi constant voltage which allows constant current to flow through the Vref. This regulated 5V line provides a very stable voltage even when the SMPS Aux Output varies from 7 to 30V.
AN1051 - APPLICATION NOTE
Figure 5 : Improved Voltage Reference Line Regulation
Q1 R1 D' Q' R2 R' C1 Vref C2 +5V
R3
Caution :
Li-ion batteries have a very high energy density. Exercise precaution when handling and testing. Do not short circuit, overcharge, crush, mutilate, nail penetrate, apply reverse polarity, expose to high temperature or disassemble. High case temperature resulting from abuse of the cell could cause physical injury.
Information furnished is believed to be accurate and reliable. However, STMicroelectronics assumes no responsibility for the consequence s of use of such information nor for any infringement of patents or other rights of third parties which may result from its use. No license is granted by implication or otherwise under any patent or patent rights of STMicroelectronics. Specifications ment ioned in this publication are subject to change without notice. This publication supersedes and replaces all information previously supplied. STMicroelectronics products are not authorized for use as critical components in life support devices or systems without express written approval of STMicroelectronics. The ST logo is a trademark of STMicroelectronics 1999 STMicroelectronics Printed in Italy All Rights Reserved STMicroelectronics GROUP OF COMPANIES Australia - Brazil - Canada - China - France - Germany - Italy - Japan - Korea - Malaysia - Malta - Mexico - Morocco The Netherlands - Singapore - Spain - Sweden - Switzerland - Taiwan - Thailand - United Kingdom - U.S.A. http://www.st.com
9/9
|