Performance
Overview
Chemicals
Our manufacturing processes require significant amounts of chemicals especially in front-end processes. Since some chemicals have a potential impact on the environment and also carry health and safety risks, we work hard to keep their use to a minimum. The chemicals we target are photoresists, developers, sulfuric acid, hydrogen peroxide, hydrofluoric acid, and a selection of solvent compounds.
STEV64; §2.3 Decalogue
We have exceeded our target of reducing by 5% a year the consumption of chemicals per unit of production. In 2005, our front-end sites reduced the consumption of chemicals per production unit by 0.3% versus 2004, while back-end sites reduced by 22% over the same period.
As in the case of water consumption, the increase in absolute values (+10% from 2000 to 2005) is due to the significant increase in production (+83% over the same period).
| Consumption of chemicals: absolute values |
| Net consumption |
2000 |
2001 |
2002 |
2003 |
2004 |
2005 |
| Tons of chemicals |
16,947 |
13,053 |
14,188 |
15,345 |
16,938 |
18,669 |
These net values would have been much higher without the actions we have taken.
The chart below shows our performance against our Decalogue target (reduction by 5% per year) since 2000 (our reporting system for chemicals was not reliable enough to publish before that date).
| Consumption of chemicals: normalized values |
 |

|
| |
2000 |
2001 |
2002 |
2003 |
2004 |
2005 |
| kg/production unit |
100 |
79.1 |
71.1 |
65.5 |
61.1 |
60.2 |
| Target |
100 |
95.0 |
90.3 |
85.7 |
81.5 |
77.4 |
See the Environmental costs versus savings table for details of the cost savings resulting from reduction of consumption of chemicals.
|