Section
 

Issue No. 2 - June 1999
testata
New and Views from STMicroelectronics



cover


botton Editorial Notes
botton MP3: THE SOUND of MUSIC
The Internet is alive with the sound of music thanks to MP3, an audio compression standard that allows digital music files to be compressed by a factor of ten without compromising quality.
botton PERFECT VISION :
New perspectives in system-on-chip technology with ST's acquisition of Vision Group plc, a leading designer and supplier of CMOS image sensors. ST now offers the most comprehensive family of CMOS video camera reference designs and chipset solutions for both analog and digital video applications.
botton TALK TO ME !
Euterpe is a new chip family from ST that simplifies the task of adding speech recognition, text-to-speech and other key voice-related functions to automotive systems, household appliances, instrumentation and many other applications that will benefit from the most natural of all man-machine interfaces.
botton Around the World
News and views from STMicroelectronics around the world.
botton REDEFINING THE DSP
The ST100 is offers 'future proof' , state-of-the-art performance thanks to a scaleable architecture with multiple instruction sets.
botton EXTENDING EMBEDDED FLASH TECHNOLOGY
The ST92F120 is the latest edition to ST's 8/16-bit ST9 family. It provides a unique emulated EEPROM (E3PROM) capability that removes the need for external EEPROM memory.
botton Fact File
botton Brain Teaser
botton Show Time

Editorials Notes Head

More than Meets the Eye

A quick look at the contents of this number of Challenge might give the impression that we set out to produce a special DSP issue. In addition to the article describing the innovative architecture of the ST100 core, which was recently unveiled at the Embedded Processor Forum in San Jose, two of the other main products featured in this issue - the Euterpe voice processors and the STA013 MP3 decoder - also use built-in DSPs to achieve their high performances.

In fact, this apparent focus on DSP is coincidental but illustrates one of ST's less well-known strengths: the depth and breadth of its competence in Digital Signal Processing. The Company does not compete in the stand-alone general purpose DSP market but it has accumulated a wealth of expertise in DSP which it uses internally to develop standard products and makes available to customers through its ASIC libraries.

Around ten years ago, ST pioneered the concept of embedding a DSP core in an ASIC device and launched the world's first embedded DSP core in 1991. Since then, PC sound cards, cellular phones and hard disk drives are among the applications where ST has shipped high volumes of customer-specific devices containing embedded DSPs, while many standard products such as modem chips are based on the same cores.

Today, ST designers can draw upon a range of DSP cores, including cores that are optimized for particular kinds of applications such as audio products. These are all part of one of the world's most comprehensive portfolios of libraries and technologies developed to ensure that ST can deliver leading-edge devices, whether they are standard products or complete system-on-chip solutions.

Two of the other articles in this issue underline this point. ST's patented Emulated EEPROM (E3PROM) technology offers a unique advantage to designers who need a high performance microcontroller with on-chip Flash memory for code storage, while the recent acquisition of Vision Group opens up many exciting new opportunities for integrating image capture and image processing on the same chip.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.