Section
 

Issue No. 4 - December 2000
testata
New and Views from STMicroelectronics



cover october


2001

botton Editorial Notes
botton THE BIG PICTURE
Challenge looks at the comple factors that determine how semiconductor
manufacturers can respond to the System-on-Chip challenge.
botton EASING THE INTERNET BOTTLENECK
With Internet complexity nearing the "choke zone" ST and San Jose-based
Lara Technologies, are working to standardize APT search engines
as network database search accelerators, and extend their use to image,
voice and pattern recognition applications.
botton THREE NEW SYSTEM-on-CHIP
INFORMATION APPLIAMCE ENGINES

ST launches three additions to its range of 5th generation STPC products
at astonishing speeds and astonishing prices.
botton Around the World
DOING GOOD and DOING WELL
Topping 14 global semiconductor enterprises, ST was the only company to earn an AAA rating for eco-efficiency in a recent in-depth report. Challenge looks at some of ST's ambitious environmental goals and impressive achievements.

RADIO ENTERS the 21st CENTURY
botton POWERING the CAR DASHBOARD REVOLUTION
Investigating the replacement of mechanical instruments in a conventional
car dashboard by a single display which will deliver all information
via a single, customizable unit.
botton PERVASIVE PASSIVES
The more we integrate intelligence and functionality into the SoC solution,
the more frustrating it is that resistors, capacitors, inductors and protection
diodes are needed to make it all work reliably. Enter ST's IPAD™
technology (Integrated Passives and Active Devices), which is making
a huge difference.
botton FINE-TUNING the VOICE over INTERNET PROTOCOL
botton NAND vs NOR
The end of the debate on NAND versus NOR
botton Brain Teaser

Editorials Notes Head

The Tip of the Iceberg

Moore's Law, that the number of transistors that can be integrated onto a single chip doubles about every 18 months, has played such an important role in the evolution of the electronics industry that it has now become well known even outside the industry. Less well known are other trends where the pace of change is even faster. Connectivity bandwidth, for example, doubles every 12 months, while the amount of embedded software shipped with new products doubles every ten months.

To these we can add the more general market trend of "consumerization" i.e. increasingly unpredictable market cycles, continuous upgrading of models to gain short-lived price/performance advantages, increasing pressures on profit margins, the growing role of brand recognition and distribution channels ... and so on. Even the acronyms we use are coming under pressure: VoIP, for example, means Voice over Internet Protocol today but tomorrow it will mean Video over Internet Protocol.

Although Moore's Law remains the most significant and visible driving force in our industry, it is just the tip of the iceberg and staying at the forefront of technology is just one of many different challenges for today's chip manufacturers.

The nature of some of these challenges were examined at ST's recent "Big Picture" event that is the lead article in this issue of Challenge. Other articles in this issue reflect one of the most important of these challenges, which is the need for chip manufacturers to be work with a wide variety of partners to enable the exploding technological capabilities to be applied in highly dynamic markets. These include partnerships with specialist companies such as Lara Networks (for IP packet processing engines) and Netergy Networks (for VoIP), as well as research projects such as ACTIVE that bring together multiple, complementary skills.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.