Section
 

September 2000
pnews title


cover

switch mode power supplies

botton Editorial Notes
botton VIPer : TIME to SWITCH
botton L6590 : A FULLY INTEGRATED
POWER SUPPLY
botton L6561 POWER
FACTOR CORRECTOR
botton L6598 : HIGH VOLTAGE HALF
BRIDGE SUPPLY CONTROLLER
botton L5991 and L5991A :
HIGH PERFORMANCE
PWM CONTROLLERS
botton NEW GENERATION
LOW VOLTAGE MOSFETs
botton NEW GENERATION HIGH
VOLTAGE MOSFETs
botton L5970 : HIGH EFFICIENCY
STEP-DOWN
SWITCHING CONVERTER
botton L4957 ULDO LINEAR REGULATOR
botton THE ULTRA FAST 300V
DIODE ADVANTAGE
botton TSM102 and TSM104 : the MORE
INTELLIGENT BATTERY
CHARGERS
botton TSM101 and TSM103 :
the VOLTAGE PRECISION
and CURRENT CONTROL
in BATTERY CHARGERS
and ADAPTERS
botton LD1084/5/6 SERIES for POST
REGULATION in SMPS

Editorial Notes


Dear Reader,

Switch mode power supplies today are used in almost every type of electronic equipment. The change from the traditional 50/60Hz transformer to switch mode power has been driven by the increasing demand from the equipment manufacturer and end-user for higher output power and efficiency, smaller size and less weight.

Accordingly, the components change. In place of slow diodes for the bridge rectifier and linear regulators for post regulation, we now find high frequency switches such as MOSFETs; fast rectifiers with low forward voltage and small recovery chargers such as Schottky diodes; PWM controllers and monolithic DC/DC-converters. At the same time, new standards are emerging that will require new and improved semiconductors: for reduced standby power consumption, or for sinusoidal in-phase current consumption, for example.

STMicroelectronics is not only a leading supplier of semiconductors for the switch mode power supply market, the Company is also one of the few suppliers able to provide the broad range of devices necessary for this dynamic sector - from diodes and MOSFETs to control circuits and integrated converters.

In this special issue of Product News STMicroelectronics presents a selected portfolio of products specially designed for switch mode power supplies.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.