Section
Author's Guide | Reviewer's Guide

ST Journal of Research
MEMS

Vol. 3, No. 1, August 2006- Art. 4
 
Novel process for realization of multiple axis actuators suitable for the realization of an optical switch

Details of MEMS devices

by
Marco Del Sarto, Simone Sassolini, Mauro Marchi, Lorenzo Baldo, STMicroelectronics

Copyright
Copyright 2005 Society of Photo-Optical Instrumentation Engineers.

 

Abstract
A new MEMS for on-chip mechanical testing of 0.7 µm thick LPCVD polysilicon film has been designed, modelled, and fabricated. The polysilicon film is electrostatically loaded under bending until rupture in the out-of-plane direction. Electrostatical numerical simulations were carried out to evaluate the force developed by the actuator and the capacitance measured by the sensing electrodes while structural numerical simulations were used to compute the stress field into the specimen and its stiffness. Elastic properties and ultimate strength of the material were determined. Comparative studies were performed to investigate the variation of the ultimate strength of the polysilicon film with different loading conditions.

 

Download Art 4 (PDF Format) Size KB 700 page 29