Section
Author's Guide | Reviewer's Guide

ST Journal of Research
MEMS

Vol. 3, No. 1, August 2006- Art. 9
 
A simple lumped electrical model for an RF MEMS switch considering lossy substrate effects

RF MEMS switch by
Giuseppe Cusmai, Marco Mazzini, Paolo Rossi, Francesco Svelto, University of Pavia; Chantal Combi, Benedetto Vigna, STMicroelectronics

Copyright
Copyright © Elsevier, 2005 - Reprinted from Sensors and Actuators A 123–124 (2005), 515–521, http://www.elsevier.com/wps/find/journaldescription.cws_home/ 504103/description#description
 

Abstract
This work focuses on Micro-Electro-Mechanical-Systems (MEMS) capacitive switches, intended for adaptive output stage of power amplifiers. These devices are particularly attractive because, theoretically, they are capable of very high quality factor values due to the air gap between plates and the low resistivity of lines and bridge. On the other hand, substrate parasitic effects, overlooked up to now, can seriously impair device performance.
In this paper, we introduce a lumped element equivalent circuit taking into account substrate effects. Model validation is based on measurements carried out in the 50MHz-40GHz range.

 

Download Art 9 (PDF Format) Size KB 550 page 83