Section
Author's Guide | Reviewer's Guide

ST Journal of Research
Wireless Sensor Networks

Vol. 4, No. 1, May 2007 - Art. 11
 
Implementing ECC for 8-bit Systems and Power Consumption

image: multiprocessor board on music notes background

by
Guido Bertoni, STMicroelectronics; Luca Breveglieri,
Matteo Venturi, Politecnico di Milano

Copyright
Copyright © STMicroelectronics, Politecnico di Milano, 2007

 
Abstract
Public key cryptography is widely considered as the fundamental building block for key exchange; different public key algorithms are standardized and used in many applications. Among them, ECC (Elliptic Curve Cryptography) is considered the best solution in terms of security, computational requirements, and storage needs for secret and public keys. Energy consumption is one of the main constraints to be considered in wireless sensor networks. In the case of sensor networks, the typical approaches of minimizing latency via a complete hardware coprocessor and of reducing area overhead via an efficient implementation of finite field operations might not provide the best solution. In this paper, two coprocessors for minimizing both additional resources and power consumption are presented. Costs and performances of such coprocessors are compared with known results, showing that space exists for the reduction of energy consumption without degrading the other performance figures.
 

Download Art 11 (PDF Format) Size 510 KB page 154