Section
 

Memory Chip Combines FLASH and EEPROM

SGS-THOMSON, the world's number one supplier of EEPROM memories, has announced the availability of the M39432, a product that combines a 4Mbit FLASH memory and a 256Kbit parallel EEPROM memory on the same chip. Designed for use in cellular phones and other hand-held portable equipment where designers have up till now been forced to use separate FLASH and EEPROM memories, the M39432 is the first of a series of FLASH+ memories built with a proprietary technology that combines the functionality of EEPROM with the cost-effectiveness of a single-transistor FLASH process.

Housed in a 40-pin TSOP package, the M39432 allows the two separate devices currently required to be replaced by a single device without any loss of functionality; the flash memory is a 4Mbit array with sector protection and erase suspend/resume features while the EEPROM is a full featured 256Kbit memory with software data protection, 64 byte page mode and enhanced end-of-write detection. Because both memory functions are implemented in the same technology, much of the support circuitry that would be duplicated in discrete flash and EEPROM devices, including charge pumps for on-chip generation of the programming voltage, address logic, state machine and I/O buffers, is shared.

The M39432 offers substantial benefits compared with the alternative technique of emulating the EEPROM function in a flash memory. The emulation method involves storing “EEPROM” data as linked lists in a sector of the flash memory, with a second sector reserved to take over when the first sector becomes full. To access an “EEPROM” location, the host processor performs a series of reads from the bottom of the linked list until it locates the final value. Every time the data is changed, the time taken to access it again increases. In addition, simulation requires about 16Kbyte of software that must run on the host processor and around 4Kbyte of code that must be copied to external RAM.

The M39432 eliminates this cumbersome procedure by offering concurrent operation of the FLASH and EEPROM functions. Because the EEPROM block manages its write cycle internally once the host controller has issued the Program command, the host controller can read the flash memory while an EEPROM write cycle is in progress. Other immediate benefits include lower component and inventory management costs, reduced PCB area, greater reliability (thanks to the reduction in the number of solder joints) and lower power consumption.

FLASH+ technology is based on a standard 0.6 micron FLASH memory process with proprietary enhancements to yield a double poly/double metal process that is a little more complex than the industry standard double poly/single metal EEPROM process but provides significantly greater memory densities. The process is also being used to build high density parallel EEPROMs.

Should you require more information, please select the appropriate contact from the "Related Topics" menu.