Section
 

DELPHI AUTOMOTIVE SYSTEMS AND STMICROELECTRONICS ANNOUNCE THE DEVELOPMENT OF MOBILE MULTIMEDIA LINK

BRUSSELS, Belgium December 3rd, 98 – STMicroelectronics (ST) and Delphi Automotive Systems have signed an agreement at the ERTICO meeting here today to accelerate the development and licensing of an advanced automotive grade multimedia bus architecture called Mobile Multimedia Link, or MML. ST is responsible for the design of the MML integrated circuit (IC) in advanced CMOS technology, which combines the protocol handler and physical layer in a single IC.

Delphi Automotive Systems has developed the entire MML system architecture including software protocols, the physical implementation of the MML IC and optical physical layer. Based on the success of prototype systems utilizing first silicon, both companies believe the MML system will be ready for production in the 2002CY timeframe.

The MML bus system, which utilizes plastic optical fiber technology in a star architecture, is capable of speeds in excess of 100Mbit/sec. At these speeds, it will allow full MPEG2 stream transmission for high quality video with any display size. ST is a recognized leader on MPEG2 technology. In addition, its star design topology using Delphi’s patented optical star technology, makes it fault tolerant and plug and play ready. These key characteristics make it the most advanced bus architecture for automotive applications in the world.

The MML bus architecture is currently open to the market, with a full set of third party development tools provided by C&C Electronics.

Delphi Automotive Systems is helping to bring enhanced communications, information and entertainment into vehicles through its experience in designing and producing advanced electronics, optical systems, including optical connection systems with integrated optoelectronic devices and passive optical stars.

Delphi Automotive Systems, with headquarters in Troy, Mich., USA is the world’s most diversified supplier of automotive components and systems. Delphi operates 171 wholly owned manufacturing facilities, 46 joint ventures and 27 technical centers in 36 countries. Regional headquarters are located in Paris, Tokyo and Sao Paulo.

STMicroelectronics (formerly SGS-THOMSON Microelectronics) is a global independent semiconductor company, whose shares are traded on the New York Stock Exchange, on the Bourse de Paris and on the Milan Stock Exchange. The Company designs, develops, manufactures and markets a broad range of semiconductor integrated circuits (ICs) and discrete devices used in a wide variety of microelectronic applications, including telecommunications systems, computer systems, consumer products, automotive products and industrial automation and control systems. In 1997, the Company received numerous awards, including the European Quality Award, and has been recognized as one of the world's best companies by Industry Week and Upside magazine.

C&C founded in 1990 as a joint venture between Philips and Matsushita, Communication and Control Electronics Limited is an independent leading systems house dedicated to the design and development of in-car entertainment and information networks (known as D2B Optical). The company provides a total solution that encompasses system specifications, hardware and software, test, development tools and consultancy. Communication and Control Electronics Limited is headquartered in Guildford, UK and has an additional office in Germany.

For further information please contact:

Delphi Automotive Systems Paul E. Stefens
Tel: +32 3 633 05 11
Fax: +32 3 633 04 41
Mishaegen 132 B 2930 Brasschaat, Belgium Milton Beach Public Affairs
Tel: (765) 451- 0655
Fax: (765) 451-0659 P.O.
Box 9005 Kokomo, Indiana 46902 U.S.A.
Delphi can be found on the Internet at http://www.delphiauto.com. C&C Electronics Ab van de Water, Sales & Marketing Director. C&C Electronics. Tel. +44 1483 540 222 Fax. +44 1483 540 200 E-mail:helpdesk@candc.co.uk C&C can be found on the Internet at http://www.candc.co.uk


Should you require more information, please select the appropriate contact from the "Related Topics" menu.