Section
 

High-Voltage Power MOSFETs from STMicroelectronics Combine High Performance and Low Price

Highly rugged, first SuperMESH™ devices offer low RDS(on), high speed, and low cost

P1080C PHOTO Geneva, February 4, 2002 - STMicroelectronics (NYSE: STM)
has announced three high-voltage N-channel Power MOSFETs that combine exceptionally high efficiency and speed with ruggedness and low cost. Significantly, these are the first devices to be introduced using STMicroelectronics' SuperMESH technology, which complements the company's wide range of MOSFET technologies, including its highly advanced MDmesh™ family of devices.

The three MOSFETs are the STL5NK65Z, a 650V device having a typical on-resistance of 1,600 m ohm; the 600V STP13NK60Z, with a typical on-resistance of 480 m ohm; and the 500V STP14NK50Z, whose typical on-resistance is 340 m ohm. All three MOSFETs will find ready applications in off-line and switch-mode power supplies, adaptors, power factor correctors, lamp ballasts, and high-intensity discharge lamps.

SuperMESH technology is a highly optimized version of STMicroelectronics' basic strip-based Mesh Overlay™ process designed for high-volume applications. SuperMESH (NKxxZ-family) MOSFETs have better than 30% lower on-resistance (RDS(on)) than previous generation (NC-family) devices. For power equipment designers, the lower resistance allows the use of smaller and less costly heat sinks.

In addition, SuperMESH MOSFETs also benefit from a reduced VGS(th) spread from 2V to 1.5V that allow optimized driving control.

Yet another feature of the SuperMESH family is its built-in, back-to-back Zener diodes between the gate and source terminals. These Zener diodes improve resistance to destructive electrostatic discharges as well as protect the gate oxide against damage from spurious voltage spikes. Moreover, because they are built into the device, the Zener diodes preclude the need for external protection devices. The MOSFETs also feature excellent avalanche characteristics and are fully avalanche tested during manufacture.

Key Specifications for SuperMESH Devices

Part Number Drain-Source
Breakdown Voltage
(BVDSS)
On Resistance
(RDS(on))
Source-Drain Current,
(ISD)
STP13NK60Z 600V 480mOhm (typ) 13A
STP14NK50Z 500V 340mOhm (typ) 14A
STL5NK65Z 650V 1,600mOhm (typ) 5A

The STL5NK65Z is available in the new PowerFLAT™ packages, while STP13NK60Z, and STP14NK50Z are available in D2PAK, I2PAK, and TO-220 packages. Units are available now in volume quantities.

About STMicroelectronics
STMicroelectronics is the world's third largest independent semiconductor company. The Company shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. The Company designs, develops, manufactures and markets a broad range of semiconductor integrated circuits (ICs) and discrete devices used in a wide variety of microelectronic applications, including telecommunications systems, computer systems, consumer products, automotive products and industrial automation and control systems. In 2000, the Company's net revenues were $7,813.2 million and net earnings were $1,452.1 million. Further information on ST can be found at www.st.com


Should you require more information, please select the appropriate contact from the "Related Topics" menu.