Section
 

Step-up Converter from STMicroelectronics Simplifies LNB Control for Digital Satellite TVs

Integrated I2C bus eases control and diagnostics

LNBH21 (Click for Larger Image)Geneva, September 10, 2004 - STMicroelectronics (NYSE: STM)
has introduced a power supply and control IC for the low noise blockers (LNBs) used in set-top boxes and integrated digital televisions.

The LNBH21 includes a step-up voltage converter that works from a single input voltage of between 8V and 15V, simplifying system design. The converter is typically 94% efficient at a 750mA load.

The part also keeps the voltage drop on the internal linear regulator to a typical 2.2V, as compared with the 3.4V of previous models, reducing the power dissipation to 1.1W at 500mA load.

The part has an I2C interface and 22kHz tone signaling to provide a complete bi-directional interface between the LNB and the system that is controlling it. This further simplifies design and makes the part suitable for energy-saving digital set-top box designs.

The fast start-up of the oscillator enables DiSEqC encoding and the integrated tone detector supports bi-directional DiSEqC 2.0 signaling. Two output pins can be used to bypass any output filters, to avoid tone distortion.

The part is compliant with both the Eutelsat and DirecTV output specification and offers digital compensation for cable length.

The part also offers LNB short-circuit and over-temperature protection, with diagnostic bits presented to the I2C interface.

It supports two output currents, of 450mA and 750mA and has an ESD rating of 4KV on the power output pins.

US pricing is 1$US in quantities of 1K. Further information is available at www.st.com/vregs

About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2003, the Company's net revenues were $7.24 billion and net earnings were $253 million. Further information on ST can be found at www.st.com.

Should you require more information, please select the appropriate contact from the "Related Topics" menu.