|
STLC8201 simplifies design and cuts the cost of 802.11a/b/g
applications.
Geneva, June 8, 2004 - STMicroelectronics (NYSE:STM) today announced
the availability of its next generation STLC8201 multi-mode wireless
LAN baseband processor chip. The STLC8201, along with the previously
announced STLC8100 dual band wireless LAN RF transceiver, form the latest
STLC8000 series platform enabling an array of low cost IEEE802.11a/b/g
systems including wireless ADSL gateways, broadband routers, access
points, media servers, bridges, print servers as well as clients and
other wireless modules.
The STLC8201 wireless baseband processor combines the functions of a
media access controller (MAC) and physical layer processor. Using the
technique of Band Interleaving, the STLC8201 delivers low-cost dual
band operation for access point and infrastructure equipment. By dynamically
sharing available bandwidth between 2.4 and 5GHz clients, without the
need for duplicate baseband or RF circuits, STLC8201 systems seamlessly
adapt to support the client mix. Band Interleaving enables adoption
of 5GHz technology, which is key to avoiding looming channel overload
at 2.4GHz and removing the barriers to media-based applications.
Key features of the STLC8201 baseband include support for Quality of
Service (QoS) based upon the draft IEEE 802.11e standard, with support
for the Wi-Fi Alliances' Wireless Multimedia Extensions (WME). WME delivers
interoperable QoS for emerging voice and media-based applications.
v In addition, the STLC8201 offers uncompromised security. Built-in
hardware based encryption engines for WEP, Wi-Fi Protected Access (WPA),
Advanced Encryption System (AES), as well the latest WPA2 ensure no
loss of throughput.
Uncompromising speeds of up to 150 megabit per second (Mbit/s) data
throughput for wireless networking products allow for voice, data and
video transmission in any application. This accelerated throughput is
accomplished through enhanced standards-based software capabilities
and other enhancements, allowing the 8000 series platform users to easily
shift into turbo mode. With the addition of Quality of Service (QoS)
techniques, customers are assured the highest performing multi-mode
solution on the market, enabling seamless mobility, connectivity and
broad compatibility.
"We believe that low cost dual band a/b/g systems or modules are the
next natural and logical evolution for today's b/g products," said Giacomo
Piccini, Vice President of ST's Networking Division. "By selecting the
8000 series platform, ODM and OEM designers can quickly bring to market
low cost, high performance dual band wireless products to market that
fit the needs of next generation products."
The 8000 series platform is supplemented with a comprehensive software
suite that includes station and access point firmware; Windows, and
Linux drivers; engineering test functions; client GUI; and access point
management entity. In addition, to further assist developers in quickly
bringing to market products based on the platform to market quickly,
ST offers manufacturing ready reference designs for dual and single
band applications, including clients and access points.
The STLC8201 dual band wireless LAN baseband processor comes in a 256-pin
ball grid array package and sells for $8.00 each in quantities of 10,000.
Samples are available now, with production volumes scheduled for August.
About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering
semiconductor solutions across the spectrum of microelectronics applications.
An unrivalled combination of silicon and system expertise, manufacturing
strength, Intellectual Property (IP) portfolio and strategic partners
positions the Company at the forefront of System-on-Chip (SoC) technology
and its products play a key role in enabling today's convergence markets.
The Company's shares are traded on the New York Stock Exchange, on Euronext
Paris and on the Milan Stock Exchange. In 2003, the Company's net revenues
were $7.24 billion and net earnings were $253 million. Further information
on ST can be found at www.st.com.
|