How to calculate the demagnetization energy by using the datasheet indication (Vdemag)
How to choose the proper HSD in comparison to its demagnetization energy capability (an example based on VN820)
How to protect an HIGH SIDE DRIVER in the event of reverse polarity when driving resistive or inductive loads
How to detect an OPENLOAD fault
How to detect the OPENLOAD fault if the HIGH SIDE DRIVER is in ON STATE
How to detect the OPENLOAD fault if the HIGH SIDE DRIVER is in OFF STATE
How to choose the pull-up REXT resistor used in the OPENLOAD OFF state detection
Can I apply a 5V (TTL input) signal to INPUT pin to drive the HIGH SIDE DRIVER?
How can I drive an inductive load?
What is an HIGH SIDE DRIVER with current sense feature?
How to choose the sense resistor