![]() |
||
|
|
||
ST solutions for radio-frequency identification
|
||
|
Countless business applications, from product manufacturing to end-customer sales, can benefit from radio-frequency identification (RFID). With RFID, logistics becomes more effective, stock handling is easier, traceability is guaranteed, cloning and counterfeiting can be avoided, antitheft protection is enabled, and warranty problems can be easily eliminated.
DEFINITIONS What is radio frequency identification? RFID technology uses radio communications to uniquely identify items, such as goods, people, or animals. It enables automated collection of information on identified items independently from their position, without the need of a direct optical link or human intervention. RFID also frees the user from harsh or dirty environment concerns that restrict other automatic identification solutions such as barcode. In addition, RFID is used as a bidirectional data carrier, since it allows information attached to the item to be written and updated on the fly. What does an RFID system consist of? Contactless memory tags (transponders) are the backbone of the RFID system since they contain the data that identify the items. A contactless memory tag is made of a non-volatile memory associated with a radio-frequency communication block that performs RF signal modulation, demodulation, and power supply regulation, and an antenna. A transponder can be read-only (ROM), one-time-programmable (OTP), or read/write (EEPROM), and it can be embedded in various package formats (such as inlays, cards, and buttons). The reader (or reader station unit) is connected to the antenna that transmits and receives the radio-frequency signal to and from a transponder. The reader sends an RF signal to the transponder’s antenna. This signal generates a voltage that is rectified and provides a power source to the transponder. The power is transferred from the reader to the transponder through an inductive coupling between the two coils in 125 kHz and 13.56 MHz systems. For ultra-high frequencies (UHF), the electric field generated by the reader is used to power the tag. In other words, the transponder does not need a dedicated power supply. During the reader-transponder communication, the RF signal generated by the reader is modulated according to the data to be sent. In the transponder-reader direction, no modulation is applied on the reader RF signal and the communication is done through load modulation in inductive coupling systems. The reader interfaces with the RFID system control host through a serial interface such as RS232, RS422/485, or USB. TECHNICAL PRINCIPLES Unique identifier (also tag ID or TID) Chip identifier or chip_ID Application family identifier or AFI Anti-clone function (ACF) OPERATING RANGES AND APPLICATIONS The close-coupling range covers transponder-reader distances up to 5 cm. Brand protection, anti-counterfeiting of electronic goods and food consumables, as well as electronic purchases at vending machines operate in the close-coupling range. These applications employ low-cost readers operating with a limited number of transponders and require security features such as password, anti-clone, or cryptographic capabilities. RF systems are also a universal solution for various ticketing applications, no matter what means of transport (public transportation or private car) are used. Contactless systems can also be used in a wide range of access-control applications, including entrance systems to and within public buildings (offices), time and attendance systems, room logistics at hotels, locking systems, and amusement parks. These short-range or proximity-range applications use low-cost transponders embedded in plastic cards or paper tickets and they operate in the range up to 20 cm. Readers and transponders from different suppliers must be fully interoperable. Required security levels are satisfied through password, anti-clone, or cryptographic capabilities. These long-range or vicinity-range applications operate within one meter from the reader and typically involve a large number of low-cost transponders (100+), requiring reliable anti-collision mechanisms and transponder-reader interoperability. Extended or very long-range (up to 10 meters) RFID systems will be instrumental in creating low-cost contactless solutions for new supply chain, logistics, and tracking applications that can offer improved efficiency, accuracy, and security standards to major manufacturers, retailers, and their customers. ST offers ISO-standard and custom RFID products and helps its key customers to access and exploit the contactless application world. The Company’s current portfolio of contactless memories will be extended to match different target applications, in accordance with open standards. Committed to high-volume/low-cost identification solutions, ST offers low-cost, standard-compliant RFID chips and complete systems through its wide partner network (reader and converter makers, inlets makers). The Company has built strong relationships with key players in this field and developed a wide variety of RFID products for applications in retail, mass transit, vending machines and many others. ST's experience in the contactless domain, partnerships with system integrators, and strong involvement in standardization activities have enabled the Company to develop a highly cost-efficient, flexible, and interoperable portfolio of contactless identification products. For more information on ST’s offering in RFID visit www.st.com/rfid
|
|
|||||||||||||||||||
|