About ST
Products
Applications
Support
Buy
News & Events
ST Worldwide
Contact Us
Login
Application Notes
|
Smartcard interface with the STM32F101xx and STM32F103xx
Application Note
Format:
(443 kb)
or
(67 kb)
Last Updated: 30/05/2008
Pages: 40
Related Datasheets
Medium-density access line, ARM-based 32-bit MCU with 32 to 128 KB Flash, six timers, ADC and 7 communication interfaces
Medium-density performance line ARM-based 32-bit MCU with 32 to 128 KB Flash, USB, CAN, 7 timers, 2 ADCs, 9 communication interfaces
Related Information
Source file for Smartcard interface with STM32F10xxx
Raw Ascii Text
- (
Hide
)
(Unformatted textual content of the document used by search engines)
AN2598 Application note
Smar tcard interface with the STM32F101xx and STM32F103xx
Introduction
This document describes a firmware and hardware Smartcard interface solution based on the STM32F10xxx USART peripheral. The main purpose of this firmware and hardware package is to provide resources that facilitate the development of an application using the USART peripheral in Smartcard mode. The firmware interface consists of library source files developed so as to support the ISO 7816-3/4 specification. An application example based on STMicroelectronics STM3210B-EVAL and STM3210E-EVAL evaluation boards is also provided. This document and its associated firmware are available for download from the STMicroelectronics website: www.st.com.
Glossary
Medium-density devices are STM32F101xx and STM32F103xx microcontrollers where the Flash memory density ranges between 32 and 128 Kbytes. Medium-density devices are implemented in the STMicroelectronics STM3210B-EVAL evaluation board. High-density devices are STM32F101xx and STM32F103xx microcontrollers where the Flash memory density ranges between 256 and 512 Kbytes. High-density devices are implemented in the STMicroelectronics STM3210E-EVAL evaluation board.
May 2008
Rev 2
1/40
www.st.com
Contents
AN2598
Contents
1 Smartcard interface description . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
1.1 1.2 1.3 1.4 Introduction . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 External interface . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 Protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 Smar tcard clock generator . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7
2 3
Smartcard reader hardware connection . . . . . . . . . . . . . . . . . . . . . . . . . 8 ISO 7816: protocol overview . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10
3.1 3.2 Introduction . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10 ISO 7816-2 pin location . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10
4
ISO 7816-3 Electronic signal and transmission protocol . . . . . . . . . 12
4.1 4.2 4.3 Card power-up and reset . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13 Data transfer . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14 Answer to reset (ATR) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
5
ISO 7816-4 Smartcard commands . . . . . . . . . . . . . . . . . . . . . . . . . . . 17
5.1 5.2 T0 protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 17 Application-level protocols . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19
5.2.1 5.2.2 5.2.3 5.2.4 The ISO 7816-4 APDU . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20 File system API . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 21 ISO 7816-4 functions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 22 Security API . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 23
6
Smartcard interface library: description . . . . . . . . . . . . . . . . . . . . . . . . 25
6.1 6.2 File organization . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 Smar tcard interface library functions . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25
6.2.1 6.2.2 6.2.3 6.2.4 6.2.5 SC_Handler function . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 SC_PowerCmd . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 SC_Reset . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 SC_ParityErrorHandler . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 30 SC_PTSConfig . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 30
2/40
AN2598
Contents
6.3
How to send APDU commands to the Smartcard . . . . . . . . . . . . . . . . . . 30
6.3.1 6.3.2 6.3.3 6.3.4 6.3.5 6.3.6 6.3.7 SC_GET_A2R . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 31 SELECT_FILE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 31 SC_GET_RESPONSE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 31 SC_READ_BINARY . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 32 SC_CREATE_FILE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 32 SC_UPDATE_BINARY . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 33 SC_VERIFY . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 33
6.4
Parity error management . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 34
6.4.1 6.4.2 Data sent from card to reader . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 34 Data sent from reader to card . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 34
7
Smartcard interface example . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 35
7.1 Firmware package description . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 35
7.1.1 7.1.2 FWLib folder . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 35 Smar tcard_AN folder . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 35
7.2
Firmware description . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 35
7.2.1 7.2.2 7.2.3 7.2.4 Smar tcard startup: answer to reset (A2R) . . . . . . . . . . . . . . . . . . . . . . . 36 Reading a file at a specified path . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 36 Enabling/disabling the PIN1 (CHV1) code . . . . . . . . . . . . . . . . . . . . . . . 37 Verifying the PIN1 (CHV1) code . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 37
8 9
Conclusion . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 38 Revision history . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 39
3/40
List of tables
AN2598
List of tables
Table 1. Table 2. Table 3. Table 4. Table 5. Table 6. Table 7. Table 8. Table 9. Table 10. Table 11. Table 12. Table 13. Table 14. Table 15. Smartcard pins . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 STM32F10xxx and Smartcard connection . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 8 Pin assignment . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11 Answer-to-reset structure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16 CLA instruction set definitions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18 ISO 7816-4 INS codes . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18 File library description . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 Smartcard library functions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 SC_Handler . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 SCState . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26 SC_PowerCmd . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 SC_Reset . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 SC_ParityErrorHandler . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 30 SC_PTSConfig . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 30 Document revision history . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 39
4/40
AN2598
List of figures
List of figures
Figure 1. Figure 2. Figure 3. Figure 4. Figure 5. Figure 6. Figure 7. Figure 8. Figure 9. Figure 10. Figure 11. ISO 7816-3 asynchronous protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 Smartcard interface hardware connection . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9 Contact definitions for Smartcards . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10 Reader and card FSM . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12 Answer to reset . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13 Application communication architecture . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19 Command APDU structure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20 Response APDU structure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20 Smartcard file system architecture(1) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 21 State machine for smartcard operation. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27 Smartcard example: file system description . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 36
5/40
Smartcard interface description
AN2598
1
1.1
Smartcard interface description
Introduction
The Smartcard interface is developed using the USART Smartcard mode. For the description of the USART registers, please refer to the STM32F10xxx reference manual. The USART Smartcard mode supports asynchronous protocol Smartcards as defined in the ISO 7816-3 standard. With the Smartcard mode enabled, the USART must be configured as:
eight data bits plus parity 0.5 or 1.5 stop bits
A 5-bit prescaler and the Smartcard clock generator provide the clock to the Smartcard. GPIO pins in conjunction with software are used to provide the rest of the functions required to interface to the Smartcard. The inverse signalling convention as defined in ISO 7816-3, inverted data and MSB first, is not handled in the software.
1.2
External interface
Table 1. Smartcard pins
Smartcard pin CLK IO RST VC C VPP Function Smar tcard clock IO serial data: open drain Reset to card Supply voltage Programming voltage STM32F10xxx pin USART CK USART_TX Any GPIO Any GPIO Any GPIO
The Smartcard_RST (Smartcard reset), Smartcard_3/5V (3 V or 5 V), Smartcard_CMDVCC (command for VCC), and Smartcard_OFF signals (signal for card detection) are provided by GPIO bits of the I/O ports under software control. Programming the GPIO bits of the port for alternate function open-drain mode connects the USART_TX data signal to the Smartcard_IO pin with the correct driver type and the clock generator to the Smartcard_CLK pin configured in alternate function output push-pull.
1.3
Protocol
The ISO 7816-3 standard defines the bit times for the asynchronous protocol in terms of time units called ETUs (elementary time units), that are related to the clock frequency input to the card. The length of an ETU is a bit time. The USART transmitter output and receiver input are internally connected through the Rx_SW line. For the transmission of data from the STM32F10xxx to the Smartcard, the USART must be set up in Smartcard mode.
6/40
AN2598 Figure 1. ISO 7816-3 asynchronous protocol
Smartcard interface description
Line pulled low by receiver during stop in case of parity error
S Star t bit
a
b
c
d
e
f
g
h
P Parity ETU bit
ai14612
8 data bits
1.4
Smartcard clock generator
The Smartcard clock generator provides a clock signal to the connected Smartcard. The Smartcard uses this clock to derive the baud rate clock for the serial I/O between the Smartcard and another USART. The clock is also used for the CPU in the card, if present. Operation of the Smartcard interface requires that the clock rate to the card is adjusted while the CPU in the card is running code so that the baud rate can be changed or the performance of the card can be increased. The protocols that govern the negotiation of these clock rates and the altering of the clock rate are detailed in the ISO 7816-3 standard. The clock is used as the CPU clock for the Smartcard, therefore updates to the microcontroller clock rate must be synchronized to the Smartcard clock, that is the clock high or low pulse widths must not be shorter than either the old or new programmed value.
7/40
Smartcard reader hardware connection
AN2598
2
Smartcard reader hardware connection
To interface to the Smartcard, the ST8024 device was used. The ST8024 is a complete lowcost, analog interface for asynchronous 3 V and 5 V Smartcards. It is placed between the Smartcard and the STM32F10xxx with few external components to perform all supply protection and control functions. Table 2. STM32F10xxx and Smartcard connection
STM3210E-EVAL Smartcard pins Function Smar tcard clock: alternate function pushpull IO serial data: alternate function open drain Reset to card: output push-pull Supply voltage: output push-pull Smar tcard detect: input floating 3 V or 5 V: output push-pull
STM3210B-EVAL
USART3 CK: PB12 USART3 CK: PB12 C3: CLK USART3_TX: PB10 USART3_TX: PB10 C7: IO PB.11 PE.07 PE.14 PD.11 PB.11 PC.06 PC.07 PB.00 C2: RST C1: VCC OFF 3/5V
8/40
AN2598 Figure 2.
Smartcard reader hardware connection Smartcard interface hardware connection
9/40
ISO 7816: protocol overview
AN2598
3
3.1
ISO 7816: protocol overview
Introduction
"ISO 7816: Identification cards -- Integrated circuit(s) cards with contacts" provides the basis to transition the relatively simple identification card from a token that can be compromised through forgery, theft, or loss into a tamper-resistant and "intelligent" integrated circuit card (ICC), more popularly known as a Smartcard. ISO 7816 includes at least six approved parts and has several additional parts under review:
Par t 1: Physical characteristics Par t 2: Dimensions and location of the contacts Par t 3: Electrical interface and transmission protocols Par t 3: Amendment 2-Revision of protocol type selection Par t 4: Organization, security and commands for interchange Par t 5: Registration of application providers
3.2
ISO 7816-2 pin location
ISO 7816-2 specifies an ICC with eight electrical contacts present in a standardized position on the front face of the card. These are referred to as C1 through C8. Some of these contacts are electrically connected to the microprocessor chip embedded within the card; some are not, having been defined to allow for enhancements but unused at the present time. Figure 3 shows the contact positions. Figure 3. Contact definitions for Smartcards
ISO 7816-2 Governs the dimension and location of the chip contacts
1-VCC 2-RST 3-CLK 4-RFU
GND-5 VPP-6 I/O-7 RFU-8
Only one location accepted by ISO since 1/1/93. Chip can still be on the front or back of the card.
ai14617
10/40
AN2598 Table 3. Pin assignment
Pins C1 C2 C3 C4 C5 C6 C7 C8
ISO 7816: protocol overview
Functions VCC = 5 V or 3.3 V Reset Clock RFU GND VPP I/O RFU
11/40
ISO 7816-3 Electronic signal and transmission protocol
AN2598
4
ISO 7816-3 Electronic signal and transmission protocol
ISO 7816-3 begins to delve into the specification of the "intelligent" aspects of the Smartcard. This standard describes the relationship between the Smartcard and the reader as one of "slave" (the Smartcard) and "master" (the reader). Communications are established by the reader signaling to the Smartcard through the contacts noted previously and are continued by the Smartcard responding accordingly. Communication between the card and reader proceed according to various state transitions illustrated in Figure 4. Figure 4. Reader and card FSM
Reader state diagram Card removal
Ca
Card state diagram
Reader "idle"
rd
ins
er t
ion
Power off
Ca
rd
res
et
Protocol fail Card removal
No
AT R
Power the cord
ue
Prepare ATR
R AT
R AT ive Protocol ce negotiation Re
APDU dispatch idle Issue response to reader
Iss
Set protocol
Se AP Idle DU to command ca rd Re cei res ve po ful Wait for nse l response and mm t coetion s que pl nse Re com spo l re r tia Pa Command completion wait nd
Dispatch APDU to processor
APDU processing
ai14618
The communication channel is single-threaded; once the reader sends a command to the Smartcard, it blocks until a response is received.
12/40
AN2598
ISO 7816-3 Electronic signal and transmission protocol
4.1
Card power-up and reset
When a card is inserted into a reader, no power is applied to any of the contacts. The chip on the card could be seriously damaged by applying power to the wrong contacts, and this situation could easily occur if a card were inserted across powered contact points. The contacts remain unpowered until an edge detector determines that the card is properly aligned with the contact points to within some acceptable (for the reader) mechanical tolerance. When the reader detects that the card is properly inserted, power is applied to the card. First, the contacts are brought to a coherent idle state, as shown in Table 3. A reset signal is then sent to the card via the RST contact line. The idle state occurs when the power (VCC) contact is brought up to a normal, stable operating voltage of 5 V. An initial power setting of 5 V is always applied first, even though some microprocessor chips being introduced operate at 3 V when in an I/O state. The I/O contact is set to a reception mode on the reader side and a stable clock (CLK) is applied. The reset line is in a low state. It must remain in a low state for at least 40 000 CLK cycles before a valid reset sequence can be started by the reader, raising the reset line to a high state. Figure 5. Answer to reset
Contacts properly positioned Card inser ted GND T0
VCC
CLK
t3(1)
RST ATR must come from card here(2) I/O Reader not listening Reader listening
ai14619
1. t3 = 40 000 clock cycles. 2. ATR must be issued by card between 400 clock cycles and 40 000 clock cycles after RST goes high.
13/40
ISO 7816-3 Electronic signal and transmission protocol
AN2598
4.2
Data transfer
Data transfer between the reader and the card occurs through the concerted action of two of the contact lines: CLK and I/O. The I/O line conveys a single bit of information per unit of time as defined by the CLK depending on its voltage relative to GND. A 1 bit can be conveyed either through a +5 V value or through a 0 V value. The actual convention used is determined by the card and is conveyed to the reader through the "initial character" of the ATR, which is referenced as TS. To transfer 1 byte of information, 10 bits are actually moved across the I/O line; the first is always a "start bit" and the last is always a parity bit used to convey even parity. Considering that the I/O line can be (in one bit period) either in a high (H) state or a low (L) state, the TS character of the form HLHHLLLLLLH signals that the card wants to use the "inverse convention," meaning that H corresponds to a 0 and L corresponds to a 1. A TS character of the form HLHHLHHHLLH signals that the card wants to use the "direct convention," meaning that H corresponds to a 1 and L corresponds to a 0. The direct convention and the inverse convention also control the bit ordering with each byte transferred between the card and the reader. In the direct convention, the first bit following the start bit is the low-order bit of the byte. Successively higher-order bits follow in sequence. In the inverse convention, the first bit following the start bit is the high-order bit of the byte. Successively lower-order bits follow in sequence. Parity for each byte transferred should be even; this means that the total number of 1 bits in the byte, including the parity bit, must be an even number. The I/O line comprises a half-duplex channel; that is, either the card or the reader can transmit data over the same channel, but they both cannot be transmitting at the same time. So as part of the power-up sequence, both the reader and the card enter a receive state in which they are listening to the I/O line. With the start of the reset operation, the reader remains in the receive state while the card must enter a send state in order to send the ATR back to the reader. From this point on, the two ends of the channel alternate between send states and receive states. With a half-duplex channel, there is no reliable way for either end to asynchronously change a state from send to receive or from receive to send. Rather, if this is desired, that end must go into a receive state and allow a timeout of the operation in progress; then a reader end will always try to re-establish a known sequence by re-entering a send state. The CLK and I/O lines can support a wide variety of data transmission speeds. The specific speed is defined by the card and is conveyed back to the reader through an optional character in the ATR. The transmission speed is set through the establishment of one bit time on the I/O line, which means that an interval is established at which the I/O line may be sampled in order to read a bit and then each successive bit. This time is defined as an elementary time unit (ETU) and is established through a linear relationship between several factors. Note that the TS character is returned before any definition of the ETU can be made. This is possible because the ETU during the ATR sequence is always specified to be ETU0=372/(CLK frequency) where the CLK frequency is always between 1 MHz and 5 MHz; in fact, the frequency is almost always selected such that the initial data transfer rate is 9,600 bits per second.
14/40
AN2598
ISO 7816-3 Electronic signal and transmission protocol
4.3
Answer to reset (ATR)
Once an RST signal is sent from the reader to the card, the card must respond with the first character of the ATR within 40 000 CLK cycles. The card might not respond with an ATR for a number of reasons, the most prevalent being that the card is inserted incorrectly into the reader (probably upside down). In some instances, the card may not be functioning because it has been damaged or broken. Whatever the case, if the ATR is not returned within the prescribed time, the reader should begin a sequence to power down the card. During this sequence, the reader sets the RST, CLK, and I/O lines low and drops voltage on the VCC line to nominal 0 (that is, less than 0.4 V). The ATR is a string of characters returned from the card to the reader following the successful completion of the power-up sequence. As defined in ISO/IEC 7816-3, the ATR consists of 33 or fewer characters comprising the following elements:
TS - a mandatory initial character T0 - a mandatory format character TAi TBi TCi TDi - optional interface characters T1, T2,TK - optional historical characters TCK - a conditional check character
The historical characters can be defined at the discretion of the card manufacturer or the card issuer. These characters are typically used to convey some type of designation of the type, model, and use of this specific card. When used in this way, the historical characters provide a mechanism through which systems can automatically detect the use of an inserted card (within that system) and can initiate other actions (or software) accordingly. The check character provides a mechanism through which the integrity of the ATR can be measured; that is, whether a transmission error has occurred in sending the characters from the card to the reader. The structure of the ATR is illustrated in Table 4. As discussed previously, the initial TS character is used to establish the bit-signaling and bit-ordering conventions between the reader and the card. The T0 character is used to signal the presence or absence of subsequent interface characters or historical characters. The interface characters are used to tailor the characteristics of the I/O channel, including the specific protocol used by the card and reader during subsequent exchange of commands (from the reader to the card) and responses (from the card to the reader). The historical characters, if present, are used to convey card-manufacturer-specific information from the card to the read, and hence to the application system being served by the reader. There is really no established standard for the information presented in the historical bits.
15/40
ISO 7816-3 Electronic signal and transmission protocol
AN2598
The total length of the ATR sequence is limited to 33 bytes and must adhere to the following format: Table 4. Answer-to-reset structure
Character ID Initial character section Format character section TS T0 TA1 TB1 TC1 TD1 TA2 Interface character section TB2 TC2 TD2 TA3 ..TDi T1 Historical character section Check character section ...TKi TCK Definition Mandatory initial character Indicator for presence of interface characters Global, codes F1 and D1 Global, codes 11 and Pl1 Global, code N Codes Y2 and T Specific Global, code Pl2 Specific Codes Y3 and T TAi, TBi and TCi are specific Codes Yi+1 and T Card specific information (Maximum of 15 characters) Optional check character
16/40
AN2598
ISO 7816-4 Smartcard commands
5
ISO 7816-4 Smartcard commands
The previous chapter discussed the answer-to-reset (ATR) mechanism, which establishes a basic communication channel between the Smartcard and the reader. This channel is a halfduplex physical channel. This chapter investigates the use of more complex protocols on top of this physical channel. A link-level communication protocol resides directly on top of the physical channel, providing error-free communication between the reader and the Smartcard. Once this link-level protocol is established, application-level protocols can be defined. ISO 7816-4 defines two such application-level protocols:
File system API providing a set of functions to manipulate files (for example read, write, select, etc.). Security service API allowing the Smartcard and the reader to mutually authenticate themselves and also to encrypt data to be exchanged between the card and the reader.
ISO 7816-4 defines a protocol message structure to support the application protocol APIs. This message structure consists of application protocol data units (APDUs) which are exchanged between the reader application and the Smartcard application by the link-level protocol. This chapter will provide an overview of the file access and security APIs.
5.1
T0 protocol
The T0 protocol is a byte-oriented protocol where a character is transmitted across the channel between the reader and the card. In addition, error handling is performed on each byte by looking at the parity bit. If the actual parity bit does not correspond to the parity of the transmitted data, then an error must have occurred. In the T0 protocol, the receiving side signals that it requires the byte to be retransmitted in the case of detecting a parity error. This is done by holding the I/O line low (normally the I/O line is set high preceding the transfer of a byte). When the transmitting side detects this, it resends the byte that was not received correctly. The reader and the Smartcard exchange data structures known as transmission protocol data units (TPDUs). It consists of two distinct structures:
a command that is sent from the reader to the card a response that is sent from the card to the reader CLA: class designation of the command set to establish a collection of instructions INS: specifies a specific instruction from within the set of instructions P1: used to specify the addressing used by the [CLA, INS] instruction P2: also used to specify the addressing used by the [CLA, INS] instruction P3: specifies the number of data bytes transferred to or from the card as part of the [CLA, INS] instruction execution.
The command header includes the following five fields each of one byte in length:
Each value of CLA defines an application-specific set of instructions. Table 5. below lists values for some sets of instructions.
17/40
ISO 7816-4 Smartcard commands Table 5. CLA instruction set definitions
CLA byte 0x 10 to 7F 8x or 9x Ax B0 to CF D0 to FE FF Instruction set ISO 7816-4 instructions (files and security) Reserved for future use ISO 7816-4 instructions Application/vendor specific instructions ISO 7816-4 instructions Application/vendor specific instructions Reserved for protocol type selection
AN2598
The INS byte is used to identify a specific instruction within a class of instructions identified by the value of CLA.Table 6. lists the instructions in the ISO 7816-4 standard used to access file system and security functions. Table 6. ISO 7816-4 INS codes
Command name Erase Binary Verify Manage Channel External Authenticate Get Challenge Internal Authenticate Select File Read Binary Read Record(s) C0 C2 CA D0 D2 D6 DA DC E2 INS value Command name Get Response Envelope Get Data Write Binary Write Record Update Binary Put Data Update Record Append Record
INS value 0E 20 70 82 84 88 A4 B0 B2
The parameters P1 and P2 are defined at the link level but are actually dependent on the specific instruction (application level). They provide control or addressing parameters for the various application-specific instructions. For example, in the Select File instruction, P1 is used to indicate how the file will be referred to (by identifier, name, path etc.) and P2 offers further refinement as to which file is to be selected. P3 defines the number of bytes to be transmitted during the execution of the INS specified instruction. The convention used to indicate movement of data is card-centric that is, outgoing refers to data moving from the card to the reader and incoming refers to data moving from the reader to the card. For each command TDPU sent from the reader, a response TPDU is sent by the card. The response includes three mandatory fields and one optional field (all one byte in length):
ACK: indicates that the card has received the [CLA, INS] command NULL: used for flow control on the I/O channel by the card. It signals (to the reader) that the card is still processing the command and so the reader must wait before sending another command SW1: status response of the current command SW2: (optional) also conveys a status response to the reader
18/40
AN2598
ISO 7816-4 Smartcard commands The ACK byte is a repeat of the INS byte from the command TPDU. If the response does not reach the reader within a specified time, the reader may initiate an RST sequence to restart the protocol between the reader and the card. This can be prevented if the reader receives at least one NULL byte from the card. SW1 informs the reader of the result of the requested instruction. The values allowed for SW1 are defined as part of the application protocol. Some instructions require the card to send data to the reader. In this case SW2 is returned to the reader, triggering the reader to execute a GetResponse command. The card will then return the data bytes generated by the execution of the previous command.
5.2
Application-level protocols
The ISO 7816-4 standard addresses two areas of functionality for application software:
File system: a set of functions is provided in the form of an API. By using this API application software on the reader side can access files in the file system. Security functions: these can be used to limit access to application software or to files on the card.
The T0 protocol is used to support application-level protocols between the Smartcard application and the reader application. These application protocols exchange data structures called application protocol data units (APDUs). The following diagram illustrates this architecture: Figure 6. Application communication architecture
Application APDU Reader Response Command T0 or T1 link protocol Response Card APDU Response APDU processor
Specific functions, e.g. Select File, Read file, etc.
ai14620
The APDU structure defined by ISO 7816-4 is very similar to the TPDU structure used in the T0 protocol. In fact, when an APDU is transported by the T0 protocol, the elements of the APDU directly overlay the elements of the TPDU.
19/40
ISO 7816-4 Smartcard commands
AN2598
5.2.1
The ISO 7816-4 APDU
There are two types of messages used to support the ISO 7816-4 application protocols: the command APDU (sent from the reader to the card) and the response APDU (sent from the card to the reader). Figure 7. Command APDU structure
Header Body
CLA
INS
P1
P2
Lc field
Data field
Le field
ai14621
The command APDU consists of a header and a body (this can be seen in the diagram above). The header includes CLA, INS, P1 and P2 fields. As in the T0 protocol, CLA and INS specify an application class and instruction. P1 and P2 are used to qualify specific instructions and are given specific definitions by each [CLA, INS] instruction. The body of the APDU can vary in size and is used to transmit data to the card's APDU processor as part of a command or to convey a response from the card to the reader. The Lc field specifies the number of bytes to be transmitted to the card as part of the instruction, that is, the length of the data field. The data field contains information that must be sent to the card to allow its APDU processor to execute the command specified in the APDU. The Le field specifies the number of bytes that will be returned to the reader in the response APDU. The body of the APDU can take on four different forms:
Case 1: No data is transferred to or from the card, so the APDU only contains the header. Case 2: No data is transferred to the card, but data is returned from the card. The body of the APDU only contains a non-null Le field. Case 3: Data is transferred to the card, but none is returned from it. The body of the APDU includes the Lc and data fields. Case 4: Data is transferred to the card and is also returned from the card as a result of the command. The body of the APDU includes the Lc, data and Le fields. Response APDU structure
Body Trailer
Figure 8.
Data field
SW1
SW2
ai14622
The response APDU has a much simpler structure than that of the command APDU. It consists of a body and a trailer. The body is either null or it includes a data field - depending on the specific command. The length of the data field is determined by the Le field in the corresponding command APDU. The trailer consists of up to two fields of status information called SW1 and SW2. These fields return a status code in which one byte is used to specify
20/40
AN2598
ISO 7816-4 Smartcard commands an error category and the other is used to specify a command-specific status or error indication.
5.2.2
File system API
The file system is used on the non-volatile memory or EEPROM. It is defined as a simple hierarchical structure (similar to conventional file systems). The file system may contain three types of files (identified by a 2-byte identifier):
Master file (MF) Dedicated file (DF) Elementary file (EF)
There is one master file found on each Smartcard and it is the root of the file system. A master file may contain dedicated files or elementary files. The file identifier reserved for the master file is 3F00. The directory file is essentially a container (or directory) for elementary files - a DF may contain zero or more EFs. Dedicated files partition the Smartcard into an ordered structure of elementary files. A dedicated file must be given a unique file identifier within the dedicated file or master file that contains it - allowing for a unique path for each file. A dedicated file can also be referenced by name (1-16 bytes long). The naming convention can be found in ISO 7816-5. An elementary file is a leaf node in the hierarchy and contains the actual data. An elementary file can be identified by a 5-bit identifier within a dedicated file. This file system hierarchy is illustrated in Figure 9. Figure 9. Smartcard file system architecture(1)
MF
EF
DF
EF
EF
EF
DF
EF
DF
ai14623
1. MF = master file, DF = dedicated file, EF = elementary file.
There are four types of elementary files:
Transparent file Linear, fixed-length record file Linear, variable-length record file Cyclic, fixed-length record file
A transparent file is essentially a string of bytes, that is an unstructured binary file. Consequently a byte offset from the start of the file is required when data is to be read or written to this type of file. In addition, a command to read or write to a transparent file will contain the length of the byte string to be read or written to the file. Fixed- and variable-length files contain records that are identified by a sequence number. In a fixed-length record file, all the records contain the same number of bytes. In contrast, a
21/40
ISO 7816-4 Smartcard commands
AN2598
variable-length record file contains records that may vary in length. As a result, variablelength record files have a higher overhead in read/write access times as well as a higher administrative overhead required by the file system. A cyclic file allows applications to access records in a consistent and transparent manner. It can be thought of as a ring of files. Write operations are performed on the next physical record in the ring.
5.2.3
ISO 7816-4 functions
The few functions that are defined in ISO 7816-4 for selecting, reading and writing to files will be briefly discussed below.
Select File
This command establishes a logical pointer to a particular file in the Smartcard's file system. This pointer is required for any file manipulation operation. Access to the Smartcard's file system is not multithreaded, however it is possible to have several file pointers defined at any point in time. This is accomplished by the Manage Channel command, which establishes multiple logical channels between the reader side application and the card. This allows different files on the card to be in various states of access by the reader application at the same time. The identification of the file can be provided in the following ways:
file identifier (2-byte value) DF name (string of bytes) path (concatenation of file identifiers) shor t ID
Note that not all Smartcards support all four naming mechanisms.
Read Binary
This command is used by the application on the reader side to retrieve a part of an EF on the card. However, the EF must be a transparent file (not record-oriented). If the Read Binary command is attempted on a record-oriented EF, the command will abort with an error indicator being returned from the card. The Read Binary command takes two parameters: an offset pointer from the start of the file to the initial byte to be read, and the number of bytes to be read and returned to the reader.
Write Binary
This command is used to insert data into a transparent EF on the card. This command can be used to set a series of bytes in the EF (that is set selected bits within a specified byte to a value of1), clear a series of bytes or perform a write of a series of bytes in the EF.
Update Binary
A reader-side application can utilize this command to directly erase and store a contiguous sequence of bytes in a transparent EF on the card. It effectively functions as a write command that is a string of bytes provided in the command are written into the EF on the card. The input parameters consist of an offset pointer from the start of the file as well as the number of bytes to be written.
22/40
AN2598
ISO 7816-4 Smartcard commands
Erase Binary
The Erase Binary command is used to clear bytes within a transparent EF on a card. Similarly to the previous commands, the input parameters comprise an offset from the start of the EF to the segment of bytes to be erased as well as the number of bytes to be erased.
Read Record
This command is used to read and return the contents of one or more records in an EF on a card. Unlike the previous command, the EF for the Read Record command must be a record-oriented file. If it is applied to a transparent EF, the command will abort and an error will be returned to the reader. The following may be returned from this command, depending on the input parameters:
A specified record All the records from the beginning of the file to a specific record All the records from a specific record to the end of the file
Write Record
This command is used to write a record into a record-oriented EF. As with the Write Binary command, this command can be used to write a record into an EF, set or clear specific bits within a specific record in an EF.
Append Record
The Append Record command is used to add a record to the end of a linear, record-oriented EF or to write the first record to a cyclic, record-oriented EF on a card.
Update Record
This command writes a specific record into a record-oriented EF on a card. As with the Update Binary command, the old record is erased and the new one is written into the EF.
Get Data
This command reads and returns the contents of a data object stored within the file system on the card. The Get Data command is card-specific as the definition of a data object varies between different cards.
Put Data
This command (as the name suggests) puts information into a data object on the card. As with the previous command, this is a card-specific command.
5.2.4
Security API
Each component of the file system on a Smartcard has an associated list of access properties. The access properties ensure that only authorized parties are allowed to access the particular component of the file system. The authentication can be simple, such as requiring the reader to provide a predefined personal identification number (PIN). Alternatively, it may be more complicated, such as requiring the reader to prove that it possesses some shared secret with the card (for example a key) by encrypting or decrypting a string of bytes provided by the card. A few of the functions provided by the security API are briefly discussed below.
23/40
ISO 7816-4 Smartcard commands
AN2598
Verify
This command is sent by the application on the reader side to the security system on the card. Its purpose is to convince the card that the reader knows a password maintained by the card in order to restrict access to sensitive information stored on the card. The password-type information may be associated with a specific file or to some or all of the file hierarchy. If the Verify command fails i.e. the reader provides an incorrect password, an error is returned to the reader.
Internal Authenticate
This command allows the card to authenticate itself to the reader by proving that it possesses a secret key shared with the reader. The reader application software first generates a random number and encrypts it with some algorithm known to both card and reader. This constitutes a challenge to the card. The card then decrypts this challenge with the secret key (that is stored on the card) and sends the resulting data back to the reader. If the data received by the reader matches the random number that it generated then the reader application software is assured of the identity of the card.
External Authenticate
This command is used in conjunction with the Get Challenge command to enable the reader application software to authenticate itself to the card. The reader receives challenge data (a random number) from the card and encrypts it with a secret key. This is then sent to the card using the External Authenticate command. The card decrypts the data and compares it to the random number that it generated in the previous Get Challenge command. If there is a match, then the card is assured of the identity of the reader application.
Get Challenge
This command is sent by the reader to the card. Its purpose is to provide the reader application with a random number generated by the Smartcard. As previously described, this number is used in the External Authenticate command.
Manage Channel
The Manage Channel command is used by the reader application to open and close the logical communication channels between it and the card. Initially the card opens a basic communication channel by establishing an application-level protocol with the reader application through the completion of an ATR sequence. This channel is then used to open or close additional logical channels through the Manage Channel command.
Envelope
This command supports the use of secure messaging using the T0 protocol. It enables an APDU to be encrypted and then incorporated into the Envelope command's data section (of its APDU). The APDU processor on the card can then extract and execute the command.
Get Response
As with the previous command, the Get Response command allows the use of the T0 protocol for transferring APDUs. The Case 4 type of APDU cannot be supported by the T0 protocol i.e. it is not possible to send a block of data to the card and then receive a block of data in return. So when using the T0 protocol, the initial command results in a response which indicates that more data is waiting to be sent by the card. The Get Response command is then used to retrieve this data.
24/40
AN2598
Smartcard interface library: description
6
Smartcard interface library: description
The user may access a Smartcard using directly the application layer. It allows to send/receive ADPU commands to/from the Smartcard using the following user interface:
6.1
File organization
Table 7 presents the Smartcard library modules: Table 7. File library description
File Description
Smar tcard definitions, types definitions and function prototypes smar tcard.h, smartcard.c T0 protocol management Physical layer
6.2
Smartcard interface library functions
Table 15 lists the various functions of the Smartcard library. Table 8. Smartcard library functions
Description Handles all Smartcard states and serves to send and receive all communication data between Smartcard and reader. Enables or disables the power to the Smartcard. Sets or clears the Smartcard reset pin. Resends the byte that failed to be received (by the Smartcard) correctly. Configures the IO speed (BaudRate) communication.
Function name SC_Handler SC_PowerCmd SC_Reset SC_ParityErrorHandler SC_PTSConfig
6.2.1
SC_Handler function
It is described in Table 9. Table 9. SC_Handler
SC_Handler
void SC_Handler(SC_State *SCState, SC_ADPU_Commands *SC_ADPU, SC_ADPU_Responce *SC_Response)
Function name Function prototype Behavior description Input parameter1 Input parameter2
Handles all Smartcard states and serves to send and receive all communication data between Smartcard and reader. SCState: pointer to an SC_State enumeration that will contain the Smartcard state. SC_ADPU: pointer to an SC_ADPU_Commands structure that will be initialized.
25/40
Smartcard interface library: description Table 9. SC_Handler (continued)
SC_Handler
A N25 9 8
Function name Input parameter3 Output parameter Return parameter Required preconditions Called functions
SC_Response: pointer to a SC_ADPU_Responce structure which will be initialized. None None None None
SCState
SCState informs the user about the Smartcard state and allows the user to power off the Smartcard. It can assume one of the values defined in Table 10 below. Table 10. SCState
Meaning No power is provided to the Smartcard (VCC = 0); the STM32F10xxx Smartcard interface is disabled. No clock is provided to the Smartcard. The Smartcard peripheral is enabled and initialized; no power is provided to the Smartcard; no clock is provided to the Smartcard. In this state, the RST Smartcard pin (pin 2) is driven low (RST = 0). VCC = 5 V is provided to the Smartcard; clock CLK is provided to the Smartcard. Answer to reset (ATR) procedure begins. The reader waits for an ATR frame from the Smartcard. If no answer is received, the reader forces the reset pin RST high (RST = 1) and holds it high until it receives an answer to reset. If an answer to reset is received, the reader goes in active state and decodes the ATR frame. It returns information about the used protocol. If the used protocol is T0, the reader goes in SC_ACTIVE_ON_T0 state and commands can then be sent to the Smartcard.
SCState SC_POWER_OFF SC_POWER_ON
SC_RESET_LOW
SC_RESET_HIGH SC_ACTIVE SC_ACTIVE_ON_T0
26/40
AN2598
Smartcard interface library: description Figure 10. State machine for smartcard operation
Power off User forces power-up Power-up No ATR received Reset low ATR received with RST = 0 Active T0 protocol Active on T0
ai14624
No ATR received
Reset high
ATR received with RST = 1
SC_ADPU_Commands
The SC_APDU_Commands structure is defined in the smartcard.h file:
typedef struct { SC_Header Header; SC_Body Body; } SC_ADPU_Commands;
Header Specifies the APDU command header. It is of the SC_Header type, which is defined in the smartcard.h file:
typedef struct { u8 CLA; /* Command class */ u8 INS; /* Operation code */ u8 P1; /* Selection Mode */ u8 P2; /* Selection Option */ } SC_Header;
CLA Specifies the class designation of the command set to establish a collection of instructions.
INS Specifies a specific instruction from within the set of instructions. P1 Specifies the addressing used by the [CLA, INS] instruction. P2 Specifies the addressing used by the [CLA, INS] instruction. Body Specifies the APDU command body. It is of the SC_Body type, which is defined in the smartcard.h file:
27/40
Smartcard interface library: description
typedef struct { u8 LC; u8 Data[LCmax]; u8 LE; } SC_Body;
A N25 9 8
/* Data field length */ /* Command parameters */ /* Expected length of data to be returned */
LC Specifies the number of data bytes transferred to the card as part of the [CLA, INS] instruction execution.
Data Specifies the pointer to the data buffer transferred to the card. LE Specifies the number of data bytes transferred from the card as part of the [CLA, INS] instruction execution.
SC_Response Specifies the APDU command response. It is of SC_ADPU_Response type, defined in the smartcard.h file:
typedef struct { u8 Data[LCmax]; /* Data returned from the card */ u8 SW1; /* Command Processing status */ u8 SW2; /* Command Processing qualification */ } SC_ADPU_Responce;
Data Specifies the pointer to the data buffer which will contain the returned card data. SW1 Specifies the first status code byte. This byte stores the error category. SW2 Specifies the second status code byte. This byte stores a command-specific status or error indication.
Example:
/* Select the Master Root MF */ SC_ADPU.Header.CLA = SC_CLA; SC_ADPU.Header.INS = SC_SELECT_FILE; SC_ADPU.Header.P1 = 0x00; SC_ADPU.Header.P2 = 0x00; SC_ADPU.Body.LC = 0x02; for(i = 0; i < SC_ADPU.Body.LC; i++) { SC_ADPU.Body.Data[i] = MasterRoot[i]; } while(i < LCmax) { SC_ADPU.Body.Data[i++] = 0; } SC_ADPU.Body.LE = 0; SC_Handler(&SCState, &SC_ADPU, &SC_Responce);
28/40
AN2598
Smartcard interface library: description
6.2.2
SC_PowerCmd
It is described in Table 11. Table 11. SC_PowerCmd
SC_PowerCmd
void SC_PowerCmd(FunctionalState NewState);
Function name Function prototype Behavior description Input parameter Output parameter Return parameter Required preconditions Called functions
Enables or disables the power to the Smartcard. NewState: new state of the Smartcard power supply. This parameter can be: ENABLE or DISABLE. None None None None
Example:
/* Power ON the card */ SC_PowerCmd(ENABLE);
6.2.3
SC_Reset
It is described in Table 12. Table 12. SC_Reset
SC_Reset
void SC_Reset(BitAction ResetState);
Function name Function prototype Behavior description
Sets or clears the Smartcard reset pin. ResetState: this parameter specifies the state of the Smartcard reset pin. BitVal must be one of the BitAction enum values: Bit_RESET: to clear the port pin. Bit_SET: to set the port pin. None None None None
Input parameter
Output parameter Return parameter Required preconditions Called functions
Example:
/* Set the Smartcard reset pin */ SC_Reset(Bit_SET);
29/40
Smartcard interface library: description
A N25 9 8
6.2.4
SC_ParityErrorHandler
It is described in Table 13. Table 13. SC_ParityErrorHandler
SC_ParityErrorHandler
void SC_ParityErrorHandler(void);
Function name Function prototype Behavior description Input parameter Output parameter Return parameter Required preconditions Called functions
Resends the byte that failed to be received correctly (by the Smartcard) None None None None None
Example:
/* Resend the byte to the Smartcard */ SC_ParityErrorHandler();
6.2.5
SC_PTSConfig
It is described in Table 14. Table 14. SC_PTSConfig
SC_PTSConfig
void SC_PTSConfig(void);
Function name Function prototype Behavior description Input parameter Output parameter Return parameter Required preconditions Called functions
Configures the IO speed (BaudRate) communication. None None None Must be called just after the ATR sequence. None
Example:
/* Configures the baudrate according to the card TA1 value */ SC_PTSConfig();
6.3
How to send APDU commands to the Smartcard
A detailed description on how to use the SC_Handler( ) function to send the ADPU command to the Smartcard and retrieve the card response is described below. The user has to update the SC_CLA and the Smartcard instruction values according to the Smartcard specifications.
30/40
AN2598
Smartcard interface library: description
6.3.1
SC_GET_A2R
SC_ADPU.Header.CLA = 0x00; SC_ADPU.Header.INS = SC_GET_A2R; SC_ADPU.Header.P1 = 0x00; SC_ADPU.Header.P2 = 0x00; SC_ADPU.Body.LC = 0x00; while(SCState != SC_ACTIVE_ON_T0) { SC_Handler(&SCState, &SC_ADPU, &SC_Responce); }
SCState: It stores the current Smartcard state. SC_ATR_Table: Pointer to an array (filled in by the SC_Handler function) that contains the Smartcard ATR frame.
6.3.2
SELECT_FILE
SC_ADPU.Header.CLA = SC_CLA; SC_ADPU.Header.INS = SC_SELECT_FILE; SC_ADPU.Header.P1 = 0x00; SC_ADPU.Header.P2 = 0x00; SC_ADPU.Body.LC = 0x02; for(i = 0; i < SC_ADPU.Body.LC; i++) { SC_ADPU.Body.Data[i] = FileName[i]; } while(i < LCmax) { SC_ADPU.Body.Data[i++] = 0; } SC_ADPU.Body.LE = 0; SC_Handler(&SCState, &SC_ADPU, &SC_Responce);
FileName: It contains the 16 bit file identifier. SCState: It stores the current Smartcard state. SC_Response->SW1 and SC_Response->SW2: they return the Smartcard response to the SC_SELECT_FILE command.
6.3.3
SC_GET_RESPONSE
SC_ADPU.Header.CLA = SC_CLA; SC_ADPU.Header.INS = SC_GETRESPONSE; SC_ADPU.Header.P1 = 0x00; SC_ADPU.Header.P2 = 0x00; SC_ADPU.Body.LC = 0x00; i = 0; while(i < LCmax) { SC_ADPU.Body.Data[i++] = 0; } SC_ADPU.Body.LE = SC_Responce.SW2;
31/40
Smartcard interface library: description
SC_Handler(&SCState, &SC_ADPU, &SC_Responce);
A N25 9 8
SCState: It stores the current Smartcard state. SC_Response->SW1 and SC_Response->SW2: they return the Smartcard response to the SC_GET_RESPONSE command. SC_Response->Data: It returns the Smartcard data response to the SC_GET_RESPONSE command.
6.3.4
SC_READ_BINARY
SC_ADPU.Header.CLA = SC_CLA; SC_ADPU.Header.INS = SC_READ_BINARY; SC_ADPU.Header.P1 = OFFSET_MSB; SC_ADPU.Header.P2 = OFFSET_LSB; SC_ADPU.Body.LC = 0x00; while(i < LCmax) { SC_ADPU.Body.Data[i++] = 0; } SC_ADPU.Body.LE = LENGTH; SC_Handler(&SCState, &SC_ADPU, &SC_Responce);
SCState: It stores the current Smartcard state. OFFSET_MSB: Most significant byte of offset for reading data. OFFSET_LSB: Least significant byte of offset for reading data. LENGTH: It contains size (in byte) of the area to read (valid only for the elementary file). SC_Response->Data: It returns the Smartcard data to read. SC_Response->SW1 and SC_Response->SW2: they return the Smartcard response to the SC_READ_BINARY command.
6.3.5
SC_CREATE_FILE
SC_ADPU.Header.CLA = SC_CLA; SC_ADPU.Header.INS = SC_CREATE_FILE; SC_ADPU.Header.P1 = 0x00; SC_ADPU.Header.P2 = 0x00; SC_ADPU.Body.LC = 0x10; for(i = 0; i < SC_ADPU.Body.LC; i++) { SC_ADPU.Body.Data[i] = FileParameters[i]; } while(i < LCmax) { SC_ADPU.Body.Data[i++] = 0; } SC_ADPU.Body.LE = 0; SC_Handler(&SCState, &SC_ADPU, &SC_Responce);
32/40
AN2598
Smartcard interface library: description FileParameters: It contains the 16 bytes file parameters (File ID, FILE Access Conditions...). SCState: It stores the current Smartcard state. SC_Response->SW1 and SC_Response->SW2: they return the Smartcard response to the SC_CREATE_FILE command.
6.3.6
SC_UPDATE_BINARY
SC_ADPU.Header.CLA = SC_CLA; SC_ADPU.Header.INS = SC_UPDATE_BINARY; SC_ADPU.Header.P1 = OFFSET_MSB; SC_ADPU.Header.P2 = OFFSET_LSB; SC_ADPU.Body.LC = LENGTH; while(i < LCmax) { SC_ADPU.Body.Data[i++] = 0; } SC_ADPU.Body.LE = 0x00; SC_Handler(&SCState, &SC_ADPU, &SC_Responce);
SCState: It stores the current Smartcard state. OFFSET_MSB: Most significant byte of offset for reading data. OFFSET_LSB: Least significant byte of offset for reading data. LENGTH: It contains the size (in byte) of the area to write (valid only for the elementary file). SC_Responce->Data: It contains the Smartcard data to write. SC_Responce->SW1 and SC_Responce->SW2: they return the Smartcard response to the SC_UPDATE_BINARY command.
6.3.7
SC_VERIFY
SC_ADPU.Header.CLA = SC_CLA; SC_ADPU.Header.INS = SC_VERIFY; SC_ADPU.Header.P1 = 0x00; SC_ADPU.Header.P2 = 0x00; SC_ADPU.Body.LC = 0x08; for(i = 0; i < SC_ADPU.Body.LC; i++) { SC_ADPU.Body.Data[i] = CHV1[i]; } while(i < LCmax) { SC_ADPU.Body.Data[i++] = 0; } SC_ADPU.Body.LE = 0; SC_Handler(&SCState, &SC_ADPU, &SC_Responce);
CHV1: It contains the 8-byte CHV1 code. SCState: It stores the current Smartcard state. SC_Responce->SW1 and SC_Responce->SW2: they return the Smartcard response to the SC_VERIFY command.
33/40
Smartcard interface library: description
A N25 9 8
6.4
Parity error management
In the T0 protocol, error handling is performed on each byte by looking at the parity bit. If the actual parity bit does not correspond to the parity of the transmitted data, then an error must have occurred; the receiving side signals that it requires the byte to be retransmitted in the case of detecting a parity error. This is done by holding the I/O line low (normally the I/O line is set high preceding the transfer of a byte). When the transmitting side detects this, it resends the byte that was not received correctly.
6.4.1
Data sent from card to reader
STM32F10xxx is able to detect a parity error on a received data via hardware, by pulling down the data line during the stop bit.
6.4.2
Data sent from reader to card
Vice versa if the Smartcard pulls down the I/O line to signal that a parity error occurred, the STM32F10xxx is able to detect a frame error via hardware. The Smartcard library uses the SC_ParityErrorHandler() function to check whether a parity error has occurred and, to manage the error if any. Each time the SC_ParityErrorHandler function is called it resends the byte where the error was detected. After a byte is sent from the microcontroller to the card, the Smartcard captures the data sent on the I/O line. If a parity error is detected from the card, the I/O line is pulled down during the stop bits. A frame error event occurs and the related IRQ event invokes the SC_ParityErrorHandler() function that resends the last data.
34/40
AN2598
Smartcard interface example
7
Smartcard interface example
An example is provided in conjunction with the Smartcard library in order to help the user develop its custom application. The example provides simple operations with an ISO 7816-3/4-compatible GSM11.11 Smartcard, such as file system exploration, pin1 enable/disable, read/write operation on files and pin verify on protected files. This example runs on the STM3210B-EVAL and STM3210E-EVAL STMicroelectronics evaluation boards. The boards provide all the hardware needed to interface a Smartcard, and you can easily tailor them to any other hardware. To select the STMicroelectronics evaluation board you wish to use to run the example, uncomment the corresponding line in the platform_config.h file.
7.1
Firmware package description
The STM32F10xxx Smartcard application note firmware package contains both the Smartcard library and the example described in this section. The firmware package contains the following subfolders:
7.1.1
FWLib folder
The FWlib folder contains all the subdirectories and files that make up the core of the STM32F10xxx firmware library:
inc subfolder contains the firmware library header files src subfolder contains the firmware library source files
7.1.2
Smartcard_AN folder
The Smartcard_AN folder contains all the subdirectories and files that make up the core of the Smartcard Interface application example:
include subfolder contains the example header files source subfolder contains the example source files project subfolder contains two projects that compile the example files: EWARMv5: contains the project for the EWARM version 5 toolchain HiTOP: contains the project for the HiTOP toolchain RIDE: contains the project for the RIDE toolchain RVMDK: contains the project for the RVMDK toolchain
7.2
Firmware description
Three directories have been defined for the GSM Smartcard directory tree: MasterRoot[3]={0x3F, 0x00}; GSMDir[3]={0x7F, 0x20}; TelecomDir[3]={0x7F, 0x10};
35/40
Smartcard interface example Figure 11. Smartcard example: file system description
AN2598
At the end of the example:
The ICCID file located under the MasterRoot directory is read The IMSI file, under GSMDir, that has a secure access through PIN1, is read The PIN1 is enabled/disabled
7.2.1
Smartcard startup: answer to reset (A2R)
The first action to perform when the reader wants to access a card is the answer-to-reset procedure. To this aim the SC_Handler is invoked as follows:
SC_ADPU.Header.CLA = 0x00; SC_ADPU.Header.INS = SC_GET_A2R; SC_ADPU.Header.P1 = 0x00; SC_ADPU.Header.P2 = 0x00; SC_ADPU.Body.LC = 0x00; while(SCState != SC_ACTIVE_ON_T0) { SC_Handler(&SCState, &SC_ADPU, &SC_Responce); }
When a card is detected, the A2R sequence is generated, received and decoded. If the recognized protocol is the T0 protocol, the Smartcard state of the reader is active (SC_ACTIVE_ON_T0) and the Smartcard is available for operations on the file system. The procedure type selection (PTS) will be applied after the ATR using the SC_PTSConfig() function. For the used GSM card, the PTS procedure is as follows:
PTSS = 0xFF PTS0 = 0x10 PTS1 = 0x95 PCK = 0x7A
PTS1 = 0x95, F = 9 and D = 5, Fi = 512, Di = 16, BaudRate = 112500 baud.
7.2.2
Reading a file at a specified path
The specified reading path is assumed to be: MasterRoot/GSMDir/IMSI To reach it, the following actions are performed:
Select GSMDir using a SelectFile APDU command Select IMSI File using a SelectFile APDU command
The user has to get the file characteristics to check its access conditions. The IMSI file has a CHV1(PIN1) read condition, so PIN1 has to be checked before reading it. The verify command must be executed under the directory containing the file to be read, the GSMDir must be selected in the example.
36/40
AN2598 To get file characteristics:
Smartcard interface example
Select the file the characteristics of which are needed Get the data returned after issuing the SelectFile APDU command by sending a GETRESPONSE command
The IMSI file has 9 data bytes, so to run correctly the READ_BINARY commands, the following parameters are used:
P1 = 0x00 P2 = 0x00 LE = 0x09
7.2.3
Enabling/disabling the PIN1 (CHV1) code
At the beginning of the application, the PIN1 (CHV1) status is checked. This can be done by a GET_RESPONSE command after a successful MasterRoot selection. In this example, the PIN1 status is checked. If it is enabled, the PIN1 will be disabled to give access to all files that have a secure access conditions. To check the PIN1 status, the procedure is the following:
Select the MasterRoot directory using a SelectFile APDU command Get the data returned after issuing the MasterRoot SelectFile command by sending a GETRESPONSE command. Check the bit8 of the 14 received bytes: if bit8 is 0: PIN1 is enabled else the PIN1 is disabled.
To enable or disable PIN1, the CHV1 code must be sent to the card. The CHV1 code is 8byte long.
7.2.4
Verifying the PIN1 (CHV1) code
Some files have a restricted access conditions such as IMSI, CHV1 file, CHV2. The access conditions of these files must be met for the user to be allowed to execute the restricted operations (read, update, change CHV1). To verify the PIN1 (CHV1) condition, the procedure is as follows:
Go to the directory which contain the file to be accessed Use the Verify APDU command by presenting the CHV1 code Select the file and execute the selected operation
37/40
Conclusion
AN2598
8
Conclusion
Thanks to the STM32F10xxx USART's Smartcard mode that supports the ISO 7816-3/4 specification, the user can develop a Smartcard-based application with reduced firmware and hardware resources.
38/40
AN2598
Revision history
9
Revision history
Table 15.
Date 03-Aug-2007
Document revision history
Revision 1 Initial release. Firmware updated to support STM32F10xxx High-density devices and to run on the STM3210E-EVAL evaluation board: Table 2: STM32F10xxx and Smartcard connection on page 8 updated. Section 7.1.2: Smartcard_AN folder on page 35 updated. Small text changes. Changes
30-May-2008
2
39/40
AN2598
Please Read Carefully:
Information in this document is provided solely in connection with ST products. STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, modifications or improvements, to this document, and the products and services described herein at any time, without notice. All ST products are sold pursuant to ST's terms and conditions of sale. Purchasers are solely responsible for the choice, selection and use of the ST products and services described herein, and ST assumes no liability whatsoever relating to the choice, selection or use of the ST products and services described herein. No license, express or implied, by estoppel or otherwise, to any intellectual property rights is granted under this document. If any part of this document refers to any third party products or services it shall not be deemed a license grant by ST for the use of such third party products or services, or any intellectual property contained therein or considered as a warranty covering the use in any manner whatsoever of such third party products or services or any intellectual property contained therein.
UNLESS OTHERWISE SET FORTH IN ST'S TERMS AND CONDITIONS OF SALE ST DISCLAIMS ANY EXPRESS OR IMPLIED WARRANTY WITH RESPECT TO THE USE AND/OR SALE OF ST PRODUCTS INCLUDING WITHOUT LIMITATION IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE (AND THEIR EQUIVALENTS UNDER THE LAWS OF ANY JURISDICTION), OR INFRINGEMENT OF ANY PATENT, COPYRIGHT OR OTHER INTELLECTUAL PROPERTY RIGHT. UNLESS EXPRESSLY APPROVED IN WRITING BY AN AUTHORIZED ST REPRESENTATIVE, ST PRODUCTS ARE NOT RECOMMENDED, AUTHORIZED OR WARRANTED FOR USE IN MILITARY, AIR CRAFT, SPACE, LIFE SAVING, OR LIFE SUSTAINING APPLICATIONS, NOR IN PRODUCTS OR SYSTEMS WHERE FAILURE OR MALFUNCTION MAY RESULT IN PERSONAL INJURY, DEATH, OR SEVERE PROPERTY OR ENVIRONMENTAL DAMAGE. ST PRODUCTS WHICH ARE NOT SPECIFIED AS "AUTOMOTIVE GRADE" MAY ONLY BE USED IN AUTOMOTIVE APPLICATIONS AT USER'S OWN RISK.
Resale of ST products with provisions different from the statements and/or technical features set forth in this document shall immediately void any warranty granted by ST for the ST product or service described herein and shall not create or extend in any manner whatsoever, any liability of ST.
ST and the ST logo are trademarks or registered trademarks of ST in various countries. Information in this document supersedes and replaces all information previously supplied. The ST logo is a registered trademark of STMicroelectronics. All other names are the property of their respective owners.
2008 STMicroelectronics - All rights reserved STMicroelectronics group of companies Australia - Belgium - Brazil - Canada - China - Czech Republic - Finland - France - Germany - Hong Kong - India - Israel - Italy - Japan Malaysia - Malta - Morocco - Singapore - Spain - Sweden - Switzerland - United Kingdom - United States of America www.st.com
40/40
Document Number: 13750