VIPer53DIP VIPer53SP
OFF LINE PRIMARY SWITCH
TYPICAL OUTPUT POWER CAPABILITY
TYPE DIP-8 PowerSO-10TM
Note:
European (195 - 265 Vac) 50W 65W
US / Wide range (85 - 265 Vac) 30W 40W
10
1
Above power capabilities are given under adequate thermal conditions
D I P -8
P o werS O- 1 0 TM
FEATUR ES n SWITCHING FREQUENCY UP TO 300 kHz n CURRENT LIMITATION n CURRENT MODE CONTROL WITH ADJUSTABLE LIMITATION n SOFT START AND SHUT DOWN CONTROL n AUTOMATIC BURST MODE IN STAND-BY CONDITION ("BLUE ANGEL" COMPLIANT) n UNDERVOLTAGE LOCKOUT WITH HYSTERESIS n HIGH VOLTAGE STARTUP CURRENT SOURCE n OVERTEMPERATURE PROTECTION n OVERLOAD AND SHORT-CIRCUIT CONTROL BLOCK DIAGRAM
bs O
let o
VDD
Pr e
8.4/ 11.5V 15V
du o
(s) ct
OVERTEMP. DETECTOR
so Ob OSC
DESCRIPTION The VIPer53 combines in the same package an enhanced current mode PWM controller with a high voltage MDMesh Power Mosfet. Typical applications cover off line power supplies with a secondary power capability ranging up to 30W in wide range input voltage or 50W in single European voltage range and DIP-8 package, with the following benefits: Overload and short circuit controlled by feedback monitoring and delayed device reset. Efficient standby mode by enhanced pulse skipping. Primary regulation or secondary loop failure protection through high gain error amplifier.
te le
ro P
uc d
s) t(
DRAIN
ON/OFF OSCILLATOR
PWM LATCH R1 R2 R3 S FF R4 Q R5 0.5V 150/400ns BLANKING STANDBY COMPARATOR 0.5V 4V PWM COMPARATOR 8V H COMP BLANKING TIME SELECTION 1V
UVLO COMPARATOR
CURRENT AMPLIFIER
125k ERROR AMPLIFIER
4.35V
OVERLOAD COMPARATOR OVERVOLTAGE COMPARATOR
18V
4.5V
TOVL
COMP
SOURCE
June 2004
1/24
VIPer53DIP / VIPer53SP
PIN FUNCTION
Name Function Power supply of the control circuits. Also provides the charging current of the external capacitor during start-up. The functions of this pin are managed by four threshold voltages: - VDDon: Voltage value at which the device starts switching (Typically 11.5 V). - VDDoff: Voltage value at which the device stops switching (Typically 8.4 V). - VDDreg: Regulation voltage point when working in primary feedback (Trimmed to 15 V). - VDDovp: Triggering voltage of the overvoltage protection (Trimmed to 18 V). Power Mosfet source and circuit ground reference. Power Mosfet drain. Also used by the internal high voltage current source during the start-up phase, for charging the external VDD capacitor. Input of the current mode structure, and output of the internal error amplifier. Allows the setting of the dynamic characteristic of the converter through an external passive network. Useful voltage range extends from 0.5 V to 4.5 V. The Power Mosfet is always off below 0.5 V, and the overload protection is triggered if the voltage exceeds 4.35V. This action is delayed by the timing capacitor connected to the TOVL pin. Allows the connection of an external capacitor for delaying the overload protection, which is triggered by a voltage on the COMP pin higher than 4.35V. Allows the setting of the switching frequency through an external Rt-Ct network.
VDD
SOURCE DRAIN
COMP
TOVL OSC
CURRENT AND VOLTAGE CONVENTIONS
IDD ID
VDD I OSC OSC 15V
DRAIN
VDD I TOVL VOSC
TOVL
CONNECTION DIAGRAM
COMP
O
bs
let o
OSC 2
Pr e
1 3 4
du o
8 7 6 5
(s) ct
VTOVL
Ob COMP ICOMP VCOMP
so
te le
ro P
uc d
s) t(
SOURCE
VDS
TOVL
DRAIN NC 1 2 3 4 5 10 9 8 7 6 SOURCE NC NC OSC COMP
VDD
NC NC
SOURCE
NC
VDD TOVL
SOURCE
DRAIN
DIP-8 ORDER CODES
PACKAGE
PowerSO-10TM
TUBE
VIPer53DIP VIPer53SP
TAPE and REEL VIPer53SP13TR
DIP-8 PowerSO-10TM
2/24
VIPer53DIP / VIPer53SP
ABSOLUTE MAXIMUM RATINGS
Symbol V DS ID VDD VOSC ICOMP ITOVL VESD Tj Tc Tstg Parameter Continuous Drain Source Voltage (Tj=25 ... 125C) Continuous Drain Current Supply Voltage OSC Input Voltage Range COMP and TOVL Input Current Range Electrostatic Discharge: Machine Model (R=0; C=200pF) Charged Device Model Junction Operating Temperature Case Operating Temperature Storage Temperature (See note 1) (See note 1) Value -0.3 ... 620 Internally limited 0 ... 19 0 ... VDD -2 ... 2 Unit V A V V mA
200 1.5 Internally limited -40 to 150 -55 to 150
V kV C C C
Note: 1. In order to improve the ruggedness of the device versus eventual drain overvoltages, a resistance of 1 k should be inserted in series with the TOVL pin.
THERMAL DATA
Symbol Rthj-case Rthj-amb Rthj-case Rthj-amb DIP-8 DIP-8 (See note 2) Parameter
Max Value
P o w e r S O- 1 0 TM P o w e r S O- 1 0 TM
Note: 2. When mounted on a standard single-sided FR4 board with 50mm˛ of Cu (at least 35 m thick) connected to the DRAIN pin. 3. When mounted on a standard single-sided FR4 board with 50mm˛ of Cu (at least 35 m thick) connected to the device tab.
bs O
let o
Pr e
du o
(s) ct
so Ob -
(See note 3)
eP let
ro
20
uc d
s) t(
Unit
C/W C/W C/W C/W
80 2 60
3/24
VIPer53DIP / VIPer53SP
ELECTRICAL CHARACTERISTICS (Tj=25C , VDD=13V, unless otherwise specified) POWER SECTION
Symbol BVDSS IDSS RDS(on) Parameter Drain-Source Voltage Off State Drain Current Static Drain-Source On State Resistance Fall Time Rise Time Drain Capacitance Effective Output Capacitance Test Conditions ID=1mA; VCOMP=0V VDS=500V; VCOMP=0V; Tj=125C ID=1A; VCOMP=4.5V; VTOVL=0V Tj=25C Tj=100C ID=0.2A; VIN=300V (See figure 1 and note 4) ID=1A; VIN=300V (See figure 1 and note 4) VDS=25V 200V < VDSon < 400V (See note 5) 0.9 Min. 620 150 1 1.7 Typ. Max. Unit V A ns ns pF pF
tfv t rv Coss CEon
100 50 170 60
Note 4. On clamped inductive load 5. This parameter can be used to compute the energy dissipated at turn on Eton according to the initial drain to source voltage VDSon 1.5 1 2 VD S o n and the following formula: E t o n = -- C E o n 300 --------------- 300 2
OSCILLATOR SECTION
Symbol FOSC1 FOSC2 VOSChi VOSClo Parameter Oscillator Frequency Initial Accuracy Oscillator Frequency Total Variation Oscillator Peak Voltage Oscillator Valley Voltage Test Conditions RT=8k; CT=2.2nF (See figure 9)
(See figure 12) RT=8k; CT=2.2nF VDD=VDDon ... VDDovp; Tj=0 ... 100C
bs O
let o
Pr e
du o
(s) ct
so Ob -
te le
Min. 95 93
ro P
uc d
s) t(
Typ. 100 100 9 4
Max. 105 107
Unit kHz kHz V V
4/24
VIPer53DIP / VIPer53SP
ELECTRICAL CHARACTERISTICS (Tj=25C , VDD=13V, unless otherwise specified) SUPPLY SECTION
Symbol VDSstart IDDch1 IDDch2 IDDchoff IDD0 IDD1 VDDoff VDDon VDDhyst VDDovp Parameter Drain Voltage Starting Threshold Startup Charging Current Startup Charging Current Startup Charging Current in Thermal Shutdown Test Conditions VDD=5V; IDD=0mA VDD=0 ... 5V; VDS=100V (See figure 2) VDD=10V; VDS=100V VDD=5V; VDS=100V Tj > TSD - THYST (See figure 2) (See figure 5) 0 8 9 7.5 10.2 2.6 17 8.4 11.5 3.1 18 9.3 12.8 11 Min. Typ. 34 -12 -2 Max. 50 Unit V mA mA mA mA mA V V
Operating Supply Current Fsw=0kHz; VCOMP=0V Not Switching Operating Supply Current F =100kHz sw Switching VDD Undervoltage Shutdown Threshold VDD Startup Threshold VDD Threshold Hysteresis VDD Overvoltage Shutdown Threshold (See figure 2) (See figure 2) (See figure 2) (See figure 7)
ERR OR AMPLIFIER SECTION
Symbol VDDreg VDDreg GBW AVOL Gm VCOMPlo VCOMPhi ICOMPlo ICOMPhi Parameter VDD Regulation Point VDD Regulation Point Total Variation Unity Gain Bandwidth Voltage Gain DC Transconductance Output Low Level Test Conditions ICOMP=0mA
ICOMP=0mA; Tj=0 ... 100C
Output High Level
Output Sinking Current
bs O
Note 6. In order to insure a correct stability of the error amplifier, a capacitor of 10nF (minimum value: 8nF) should always be present on the COMP pin.
let o
Output Sourcing Current
Pr e
du o
(s) ct
ICOMP=0mA
From Input =VDD to Output = VCOMP ICOMP=0mA (See figure 10) (See figure 10) (See figure 3) 40 1
Ob -
so
(See figure 3)
te le
ro P
uc d
s) t(
V V Unit V % kHz dB
19
Min. 14.5
Typ. 15 2 700 45 1.4 0.2
Max. 15.5
VCOMP=2.5V ICOMP=-0.4mA; VDD=16V ICOMP=0.4mA; VDD=14V VCOMP=2.5V; VDD=16V VCOMP=2.5V; VDD=14V
1.8
mS V V mA mA
(See note 6) (See figure 3) (See figure 3)
4.5 -0.6 0.6
5/24
VIPer53DIP / VIPer53SP
ELECTRICAL CHARACTERISTICS (Tj = 25 C, VDD = 13 V, unless otherwise specified) PW M COMPARATOR SECTION
Symbol HCOMP VCOMPos IDlim IDmax td VCOMPbl tb1 tb2 tONmin1 tONmin2 VCOMPoff Parameter VCOMP / IDPEAK VCOMP Offset Peak Drain Current Limitation Drain Current Capability Current Sense Delay to Turn-Off VCOMP Blanking Time Change Threshold Blanking Time Blanking Time Minimum On Time Minimum On Time VCOMP Shutdown Threshold Test Conditions VCOMP=1 ... 4 V dID/dt=0 dID/dt=0 ICOMP=0mA; VTOVL=0V dID/dt=0 (See figure 8) 1.7 (See figure 8) (See figure 8) 1.7 1.6 2 1.9 250 1 (See figure 11) (See figure 11) 300 100 450 250 400 150 600 350 0.5 500 200 750 450 2.3 2.3 A A ns V 2 0.5 2.3 V/A V Min. Typ. Max. Unit
VCOMP=VCOMPovl; VTOVL=0V dID/dt=0 (See figure 8) ID=1A (See figure 11) VCOMP < VCOMPBL VCOMP > VCOMPBL VCOMP < VCOMPBL VCOMP > VCOMPBL (See figure 6)
OVERLOAD PROTECTION SECTION
Symbol VCOMPovl VDIFFovl VOVLth tOVL Parameter VCOMP Overload Threshold VCOMPhi to VCOMPovl Voltage Difference VTOVL Overload Threshold Overload Delay ITOVL=0mA Test Conditions
Note 7. VCOMPovl is always lower than VCOMPhi.
OVERTEMPERATUR E PROTECTION SECTION
Symbol TSD
O
bs
THYST
let o
Thermal Shutdown Temperature Thermal Shutdown Hysteresis
Pr e
du o
(s) ct
(See fig. 5) (See fig. 5)
VDD=VDDoff ... VDDreg; ITOVL=0mA (See figure 4 and note 7) (See figure 4) COVL=100nF (See figure 4)
so Ob -
(See figure 4 and note 7)
te le
ro P
Min. 50
uc d
s) t(
V
ns ns
ns ns
Typ. 4.35 150 4 8
Max.
Unit V
250
mV V ms
Parameter
Test Conditions
Min. 140
Typ. 160 40
Max.
Unit C C
6/24
VIPer53DIP / VIPer53SP
Figure 1: Rise and Fall Time
ID
C<
t
VDD DRAIN
VDS
OSC 300V 15V
90% tfv tr v
TOVL
COMP
SOURCE
10%
t
Figure 2: Start-up VDD Current
IDD
IDD0 VDDhyst
Figure 4: Overload event
VDD
Normal operation VDDon VDDoff
VDDoff IDDch2
VDDon
V DD
VDS = 100 V FSW = 0 kHz
IDDch1
Figure 3: Output Characteristics
ICOMP
ICOMPhi
bs O
0 ICOMPlo
let o
Pr e
du o
VDDreg
(s) ct
so Ob VCOMP
VCOMPhi VCOMPovl
te le
ro P
VDIFFovl
Abnormal operation
uc d
s) t(
t
t VTOVL
VOVLth tOVL
Slope = Gm
t V DD VDS
Not switching
Switching
t
7/24
VIPer53DIP / VIPer53SP
Figure 5: Thermal Shutdown
Tj
TS D
TSD-T HYST
Figure 7: Overvoltage Event
VDD
VDDovp
t VDD
VDDon
t VCOMP
Abnormal operation
Automatic startup
Normal operation
t VCOMP VDS
t
Not switching
Switching
t
Figure 6: Shut Down Action
VOSC
VOSChi
VOSClo
VCOMP
VCOMPoff
bs O
ID
let o
Pr e
du o
(s) ct
so Ob IDpeak
IDlim IDmax
Figure 8: Comp Pin Gain and Offset
eP let
ro
uc d
s) t(
t
t
Slope = 1 / HC OMP
VCOMP t
VCOMPos VCOMPovl VCOMPhi
t
8/24
VIPer53DIP / VIPer53SP
Figure 9: Oscillator Schematic and Settings
Vcc
VDD
Rt
The switching frequency settings shown on the graphic here below is valid within the following boundaries: Rt > 2 k F S W < 300 k H z
OSC
PWM section
320
Ct
SOURCE
Frequency (kHz)
300
2.2nF
4.7nF
1nF
100
10nF
22nF
bs O
let o
Pr e
10
du o
1
(s) ct
so Ob 10
te le
ro P
uc d
s) t(
100
RT (K)
9/24
VIPer53DIP / VIPer53SP
Figure 10: Error Amplifier Transfer Function
Vin VDD DRAIN
OSC 15V
TOVL
COMP
SOURCE Vout
R
This configuration is for test purpose only. In order to insure a correct stability of the error amplifier, a capacitor of 10nF (minimum value: 8nF) should be always connected between COMP pin and ground. See figures 14, 15 and 18.
2.5 V
Gain (dB)
60
Open
40
R = 10 k
20
R = 2.2 k
0
R = 470
-20
-40
-60
1
Figure 11: Blanking Time
tb
bs O
tb1
let o
Pr e
du o
(s) ct
10 100
so Ob 1k 10k
te le
100k
ro P
uc d
s) t(
1M
10M
Frequency (Hz)
tb2
VCOMP
VCOMPbl VCOMPhi
10/24
VIPer53DIP / VIPer53SP
Figure 12: Typical Frequency Variation vs. Junction Temperature
Normalised Frequency
1.04
1.02
1
0.98
0.96
-20
0
20
40
60
80
100
120
Temperature (C)
Figure 13: Typical Current Limitation vs. Junction Temperature
Normalised IDlim
1.04
bs O
let o
Pr e
0.98 0.96
1.02
du o
(s) ct
so Ob -
te le
ro P
uc d
s) t(
1
-20
0
20
40
60
80
100
120
Temperature (C)
11/24
VIPer53DIP / VIPer53SP
Figure 14: Off Line Power Supply With Auxiliary Supply Feedback
F1
AC IN
C1
D1 T1
R1
C2
R2 C3
T2
D2
L1 D4 R4 U1 VIPer73 R3 VDD DRAIN C10 D3 C8 C9 DC OUT
OSC 15V
C4
TOVL
COMP
SOURCE
R6 1k C5 C11 10nF C6
R5
C7
bs O
PRIMARY REGULATION CONFIGURATION EXAMPLE The schematic on figure 14 delivers a fixed output voltage by using the internal error amplifier of the device in a primary feedback configuration. The primary auxiliary winding provides a voltage to the VDD pin, and is automatically regulated at 15 V thanks to the internal error amplifier connected on this pin. The secondary voltage has to be adjusted through the turn ratio of the transformer between auxiliary and secondary. The error amplifier of the VIPer53 is a transconductance one: its output is a current proportional to the difference of voltage between the VDD pin and the internal trimmed 15 V reference, i.e. the error voltage. As the transconductance value is set at a relatively low value to control the overall loop gain and insure stability, this current has to be integrated by a capacitor (C7 in the above schematic). When the steady state operation is reached, this capacitor blocks any DC current from the COMP pin and imposes a nil error voltage. Therefore, the VDD voltage is accurately regulated to 15 V.
let o
od Pr e
ct u
(s)
so Ob -
te le
ro P
uc d
s) t(
This results in a good load regulation, which depends only on transformer coupling and output diodes impedance. The current mode structure takes care of all incoming voltage changes, thus providing at the same time an excellent line regulation. The switching frequency can be set to any value through the choice of R3 and C5. This allows to optimize the efficiency of the converter by adopting the best compromise between switching losses, EMI (Lower with low switching frequencies) and transformer size (Smaller with high switching frequencies). For an output power of a few watts, typical switching frequencies are comprised between 20 kHz and 40 kHz because of the small size of the transformer. For higher power, 70 kHz to 130 kH z are generally chosen. The value of the compensation resistor R5 sets the dynamic behavior of the converter. It can be adjusted to provide the best compromise between stability and recovering time with fast load c han ges .
12/24
VIPer53DIP / VIPer53SP
Figure 15: Off Line Power Supply With Optocoupler Feedback
F1
AC IN
C1
D1 T1
R1
C2
R2 C3
T2
D2
L1 D4 R4 D3 C8 C9 DC OUT
U1 VIPer73 R3 VDD DRAIN C10
OSC 15V R8 TOVL COMP SOURCE U2
C4
C5
R9 1k
C11 10nF
R5
C6
C7
bs O
SECONDARY FEEDBACK CONFIGURATION EXAMPLE When a more accurate output voltage is needed, the definitive way is to monitor it directly on secondary side, and to drive the PWM controller through an optocoupler as shown on figure 15. The optocoupler is connected in parallel with the compensation network on the COMP pin. The design of the auxiliary winding will be made in such a way that the V DD voltage is always lower than the internal 15 V reference. The internal error amplifier will therefore be saturated in the high state, and because of its transconductance nature, will deliver a constant biasing current of 0.6 mA to the optotransistor. This current doesn't depend on the compensation voltage, and so it doesn't depend on the output load either. The gain of the optocoupler ensures consequently a constant biasing of the TL431 device (U3) which is in charge of secondary regulation. If the optocoupler gain is sufficiently low, no additional components are required to ensure a minimum current biasing of U3. Also, the
let o
ro P e
uc d
(s) t
so Ob -
te le
U3
ro P
C12
uc d
s) t(
R7
R6
low biasing current value avoid any ageing of the optocoupler. The constant current biasing can be used to simplify the secondary circuit: Instead of a TL431, a simple zener and resistance network in series with the optocoupler diode can insure a good secondary regulation. As the current flowing in this branch remains constant for the same reason as above, typical load regulation of 1% can be achieved from zero to full output current with this simple configuration. Since the dynamic characteristics of the converter are set on the secondary side through components associated to U3, the compensation network has only a role of gain stabilization for the optocoupler, and its value can be freely chosen. R5 can be set to a fixed value of 1 k, offering the possibility of using C7 as a soft start capacitor: When starting up the converter, the VIPer53 device delivers a constant current of 0.6 mA on the COMP pin, creating a constant voltage of 0.6 V in R5 and a rising slope across C7. This voltage shape together with the operating range of 0.5 V to 4.5 V
13/24
VIPer53DIP / VIPer53SP
provides a soft start-up of the converter. The rising speed of the output voltage can be set through the value of C7. C4 and C6 values must be adjusted accordingly in order to ensure a correct start-up. CURRENT MODE TOPOLOGY The VIPer53 implements the conventional current mode control method for regulating the output voltage. This kind of feedback includes two nested regulation loops: The inner loop controls the peak primary current cycle by cycle. When the Power MOSFET output transistor is on, the inductor current (primary side of the transformer) is monitored with a SenseFET technique and converted into a voltage VS. When VS reaches VCOMP, the power switch is turned off. This structure is completely integrated as shown on the Block Diagram of page 1, with the current amplifier, the PWM comparator, the blanking time function and the PWM latch. The following formula gives the peak current in the Power MOSFET according to the compensation voltage: VC O MP VCO MP os I D p e a k = --------------------------------------------HCOM P The outer loop defines the level at which the inner loop regulates peak current in the power switch. For this purpose, VCOMP is driven by the output of the error amplifier (Either the internal one in primary feedback configuration or a TL431 through an optocoupler in secondary feedback configuration, see figures 14 and 15) and is set accordingly the peak drain current for each sw itching cycle. As the inner loop regulates the peak primary current in the primary side of the transformer, all input voltage changes are compensated for before impacting the output voltage. This results in an improved line regulation, instantaneous correction to line changes and better stability for the voltage regulation loop. Current mode topology also provides a good converter start-up control. As the compensation voltage can be controlled to increase slowly during the start-up phase, the peak primary current will follow this soft voltage slope to provide a smooth output voltage rise, without any overshoot. The simpler voltage mode structure which only controls the duty cycle, leads generally to high currents at start-up with the risk of transformer saturation. The compensation pin can also be used to limit the current capability of the device (See Current Limitation section). An integrated blanking filter inhibits the PWM comparator output for a short time after the integrated Power MOSFET is switched on. This function prevents anomalous or premature termination of the switching pulse in the case of current spikes caused by primary side transformer capacitance or secondary side rectifier reverse recovery time when working in continuous mode. STA NDBY MODE The device implements a special feature to address the low load condition. The corresponding function described hereafter consists of reducing the switching frequency by going into burst mode, with the following benefits: It reduces the switching losses, thus providing low consumption on the mains lines. The device is compliant with "Blue Angel" and other similar standards, requiring less than 0.5 W of input power when in standby. It allows the regulation of the output voltage, even if the load corresponds to a duty cycle that the device is not able to generate because of the internal blanking time, and associated minimum turn on. For this purpose, a comparator monitores the COMP pin voltage, and maintains the PWM latch and the Power MOSFET in the off state as long as VCOMP remains below 0.5 V (See Block Diagram on page 1). If the output load requires a duty cycle below the one defined by the minimum turn on of the device, the error amplifier decreases its output voltage until it reaches this 0.5 V threshold (VCOMPoff). The Power MOSFET can be completely off for some cycles, and resumes normal operation as soon as VCOMP is higher than 0.5 V. The output voltage is regulated in burst mode. The corresponding ripple is not higher than the nominal one at full load. In addition, the minimum turn on time which defines the frontier between normal operation and burst mode changes according to VCOMP value. Below 1 V (VCOMPbl), the blanking time increases to 400 ns, whereas it is 150 ns for higher voltages (See figure 11). The minimum turn on times resulting from these values are respectively 600 ns and 350 ns, when taking into account internal propagation time. This brutal change induces an hysteresis between normal operation and burst mode as shown on figure 16. W hen the output power decreases, the system reaches point 2 where VCOMP equals VCOMPbl. The minimum turn on time passes immediately from 350 ns to 600 ns, exceeding the effective turn on time that should be needed at such output power level. Therefore the regulation loop will quickly drive VCOMP to VCOMPoff (Point 3) in order to pass into burst mode and to control the output voltage. The corresponding hysteresis can be seen on the switching frequency which passes from FSWnom which is the normal switching frequency set by the components connected to the OSC pin, to FSWstby. Note that this frequency is
bs O
let o
Pr e
du o
(s) ct
so Ob -
te le
ro P
uc d
s) t(
14/24
VIPer53DIP / VIPer53SP
Figure 16: Standby Mode Implementation
ton
600ns Minimum turn on 350ns 3 1 2
VCOMP
VCOM Psd VCOM Poff VC OMPb l
PIN
PRST 3 PST BY 2 1
FSW
FSW stb y FSW no m
actually an equivalent number of switching pulses per second, rather than a fixed switching frequency, as the device is working in burst mode. As long as the power remains below P RST the output of the regulation loop remains stuck at VCOMPsd and the converter works in burst mode. Its "density" increases (i.e. the number of missing cycles decreases) as the power approaches PRST and resumes finally normal operation at point 1. The hysteresis cannot be seen on the switching frequency, but the COMP pin voltage which passes brutally at that power level from point 3 to point 1. The power points value PRST and PSTBY are defined by the following formulas: 1 2 1 2 P R S T = -- F S W n o m ( t b 1 + t d ) V I N -----2 Lp 1 2 P S T B Y = -- F S W n o m I p ( V C O M P b l ) L p 2
HIGH VOLTAGE START-UP CURRENT SOURCE An integrated high voltage current source provides a bias current from the DRAIN pin during the startup phase. This current is partially absorbed by internal control circuits in standby mode with reduced consumption and also supplies the external capacitor connected to the VDD pin. As soon as the voltage on this pin reaches the high voltage threshold VDDon of the UVLO logic, the device turns into active mode and starts switching. The start-up current generator is switched off, and the converter should normally provide the needed current on the VDD pin through the auxiliary winding of the transformer, as shown on figure 14 or 15. The external capacitor CVDD on the VDD pin must be sized according to the time needed by the converter to start-up, when the device starts switching. This time tss depends on many parameters, among which transformer design, output capacitors, soft start feature and compensation network implemented on the COMP pin and possible secondary feedback circuit. The following formula can be used for defining the minimum capacitor needed: ID D 1 t s s C V D D > ---------------------VD D h yst Figure 17 shows a typical start-up event. VDD starts from 0 V with a charging current I DDch1 at about 9 mA. When about VDDoff is reached, the Figure 17: Startup Waveforms
IDD
bs O
Where Ip(VCOMPbl) is the peak Power MOSFET current corresponding to a compensation voltage of VCOMPbl (1V), that is to say about 250 mA. Note that the power point P STBY where the converter is going into burst mode doesn't depend on the input voltage. The standby frequency FSWstb y is given by: PST BY F S W s t b y = -------------- F S W n o m PRST
let o
od Pr e
uc
(s) t
so Ob IDD1 IDDc h2
te le
ro P
uc d
s) t(
t
IDDc h1
VDD
VDDre g VDDst VDDs d tsu
tss
The ratio between the nominal switching frequency and the standby one can be as high as 4, depending on the Lp value and input voltage.
t
15/24
VIPer53DIP / VIPer53SP
charging current is reduced down to IDDch2 which is about 0.6 mA. This lower current leads to a slope change on the VDD rise. The device starts sw itching for a VDD equal to VDDon, and the auxiliary winding delivers some energy to the VDD capacitor after the start-up time tss. The charging current change at VDDoff allows a fast complete start-up time tsu, and maintains a low restart duty cycle. This is especially useful for short circuits and overloads conditions, as described in the following section. SHORT-CIRCUIT AND OVERLOAD PROTECTION A VCOMPovl threshold of about 4.35 V has been implemented on the COMP pin. When VCOMP goes above this level, the capacitor connected on the TOVL pin begins to charge. When reaching typically 4 V (VOVLth), the internal mosfet driver is disabled and the device stops switching. This state is latched thanks to the regulation loop which maintains the COMP pin voltage above the VCOMPovl threshold. Since the VDD pin doesn't receive any more energy from the auxiliary winding, its voltage drops down until it reaches VDD off and the device is reset, recharging the VDD capacitor for a new restart cycle. Note that if VCOMP drops down below the V COMPovl threshold for any reason during the VDD drop, the device resumes switching immediately. The device enters an endless restart sequence if the overload or short circuit condition is maintained. The restart duty cycle DRST is defined as the time ratio for which the device tries to restart, thus delivering its full power capability to the output. In order to keep the whole converter in a safe state during this event, D RST must be kept as low as possible, without compromising the real start up of the converter. A typical value of about 10 % is generally sufficient. For this purpose, both VDD and TOVL capacitors can be used to satisfy the following conditions: 6 C O V L > 12.5 10 t s s CO V L ID D c h2 1 4 C V D D > 8 10 ----------- 1 -------------------------------- DRST VD D h ys t overload protection is not triggered, it defines the power capability of the power supply. TRANSCONDUCTANCE ERROR AMPLIFIER The VIPer53 includes a transconductance error amplifier. Transconductance Gm is the change in output current ICOMP versus change in input voltage VDD. Thus:
Gm =
I C O M P VD D
The output impedance ZCOMP at the output of this amplifier (COMP pin) can be defined as:
ZC O MP =
V C O M P
1 V C O M P = -------- G m VD D ICO MP
This last equation shows that the open loop gain AVOL can be related to Gm and ZCOMP:
AVO L = G m ZCO M P
O
Refer to the previous start-up section for the definition of tss, and CVDD must also be checked against the limit given in this section. The maximum value of the two calculus will be adopt ed. All this behavior can be observed on figure 4. In Figure 8 the value of the drain current Id for VCOMP=VCOMPovl is shown. The corresponding parameter I Dmax is the drain current to take into account for design purpose. Since IDmax represents the maximum value for which the
bs
let o
Pr e
du o
(s) ct
so Ob -
where Gm value for VIPer53 is typically 1.4 mA/V. Gm is well defined by specification, but ZCOMP and therefore AVOL are subject to large tolerances. An impedance Z must be connected between the COMP pin and ground in order to define accurately the transfer function F of the error amplifier, according to the following equation, very similar to the one above: F(s) = G m Z(s) The error amplifier frequency response is shown in figure 10 for different values of a simple resistance connected on the COMP pin. The unloaded transconductance error amplifier shows an internal ZCOMP of about 140 K. More complex impedances can be connected on the COMP pin to achieve different compensation methods. A capacitor provides an integrator function, thus eliminating the DC static error, and a resistance in series leads to a flat gain at higher frequency,
te le
ro P
uc d
s) t(
Figure 18: Typical Compensation Network
VDD DRAIN
OSC 15V
TOVL
COMP
SOURCE
Rcomp 10nF
Ccomp
16/24
VIPer53DIP / VIPer53SP
introducing a zero and ensuring a correct phase margin. This configuration is illustrated in figure 18 Figure 19: Typical Transfer Functions
Gain (dB)
60
Rcomp=4.7k Ccomp=470nF
for the schematic and figure 19 for the error
50 40 30 20 10 0 - 10 1 10 100 1k 10k 100 k 1M
Frequency (Hz) Phase ()
0 -10 -20 -30 -40 -50 -60 -70 -80 -90 -100
R comp=4.7k C comp=470nF
bs O
amplifier transfer function for a typical set of values for CCOMP and RCOMP. Note that a capacitor of 10 nF (minimum value: 8 nF) should always be connected to the COMP pin to insure a correct stability of the internal error amplifier. The complete converter open loop transfer function can be built from both power cell and error amplifier transfer functions. A theoretical example can be seen in figure 20 for a discontinuous mode flyback loaded by a simple resistor, regulated from primary side (no optocoupler, the internal error amplifier is fully used for regulation). A typical schematic corresponding to this situation can be seen on figure 14.
let o
Pr e
du o
1
(s) ct
100
so Ob 1k 1 0k
te le
ro P
uc d
s) t(
10
100 k
1M
Frequency (Hz)
The transfer function of the power cell is represented as G(s) in figure 20. It exhibits a pole which depends on the output load and on the output capacitor value. As the load of a converter may change, two curves are shown for two different values of output resistance value, RL1 and RL2. A zero at higher frequency values then appears, due to the output capacitor ESR. Note that the overall transfer function doesn't depend on the input voltage, thanks to the current mode control. The error amplifier has a fixed behavior, similar to the one shown in figure 19. Its bandwidth is limited, in order to avoid injection of high frequency noise
17/24
VIPer53DIP / VIPer53SP
Figure 20: Complete Converter Transfer Function
G(S)
P M AX 3 .2 ------------------P O U T1 P MAX 3.2 ------------------P OU T 2 1 --------------------------------------R C L1 O UT 1 --------------------------------------R C L2 O UT
F
1
1 ----------------------------------------------2 ESR C O UT
F(S)
Gm R
1 --------------------------------------------------------------2 R C C O M P CO M P COMP
FC
F
1
F(S).G(S)
1
bs O
let o
ro P e
FBW 1
du
FBW 2
(s) ct
so Ob RCO MP =
perfect first order decreasing slope until it reaches the zero of the output capacitor ESR. The error amplifier cut off then prevents definitely any further spurious noise or resonance from disturbing the regulation loop. The point where the complete transfer function has a unity gain is known as the regulation bandwidth and has a double interest: The higher it is the faster will be the reaction to an eventual load change, and the smaller will be the output voltage change. The phase shift in the complete system at this point has to be less than 135 to ensure a good stability. Generally, a first order gives 90 of phase shift, and 180 for a second order. In figure 20, the unity gain is reached in a first order slope, so the stability is ensured. The dynamic load regulation is improved by increasing the regulation bandwidth, but some limitations have to be respected: As the transfer function above the zero due the capacitor ESR is not reliable (The ESR itself is not well specified, and other parasitic effects may take place), the bandwidth should always be lower than the minimum of FC and ESR zero. As the highest bandwidth is obtained with the highest output power (Plain line with RL2 load in figure 20), the above criteria will be checked for this condition and allows to define the value of RCOMP, as the error amplifier gain depends only on this value for this frequency range. The following formula can be derived:
te le
ro P
uc d
s) t(
PO U T 2 F B W 2 RL 2 C O U T ----------------- -----------------------------------------------Gm PM A X
W ith:
2 VO U T P O U T 2 = -------------RL 2 1 2
F
And: P M A X = -- LP IL I M F S W : 2 The lowest load gives another condition for stability: The frequency FBW1 must not encounter the second order slope generated by the load pole and the integrator part of the error amplifier. This condition can be met by adjusting the CCOMP value:
R L 1 CO U T C C O M P > -------------------------------------------- 2 6.3 G m R C O M P 2 VO U T PO U T 1 = -------------RL 1 PO U T 1 ----------------PM A X
in the current mode section. A zero due to the RCOMP-C COMP network is set at the same value as the maximum load RL2 pole. The total transfer function is shown as F(s).G(s) at the bottom of figure 20. For maximum load (plain line), the load pole is exactly compensated by the zero of the error amplifier, and the result is a
18/24
W ith: The above formula gives a minimum value for CCOMP. It can be then increased to provide a natural soft start function as this capacitor is charged by the error amplifier current capacity ICOMPhi at start-up.
VIPer53DIP / VIPer53SP
SPECIAL RECOMMENDATIONS As stated in the error amplifier section, a capacitor of 10 nF (minimum value: 8 nF) should always be connected to the COMP pin to insure a correct stability of the internal error amplifier. This is represented on figures 14, 15 and 18. In order to improve the ruggedness of the device versus eventual drain overvoltages, a resistance of 1 k should be inserted in series with the TOVL pin, as shown on figures 14 and 15. Note that this resistance doesn't impact the overload delay, as its value is negligible in front of the internal pull up resistance (about 125 k). SOFTW ARE IMPLEMENTATION All the above considerations and some others are included in a design software which provides all the needed components around the VIPer device for a specified output configuration. This software is available in download on the ST internet site.
bs O
let o
Pr e
du o
(s) ct
so Ob -
te le
ro P
uc d
s) t(
19/24
VIPer53DIP / VIPer53SP
Plastic DIP-8 MECHANICAL DATA
DIM. A A1 A2 b b2 c D E E1 e eA eB L Package Weight 2.92 3.30 Gr. 470 0.38 2.92 0.36 1.14 0.20 9.02 7.62 6.10 3.30 0.46 1.52 0.25 9.27 7.87 6.35 2.54 7.62 4.95 0.56 1.78 0.36 10.16 8.26 7.11 m m. MIN. TYP MAX. 5.33
bs O
let o
Pr e
du o
(s) ct
so Ob -
te le
ro P
uc d
3.81
10.92
s) t(
P001
20/24
VIPer53DIP / VIPer53SP
PowerSO-10TM MECHANICAL DATA
DIM. A A (*) A1 B B (*) C C (*) D D1 E E2 E2 (*) E4 E4 (*) e F F (*) H H (*) h L L (*) (*)
(*) Muar only POA P013P
mm. MIN. 3.35 3.4 0.00 0.40 0.37 0.35 0.23 9.40 7.40 9.30 7.20 7.30 5.90 5.90 1.27 1.25 1.20 13.80 13.85 0.50 1.20 0.80 0 2 1.35 1.40 14.40 14.35 1.80 1.10 8 8 0.049 0.047 0.543 0.545 0.047 0.031 0 2 TYP MAX. 3.65 3.6 0.10 0.60 0.53 0.55 0.32 9.60 7.60 9.50 7.60 7.50 6.10 6.30 MIN. 0.132 0.134 0.000 0.016 0.014 0.013 0.009 0.370 0.291 0.366 0.283 0.287 0.232 0.232
inch TYP. MAX. 0.144 0.142 0.004 0.024 0.021 0.022 0.0126 0.378 0.300 0.374 300 0.295 0.240 0.248 0.053 0.055 0.567 0.565 0.070 0.043 8 8
0.050
10
bs O
let o
od Pr e
H E 1 e
0.25
ct u
B
(s)
E2
so Ob B 0 .10 A B
te le
ro P
uc d
s) t(
0.002
E4
SEATING PLANE DETAIL "A"
A
C D = D1 = = = SEATING PLANE
h
A F A1
A1
L DETAI L "A"
P095 A
21/24
VIPer53DIP / VIPer53SP
PowerSO-10TM SUGGESTED PAD LAYOUT
14.6 - 14.9
B
TUBE SHIPMENT (no suffix)
CASABLANCA MUAR
C
10.8 - 11 6.30
A A
C
0.67 - 0.73 1 2 3 4 5 10 9 8 7 6 0.54 - 0.6
B
9.5
All dimensions are in mm.
1.27
Base Q.ty Bulk Q.ty Tube length ( 0.5) Casablanca Muar 50 50 1000 1000 532 532
A
B
C ( 0.1) 0.8 0.8
10.4 16.4 4.9 17.2
TAPE AND REEL SHIPMENT (suffix "13TR")
REEL DIMENSIONS
Base Q.ty Bulk Q.ty A (max) B (min) C ( 0.2) F G (+ 2 / -0) N (min) T (max) 6 00 6 00 3 30 1.5 13 20.2 24.4 60 30.4
TAPE DIMENSIONS
According to Electronic Industries Association (EIA) Standard 481 rev. A, Feb. 1986 Tape width Tape Hole Spacing Component Spacing Hole Diameter Hole Diameter Hole Position Compartment Depth Hole Spacing W P0 ( 0.1) P D ( 0.1/-0) D1 (min) F ( 0.05) K (max) P1 ( 0.1) 24 4 24 1.5 1.5 11.5 6.5 2
bs O
All dimensions are in mm.
End
let o
Pr e
du o
(s) ct
so Ob -
te le
ro P
uc d
s) t(
All dimensions are in mm.
Start Top cover tape 500mm min Empty components pockets saled with cover tape. User direction of feed 500mm min No components Components No components
22/24
1
VIPer53DIP / VIPer53SP
DIP-8 TUBE SHIPMENT (no suffix)
A
C
B
Base Q.ty Bulk Q.ty Tube length ( 0.5) A B C ( 0.1)
All dimensions are in mm.
20 1000 532 8.4 11. 2 0.8
bs O
let o
Pr e
du o
(s) ct
so Ob -
te le
ro P
uc d
s) t(
23/24
1
VIPer53DIP / VIPer53SP
bs O
Information furnished is believed to be accurate and reliable. However, STMicroelectronics assumes no responsibility for the consequences of use of such information nor for any infringement of patents or other rights of third parties which may results from its use. No license is granted by implication or otherwise under any patent or patent rights of STMicroelectronics. Specifications mentioned in this publication are subject to change without notice. This publication supersedes and replaces all information previously supplied. STMicroelectronics products are not authorized for use as critical components in life support devices or systems without express written approval of STMicroelectronics. The ST logo is a trademark of STMicroelectronics. All other names are the property of their respective owners 2004 STMicroelectronics - Printed in ITALY- All Rights Reserved. STMicroelectro nics GROUP OF COMPANIES Australia - Belgium - Brazil - Canada - China - Czech Republic - Finland - France - Germany - Hong Kong - India - Israel - Italy - Japan Malaysia - Malta - Morocco - Singapore - Spain - Sweden - Switzerland - United Kingdom - United States h ttp://www.st.co m
let o
Pr e
du o
(s) ct
so Ob -
te le
ro P
uc d
s) t(
24/24
|