NEWS
 

STMicroelectronics Unveils New 2-Kbit Long-Range RFID Chips for Multi-Purpose Asset-Tracking Applications

New low cost chips - fully compliant to the latest RFID standards - offer high-speed data-rate capability and unrivaled reading range with optional password security

Click for larger image Geneva, May 30,2006 - STMicroelectronics (NYSE: STM), a worldwide leader in serial non-volatile memories, today announced the availability of two new 2048-bit ‘long range’ RFID memory products that are fully compliant with the ISO/IEC 15693 and ISO/IEC 18000-3 Mode 1 RFID standards for tracking applications.

The use of 2048-bit memories in the LRI2K and LRIS2K has been driven by the demand for increased memory in cost-sensitive general-purpose RFID applications requiring both data storage and security. The new devices are particularly suited for market segments such as access control, library automation, and supply-chain management, as well as for anti-counterfeiting of sensitive products, such as pharmaceuticals and high-value items.

One of the devices, the LRIS2K, also offers an innovative password feature for additional protection. Each memory block in the device can be individually ‘profiled’ using one of three available passwords. Security profiling brings a high level of flexibility and allows different parts of the supply chain to control different segments of memory.

Both the LRI2K and LRIS2K provide 2 Kbits of electrically erasable user memory (EEPROM), with an on-chip RF interface operating at the standard HF (high-frequency) 13.56MHz carrier frequency. Offering high-speed data-rate capability, an application reading range of up to 1.5m, and the advantages offered by 13.56MHz-based RFID technology, such as high reliability and low RFID reader cost, the two devices are highly suited for item-level tagging, whenever security, inventory speed, and tag size are relevant requirements.

Additionally, due to their high on-chip tuning capacitance, the LRI2K and LRIS2K also allow the design of very small antennas, thus saving space and making them suitable for use with small objects, such as medicine bottles in the pharmaceutical industry.

“These two new products are an important addition to ST’s high-frequency RFID product range,” said Francis Dell’ova, ST’s RFID Business Unit Manager. “They confirm our commitment to offer a wide HF and UHF product portfolio and meet increasing market demands for devices with larger user memories and more security features.”

Both devices offer 2048 EEPROM user bits with block lock capability (32 bits per block), a 64-bit Unique Identification number (UID) associated with the ISO-compliant anti-collision mechanism, internal tuning capacitor, and KILL function. Memory is organized as 64 blocks of 32 bits, and each block can be individually write-protected using a Lock command that prevents any subsequent modification of the data. In addition, a 64-bit read-only UID block and an 8-bit Application Family Identifier code uniquely identify the device, and an 8-bit Data Storage Family Identifier register stores data for the Anti-Collision mechanism. Thanks to their unrivaled reading range, an Electrical Article Surveillance (EAS) feature can be implemented for point-of-sale applications.

Built using ST’s highly reliable and mature CMOS technology with embedded EEPROM, and uniquely featuring 40-year data retention, the LRI2K and LRIS2K are well-suited to address high-volume cost-driven markets, as well as reliability-sensitive segments such as automotive or avionics.

Samples of the LRI2K and LRI2SK are available now, with volume production expected in July 2006. Both devices can be delivered in various formats including thin un-sawn wafers, sawn and bumped wafers, ultra-thinMLP8 2x3mm package, or as inlays. LRI2K pricing is US$0.095 in volume quantities.

Please click here for a high-resolution photo

Further information is available at www.st.com/rfid

About ST’s Memory Product Group (MPG)
STMicroelectronics offers the industry's widest range of semiconductor storage solutions for leading applications. The Company is a major supplier of non-volatile memories, including NOR and NAND Flash, EPROM/EEPROM, and Serial Flash. ST’s memory product portfolio also features a wide array of RFID ICs, as well as the most complete range of secure microcontrollers and System-on-Chip solutions for all major Smartcard application segments.


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2005, the Company's net revenues were $8.88 billion and net earnings were $266 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2006





Should you require more information, please select the appropriate contact from the "Related Topics" menu.