NEWS
 

STMicroelectronics Delivers Wide Bandwidth, CMOS Input Op-Amps That Go Easy on Battery Consumption

Click for larger image Geneva, March 09,2007 - STMicroelectronics (NYSE: STM), one of the world’s leading suppliers of operational amplifiers, today introduced two new families of rail-to-rail high Gain Bandwidth Product (GBP) op-amps that feature an excellent speed-to-current consumption ratio and come in space-saving packages to address sensor signal conditioning as well as battery-supplied and compact portable applications.

The TSV911/2/4 family offers an 8MHz gain-bandwidth product and is unity-gain stable for capacitive loads up to 200pF. The other family, the TSV991/2/4, offers a 20MHz gain-bandwidth product for gain of 3 or above.

Operating from 2.5V to 5.5V, all the devices consume only 780 microamps at 2.5V supply voltage. The op-amps’ low power, together with their improved precision and the reduced die size, make them ideal for battery-powered applications where space board and low-current consumption are major priorities.

Other key features of all op-amps include an ultra-low input bias current of 1pA and 5kV or better internal protection that protects against electrostatic discharge (ESD), minimizing handling and fabrication risks.

All of the amplifiers are characterized for the -40 to +125 degree C temperature range and are available in SOT23-5, SO8, MSO8, TSSOP14, and SO14 ECOPACK® packages.

In production now, in quantities of 1000 pieces, the TSV911/TSV991, TSV912/TSV992, and TSV914/TSV994 cost $0.36, $0.62, and $0.96, respectively.

Further information is available at: http://www.st.com/stonline/products/families/amplifiers_linear/opamps/tsv91x.htm

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2006, the Company's net revenues were $9.85 billion and net earnings were $782 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2007




ECOPACK® is an ST trademark


Should you require more information, please select the appropriate contact from the "Related Topics" menu.