NEWS
 

STMicroelectronics Advances Memory Manufacturing Technology to Deliver 512-Kbit Serial EEPROMs in 2 x 3mm Package Outline

New memories promote scaling of designs to 512-Kbit density, with high-speed SPI and I2C interfaces

Click for larger image Geneva, July 01,2009 - STMicroelectronics (NYSE: STM), the world’s largest supplier of serial EEPROMs, has leveraged its advanced non-volatile memory technology to deliver an industry first with two new 512-Kbit devices that offer the highest density memories available in the industry-standard 2 x 3 x 0.6mm 8-pin Micro Leadframe Package (MLP). Pin compatibility with memories of lower density allows designers to upgrade products quickly and efficiently by changing devices without redesigning the board.

Serial EEPROMs deliver non-volatile storage in low-pin-count packages, suitable for many consumer, industrial, medical and communication products. The devices’ built-in byte-mode erasing capability allows easy parameter update; and 128-byte page write, together with 5ms write time, results in rapid programming of assembled boards on the production line.

In addition, with read current as low as 2mA and stand-by current less than 5 microamps, the new memories save energy in power-sensitive equipment such as battery-powered personal media devices or professional portable instruments. The wide operating-voltage range, from 1.8V to 5.5V, allows the same device to be used across many applications and product variants. Both types are also offered with an operating range of 2.5V to 5.5V.

The new devices are the M95512 featuring a 20MHz SPI port, and the M24512 with an I2C interface supporting 400kHz Fast-mode or 1MHz Fast-mode Plus. With its 20MHz SPI interface, the M95512 achieves data transfer speeds equal to the fastest serial EEPROMs currently available.

Both devices are also available in industry-standard SO-8 and TSSOP-8 packages. These new devices complete a full family of EEPROMs, delivered in MLPs from 2 to 128 and 512-Kbit densities. A 256-Kbit device will be available in Q4 2009.

The M95512 and M24512 in MLP 2x3 packages are available in mass production and are priced from $0.80 for high-volume orders.

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2008, the Company's net revenues were $9.84 billion. Further information on ST can be found at www.st.com.
Information last updated Jun 2009





Should you require more information, please select the appropriate contact from the "Related Topics" menu.