NEWS
 

STMicroelectronics’ Silicon Carbide Schottky Diodes Receive Prestigious ‘Electron d'Or 2009’ Award from Electronique Magazine

STPSC806D and STPSC1006D SiC Schottky diodes recognized as best ’power conversion’ product

Geneva, June 18,2009 - STMicroelectronics (NYSE: STM), a world leader in power semiconductors, today announced that it has been awarded an “Electron d’Or 2009” by Electronique Magazine in the ‘power conversion’ category, for its new family of silicon-carbide (SiC) Schottky diodes. The winner in each award category is determined by an independent jury of recognized experts in the electronics industry, and is selected from products released in the previous year.

“The prestigious ‘Electron d'Or 2009’ award is an important validation of ST’s commitment to provide reliable and high-performance product for power applications,” said Ricardo de Sa Earp, General Manager of the ASD & IPAD product division (Application Specific Devices and Integrated Passive and Active Devices), STMicroelectronics. “We greatly value the recognition from Electronique and the panel of experts from the French electronics industry and are delighted with its selection of our SiC Schottky diodes.”

 

ST’s STPSC806D and STPSC1006D silicon-carbide diodes employ the latest substrate technology to eliminate power-supply switching losses, improving efficiency and reducing heat. While ordinary silicon diodes used in switched-mode power supplies lose up to 1% efficiency by not turning off immediately, SiC technology is able to deliver greater efficiency because no reverse recovery charge accumulates during the diode’s normal conduction period. By eliminating this reverse recovery charge, SiC Schottky diodes have much lower switching losses across the board, leading to higher efficiency and lower heat dissipation.


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2008, the Company's net revenues were $9.84 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2009





Should you require more information, please select the appropriate contact from the "Related Topics" menu.