![]() | ||
|
| ||
STMicroelectronics Introduces Versatile High-Definition Set-Top-Box Platforms at MEDC 2006
| ||
This open Windows CE platform is a complete reference design that accelerates the development cycle and helps set-top box manufacturers deliver their products to market faster. In addition, the platform lowers bill-of-materials costs. Taking full advantage of Microsoft’s recently launched Windows CE 5.0 Networked Media Device Feature Pack, ST’s base platform represents a ready-to-go solution that lets manufacturers expand their range of STB products by capitalizing on their previous efforts while benefiting from ST’s clear roadmap in powerful and market-leading high-definition Systems-on-Chip products. Thanks to the extraordinary level of integration of the STB7109 high-definition decoder, this platform delivers a cost-effective solution for consumer products requiring high-quality video and audio, high-speed interfaces, and secured connectivity. The STB reference design embeds a high-speed Ethernet interface that enables the STB to be a central part of the home network and adds greater connectivity through the availability of USB 2.0 host port and a serial ATA (SATA) port. Additionally, the design ensures secure connectivity through a high-speed digital copy-protected HDMI (High-Definition Multimedia Interface), allowing simple digital connection to any HD-ready flat panel display. The new platform supports:
“Customization based on the Networked Media Device middleware and DVR engine found in the Windows CE 5.0 Networked Media Device Feature Pack, coupled with ST’s highly integrated system-on-chips help streamline development, makes it easier for consumer-electronics developers to focus on product differentiation and innovation to build their next generation of cutting-edge networked media devices and IP set-top boxes,” said Kevin Dallas, general manager, Windows Embedded at Microsoft. ST’s platform is a standard, complete and reusable high-definition solution, making it ideal for Networked Digital products and future HD-DVD (High-Density DVD) players. ST will supply these new platforms to consumer-electronics manufacturers to enable fast market delivery of appliances such as IP set-top boxes, Networked Media Devices, HD-DVD players, digital video recorders (DVRs), and more. “Working with Microsoft, we have taken a major step toward providing consumer electronics manufacturers with a stable and cost-effective platform for the rapidly growing networked-DVR and IP-STB market,” said Christos Lagomichos, Corporate Vice President and General Manager of the Home Entertainment Group at STMicroelectronics. “Foreseeing the booming of the next generation of high-definition media, we are also closely paying attention to HD-DVD technology and already preparing for the next evolutionary step of this platform.”
About ST’s Home, Personal, Communication Group (HPC)
|
| ||||||||||||||||||||
| |||||||||||||||||||||