NEWS
 

STMicroelectronics Announces Dual DVB-S2 Demodulator to Enable Cost Effective HDTV Watch-and-Record DVR Satellite Set-Top Boxes

High level of integration, 90nm technology and fully supported reference designs ensure cost-efficient design and manufacture

Click for larger image Geneva, February 28,2007 - STMicroelectronics (NYSE: STM), the world’s leading supplier of silicon chips for set-top boxes (STBs)*, today announced a dual DVB-S2 satellite TV demodulator chip, intended for STBs that offer the viewer the ability to watch one standard or high-definition TV channel while recording another. The new multi-standard STV0900 provides in a single package the functionality of two of ST’s established STB0899 demodulators, significantly reducing STB complexity and manufacturing cost.

The STV0900 is built using state-of-the-art 90nm process technology, ensuring lower cost through increased integration, while reducing power consumption. The power requirement is intrinsically much lower than for a twin STB0899 solution, in addition further software-based power management features are built-in to help STB manufacturers obtain green accreditation. Careful attention to the overall Bill of Materials (BOM) has led to optimum integration resulting in lower costs coupled with a high level of design flexibility.

Like the STB0899 demodulator, the STV0900 supports both the latest DVB-S2 specification and the original DVB-S standard, which has been in use for more than ten years by satellite operators worldwide. The dual standard capability means that STB manufacturers can use the STB0899 and the STV0900 in ‘DVB-S2-ready’ set-top boxes to provide a seamless upgrade path for viewers as more services become available. Both products support normal QPSK (quadrature-phase-shift-keying) and 8PSK modulation, as well as the DVB-S2 pilot processing that enables more robust reception.

DVB-S2 increases the capacity of satellite communications links by 30% compared to the DVB-S standard – close to the theoretical performance limit – and in combination with other new coding and satellite technologies enables the effective deployment of high data-rate applications such as high definition TV (HDTV), broadband Internet and interactive services, as well as a significant increase in the number of standard channels that can be broadcast in a conventional transponder.

The dual demodulator is designed to integrate seamlessly with silicon tuners such as ST's STB6100, which replaces complex traditional discrete tuner circuitry and eliminates the need for specialist RF design expertise. For downstream processing it offers cost-saving glueless interfaces to the broad range of MPEG-2 and H.264/VC-1 decoders in ST’s standard and high definition OMEGA decoder family. ST provides STB manufacturers a major step for a DVB-S2 Watch-and-Record set-top box, with highly competitive pricing. Software drivers and reference designs with full documentation are provided as part of the development environment.

Support is included for two DiSEqC 2.0 (Digital Satellite Equipment Control) interfaces, a widely used protocol that allows a satellite STB to control peripheral devices connected to the coaxial cable. Extensions to the DiSEqC open standard, proposed by ST and adopted by the industry, enable the STB to manage the rooftop LNB (Low-Noise Block) and simplify installations needing to handle more than one user channel. Up to eight user channels can be combined onto a single coaxial cable eliminating the need for multiple cables or multi-core cables.

The dual demodulator is packaged in a 128-pin exposed pad LQFP, 14 x 14mm, quad flat pack, with 0.4mm pitch. The STV0900 kit – with tuners – is priced at less than US$10.00 in volumes of 100,000 units. Volume production is planned for the first half of 2007.

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2006, the Company's net revenues were $9.85 billion and net earnings were $782 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2007




* inStat MPEG report "MPEG Video ICs: Transitioning to H.264" – July 2006


Should you require more information, please select the appropriate contact from the "Related Topics" menu.