ST Life.augmented

eSTore

Introducing the eSTore dedicated initially to offer the convenience of buying boards and development kits directly from our site. Supported by our logistics and order fulfillment partner, the eSTore makes possible a quick and simple access to our available inventory of development kits and boards.

  • STM32-JAVA
    STM32Java development environment for STM32

    Take advantage of the benefits of object-oriented programming in Java to develop general purpose STM32 applications, in particular, applications with a smartphone-like look and feel graphical user interface (GUI) with STM32Java.

    All of the well known advantages of the Java design concepts are available: interface versus implementation, inheritance and composition, polymorphism, garbage collector (GC), multi-tasking, etc.

    Software productivity, agility, scalability and security are improved compared to traditional developments in C/C++ code.

    Applications can mix C code (legacy control/command code for example) with code developed in Java. STM32Java provides efficient mechanisms to interface the 2 worlds, Simple Native Interface to call C functions from Java code and Shielded Plug to exchange data between the 2 worlds.

    STM32Java provides everything required to easily and very quickly develop feature-rich GUIs, relying on the Model-View-Controller (MVC) triad, the best known solution to designing flexible and easy to maintain GUIs.

    Running STM32Java programs requires features that are embedded on special STM32 MCU series. There are two sets of special part numbers enabled for Java: MCU part numbers ending with the letter ‘J’ (for mass production) and MCU part numbers ending with the letter ‘U’ (can only be ordered as samples).

    For more information, visit www.stm32java.com.

    ... See More

    Price:  $2572.50

    Availability:  1

    Orderable Qty:  1

    Buy Direct
  • STM3220G-JAVA
    STM32 F2 series Java evaluation kit

    The STM3220G-JAVA kit is a complete platform to evaluate the development of embedded applications in Java for the STM32 F2 series microcontrollers.

    The kit is composed of the STM3220G-EVAL evaluation board and a DVD ROM which contains an evaluation version of the STM32Java software development kit based on MicroEJ®.

    MicroEJ® is based on the Eclipse™ IDE and provides extended features for using Java in embedded systems to design and deploy embedded Java applications, simulate embedded Java applications on PCs and perform automated tests.

    The main limitations of the evaluation version are 3 months of use from the first launch and 1 hour of runtime.

    A Java demo is programmed in the STM32F207IGH6 microcontroller on the evaluation board.

    For more information, visit www.stm32java.com.

    ... See More

    Price:  $341.77

    Availability:  9

    Orderable Qty:  1

    Buy Direct
  • STM3240G-JAVA
    STM32 F4 series Java evaluation kit - with STM32F407IG MCU

    The STM3240G-JAVA kit is a complete platform to evaluate the development of embedded applications in Java for the STM32 F4 series microcontrollers.

    The kit is composed of the STM3240G-EVAL evaluation board and a DVD ROM which contains an evaluation version of the STM32Java software development kit based on MicroEJ®.

    MicroEJ® is based on the Eclipse™ IDE and provides extended features for using Java in embedded systems to design and deploy embedded Java applications, simulate embedded Java applications on PCs and perform automated tests.

    The main limitations of the evaluation version are 3 months of use from the first launch and 1 hour of runtime.

    A Java demo is programmed in the STM32F407IGH6 microcontroller on the evaluation board.

    For more information, visit www.stm32java.com.

    ... See More

    Price:  $341.77

    Availability:  3

    Orderable Qty:  1

    Buy Direct
Feedback Form
Customer Feedback