STMicroelectronics Launches New Dual-Interface EEPROM Enabling Remote Access to Electronic Device Parameters
New RFID-compatible EEPROMs simplify lifetime management and enable new features and capabilitiesThe M24LR64 is an EEPROM memory with a standard I2C serial interface, providing communication with most microcontrollers or ASICs, and also a standard ISO15693 RF (radio frequency) interface for wireless communications with RFID readers. The ISO15693 standard is passive RFID technology, which gathers both the energy and the data from the RF system. No power is required to operate the M24LR64 in RF mode, which enables on-board energy savings and provides easy and convenient remote access to electronic product parameters.
“This highly innovative ability to program or read a memory wirelessly, as well as electrically, will provide tremendous added-value to our customers, enabling highly flexible supply-chain management and also stimulating new types of products with powerful features and capabilities,” said Benoit Rodrigues, General Manager, Memories Division, STMicroelectronics. “Moreover this new memory is compatible with existing RFID equipment, thereby delivering a wide range of solutions and an accessible technology to product manufacturers”
Based on two industry-standard interfaces, the new dual-interface product line provides a link between the operation of electronic devices and the RFID world. This will enable new types of products, including those requiring asset tracking, data collection, diagnostics, or traceability, such as medical devices, industrial equipment, and automotive electronics. Computer peripherals and consumer products will take advantage of the M24LR64 feature set for easy and convenient parameter and regional setting update, even when the device is in its package seal. Also, RFID systems requiring additional monitoring, such as cold-chain verification, will also benefit from the high memory density of the M24LR64.
The M24LR64 has a 64-Kbit capacity for storage of program code, product parameters, serial numbers, calibration data, or event-log data. Its RF ISO15693 interface can be accessed by a wide range of RF readers, covering hand-held devices, pad antennas, gate systems and tunnel readers. The memory also communicates with the host system via an industry-standard I2C interface operating at 400kHz from 1.8 to 5.5V. It also comes with a unique and flexible 32-bit password protection scheme to protect the application from unauthorized tampering or to prevent unexpected access to memory.
The Dual-Interface EEPROM products can be used with either on-board or off-board antenna types in a variety of form factors, allowing product designers to optimize aspects such as overall dimensions, communication range, and pc-board complexity. The M24LR64 is available in TSSOP-8, SO-8, and MLP 2 x 3 packages, or as bare die, at prices from $0.90 for orders of 1000 pieces. Sampling has already begun, with volume production scheduled for Q2 2010. ST plans to introduce additional members of the Dual-Interface EEPROM family in the second half of 2010.
Click here for the high-resolution photo
About STMicroelectronics
STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2009, the Company's net revenues were $8.51 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2010