STMicroelectronics Unveils 3D-Ready Set-Top-Box IC Enabling TV Providers to Realize Consumer-Friendly Content Convergence
STi7108 system-on-chip dramatically increases performance and features to deliver next-generation 3D graphics and TV experiences while increasing set-top-box functionality, versatility and ease of use“The STi7108 is the first in ST’s third generation of high-definition chips that will provide the end user with a really exciting 3D HDTV user experience, thanks to its unprecedented CPU performance allowing smooth web experiences,” said Philippe Lambinet, Executive VP for the Home Entertainment and Displays Group, STMicroelectronics. “It also has market-leading energy efficiency due to its low power configurable architecture, and low power manufacturing process.”
The new STi7108 has dual ST40-300 CPU host processors linked to a 256K L2 cache giving up to 2000 DMIPS performance and a total of 4000 DMIPs for flexible support of demanding AV, security and connectively applications. A 3D graphics engine enables a new class of user interfaces, supports innovations such as 3D Electronic Program Guide (EPG), and enables advanced Internet content and high-performance gaming on the STB. It is the first set-top box IC in the market to combine 3D graphics, Ethernet, USB and e-SATA interfaces to connect Internet devices, DVR storage or external Flash or hard-disk (HDD) drives.
The STi7108 utilizes the ARM® Mali-400 graphics processor, the only embedded graphics processor which has demonstrated compliance with the Khronos OpenGL ES 2.0 specifications at HD resolutions, to deliver a powerful 3D experience.
“The STi7108 builds on the broad collaboration between STMicroelectronics and ARM on high-performance graphics-processor architectures,” said Lance Howarth, general manager and EVP, ARM Media Processing Division, “The ARM Mali-400 graphics processor opens up new levels of user experience enabling STMicroelectronics to provide compelling 3D gaming and rich 3D user interfaces at 1080p resolution, as well as delivering a seamless composition of graphics and video for the next wave of web-based interactive services.”
The STi7108 is able to decode video in industry-standard formats, including H.264, MPEG2, VC-1 or WMV9 Internet video, and MPEG4 part 2, up to high-definition resolutions 1080p 50/60 simultaneously with 1080i/720p picture-in-picture or mosaic formats. The device has flexible memory-interface options offering dual 32/16-bit LMI DDR2/ DDR3 at 1066MHz.
The device provides inputs for up to six transport streams, and provides full-motion HD 3DTV over HDMI 1.3 with HDCP copy protection. Support for content sharing, according to the Digital Living Network Alliance (DLNA) specification, will also allow use in next-generation Blu-ray and HD media players.
Together with other integrated processors, including an audio processing subsystem and 2D-graphics handling, the STi7108 allows a significant leap in performance over products currently in mass production, thereby providing increased scope for STB designers to create multimedia value-added features and services to differentiate their products in the marketplace.
ST will demonstrate the STi7108’s potential at ST’s private suite for customers at the Consumer Electronics Show (CES), Las Vegas, January, 7-10, 2010. Volume production is scheduled to start early in 2010.
Click here for the high-resolution photo
About STMicroelectronics
STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2009, the Company's net revenues were $8.51 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2010
ARM is a registered trademark of ARM Limited. Mali is a trademark of ARM Limited. All other brands or product names are the property of their respective holders.