ST Life.augmented

新闻稿

Digital Compasses from STMicroelectronics Lead the Way in the Tiniest Phones and Tablets

Geneva /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications and the leading supplier of MEMS (Micro-Electro-Mechanical Systems) for consumer and portable applications 1, today expanded its sensor portfolio with an ultra-compact, high-performance e-compass module. The integration of motion and magnetic sensing in a tiny 3x3x1mm package opens new possibilities for advanced navigation and location-based services in ever-sleeker portable consumer devices.

The ST e-compass’ ability to provide accurate heading information - indicate the direction in which a person or vehicle is moving - enables a wide range of applications, including pedestrian dead-reckoning, map/display orientation, and direction finding. Tied to location-based service apps, compassing capabilities can help consumers identify and retrieve information on nearby points of interest, such as historical or geographical points of interest, restaurants or shops, by simply pointing their GPS-equipped mobile devices in the direction of the object concerned.

Reducing the size by 60% over devices currently in production, ST’s new digital compasses have effectively shrunk to the size of single-function, stand-alone motion sensors. At the same time, the new modules boast superior sensing precision with extended magnetic-scale range and minimized measurement noise. The significant size and performance benefits enable OEMs to add new compelling functionality in mobile gadgets while keeping pace in the miniaturization race.

The LSM303D module provides extremely accurate output across full-scale ranges up to ±16g (linear acceleration) and ±12 Gauss2 (magnetic field).The device embeds a temperature sensor and a programmable FIFO (first-in first-out) memory block for advanced motion recognition and smart power management. Advanced features include two programmable interrupt signals that enable immediate notification of motion detection, click/double-click events, and other conditions.

Digital compasses are becoming a standard feature in tablets and GPS mobile phones, as well as finding their way into gaming, cameras and other consumer devices. According to IHS iSuppli, a leading market research firm, global demand for digital compasses is rising rapidly and is expected to grow from 270 million units in 2010 up to 1.58 billion in 2015.

ST’s LSM303D e-compass module will start mass production in Q3 2012. Unit pricing is $1.8 for volumes in the range of 1,000 pieces. If your company has a high-volume need, please contact your ST sales office.

For further information on ST’s complete MEMS portfolio see www.st.com/mems

Click here for the high-resolution photo

About STMicroelectronics:
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power technologies and multimedia convergence applications. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.
In 2011, the Company’s net revenues were $9.73 billion. Further information on ST can be found at www.st.com.

1 IHS iSuppli: H2 2011 Consumer and Mobile MEMS Market Tracker, February 2012 
2 Gauss (G) is the unit of measurement of magnetic flux density, or the magnitude of a magnetic field at a given point. The magnetic field magnitude measured at the surface of the Earth is about half a gauss.

Feedback Form
Customer Feedback