ST Life.augmented

新闻稿

STMicroelectronics Drives Extra Performance and Value into Entry-Level 32-bit Microcontrollers

STM32 Value High Density series offers MCUs with up to 512 Kbytes of Flash and 144 pins, supporting evolution of cost-sensitive end products

Geneva /

As manufacturers seek to differentiate their products with new features that add value for customers, STMicroelectronics (NYSE: STM), a world leader in microcontrollers, is helping designers meet higher product-performance targets at ultra-competitive prices by introducing its STM32 Value High-Density microcontrollers. These new microcontrollers offer extra program memory and on-chip functions, extending the range of the STM32 Value Line family to include devices from 16 to 512 Kbytes of embedded Flash, providing a scalable alternative for cost-sensitive designs.

Microcontrollers are at the heart of today’s consumer products, such as domestic appliances, multimedia equipment and mobile devices. These products are constantly increasing in performance to cope with progressively larger and more complex software applications. ST’s STM32 ARM Cortex-M3 based microcontrollers have been among the first in the market to use an advanced 32-bit core to increase performance over proprietary 16-bit devices at a competitive price. The family now has over 140 pin- and software-compatible variants covering a wide price/performance spectrum and offering market-optimized options such as built-in USB support and access to the extensive STM32 ecosystem of development tools.

“The latest STM32 Value High Density devices build on the STM32 ARM Cortex-M3 based Value Line to set an even more exciting price-competitive entry point to 32-bit microcontroller design,” said Michel Buffa, General Manager of ST’s Microcontroller Division. “Cost-sensitive applications can now benefit from Flash memory density as high as 512 Kbytes for program and data storage, as well as extra integrated features.”

Among the new enhanced features of the family is an external memory interface, which can address numerous types of external code or data memory. The interface also supports a parallel interface mode for LCD screens with embedded controllers. This responds directly to the growing use of graphical LCD panels in products such as washing machines, audio/DVD players and RF remote controls. In addition, extra package options, with up to 112 I/O pins, help designers manage more intensive communications between the microcontroller and other system components, such as sensors, status indicators and wireless subsystems. STM32 Value High Density devices also target professional applications, such as metering, motor control and user-interface control in industrial and medical equipment.

Major features of STM32 Value High Density Line, include:

  • 24MHz ARM Cortex-M3 based processor; 1.25 DMIPS/MHz
  • 256 to 512 Kbytes Flash
  • External memory interface for larger application code storage
  • 24 to 32 Kbytes SRAM
  • 12 x 16-bit timers including motor-control timer
  • 12-bit ADC with 1.2us conversion time
  • LCD parallel interface support via external memory interface
  • 64-pin to 144-pin package options
  • Access to the extensive STM32 ecosystem of development tools

STM32 Value High Density microcontrollers are priced from $2.18 in the 64-pin LQFP64 package for 256 Kbytes and $4.33 in the 144-pin LQFP144 package for 512 Kbytes, for quantities of 10,000 units. Further pricing options are available for larger quantities.

Click here for the high-resolution photo

About STMicroelectronics
STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2009, the Company's net revenues were $8.51 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2010

 
Feedback Form
Customer Feedback