ST Life.augmented

新闻稿

STMicroelectronics Unveils Ultra-Compact Multi-Sensor MEMS Module with Programmable Motion-Recognition Capabilities

The new iNEMO® device packs 6 degrees of freedom and embedded intelligence in about 10mm3

Geneva /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications and the leading supplier of MEMS (Micro-Electro-Mechanical Systems) for consumer and portable applications 1, today announced a miniature 6-axis sensor device with custom motion-recognition capabilities. ST’s latest iNEMO® inertial module enhances user experience and motion-sensing realism in today’s space-constrained and power-hungry portable consumer devices and shortcuts the path to wearable sensor applications in sports, fitness and healthcare diagnostics.

The LSM330 module houses a 3-axis digital gyroscope and a 3-axis digital accelerometer with two embedded finite state machines – programmable blocks that enable custom motion recognition inside the module. Programmable state machines enable the identification of specific motions or gestures and initiate associated actions or applications, such as switching on an augmented-reality view of a near-by object by moving your phone with a specific gesture. Integrated processing capability in MEMS sensors helps decrease power consumption in battery-hungry portable devices and brings more freedom and flexibility to the design of motion-enabled consumer electronics.
 
ST’s newest inertial module detects acceleration up to 16g and angular rate up to 2,000 dps along the pitch, roll and yaw axes 2. The integration of high-resolution linear- and angular-motion sensing in a single device increases system robustness and the advanced module design ensures superior thermal and mechanical stability. The LSM330 multi-sensor module targets a wide range of applications that include wearable sensor applications, motion-activated user interfaces in phones and tablets; motion detection and map-matching for indoor/outdoor navigation, augmented reality and other location-based services. 

Addressing power constraints in battery-operated portable devices, the module includes power-down and sleep modes and an embedded FIFO (first-in first-out) memory block for smarter power management. In addition, it can operate with any supply voltage over the range of 2.4 to 3.6V.

Fully software-compatible with ST’s latest-generation 3-axis digital accelerometers (LIS3DSH) and gyroscopes (L3GD20), the new iNEMO module makes it easy for customers using ST’s single-function sensors to upgrade their designs, reducing the board size, number of external components, and overall application system complexity.

Housed in an ultra-compact 3x3.5x1mm LGA package, the LSM330 6-degrees-of-freedom module will start sampling by the end of Q4 2012 Unit pricing is $4.15 for volumes in the range of 1,000 pieces. If your company has a high-volume need, please contact your ST sales office.

For further information on ST’s complete MEMS portfolio see www.st.com/mems

Click here for the high-resolution photo

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power technologies and multimedia convergence applications. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.
In 2011, the Company’s net revenues were $9.73 billion. Further information on ST can be found at  www.st.com.

1 IHS iSuppli: H2 2011 Consumer and Mobile MEMS Market Tracker, February 2012
2 Pitch, roll and yaw are types of angular motion: yaw is rotation around the vertical axis; roll is rotation around the front-to-back axis and pitch is the rotation around the side-to-side axis.

Feedback Form
Customer Feedback