ST Life.augmented


STMicroelectronics Exhibits its Latest Solutions for Revolutionary Healthcare Applications at MEDTEC Japan 2013

April 24 (Wed) – 25 (Thu), 2013: Tokyo Big Sight (ST Booth: No.3314)
Tokyo /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronic applications, will exhibit its latest solutions for healthcare applications at MEDTEC Japan 2013. The field of healthcare is recognized as an area of fast-paced growth due to factors such as an ageing population, soaring medical costs, health consciousness, and prevention of infection spreads. At its booth, ST will demonstrate various solutions targeting applications for checking the state of a person’s health and diagnosing their conditions.


Demos at ST’s booth include:

Body Gateway
Remote monitoring can help understand the state of an elderly person’s health and of patients with cardiovascular disease in a timely and accurate fashion. ST’s “body gateway” remote monitoring solution is built around a wearable device integrating multiple components such as a microcontroller, an acceleration sensor, an analog front-end IC, communication IC, and a power supply IC. The device connects to a network and allows remote monitoring of the wearer’s biometric information, including heart-beat, pulse, and breathing-rate abnormalities and collapses, making the solution suitable for use in elderly homes and hospital wards. The ST demonstration at MEDTEC will showcase the collection of biometric information using a prototype wearable device and display of the information on a tablet computer.

Veredus Laboratories, a majority-owned subsidiary of ST, will present a multiplexed molecular diagnostic solution specifically designed for decentralized laboratories. The lab-on-chip, a microchip-based disposable device integrating Polymerase Chain Reaction and a DNA microarray, is able to simultaneously detect multiple pathogens and DNA mutations in a single test. This makes it particularly suited for the detection of the main influenza viruses, tuberculosis with its drug resistances, and other germs which would require multiple and complex tests to be identified. Veredus’ high-accuracy molecular test can detect pathogens in a very short time and due to its portability and ease of use, it can be deployed in a variety of locations contributing to preventing the spread of pathogens that cause numerous types of conditions.

Pulse Generator for Ultrasound Imaging
Against the backdrop of a demand for swift diagnosis, there is a growing need for the miniaturization of ultra-high-frequency devices from healthcare organizations that are unable to accommodate large-size devices and for situations outside of medical facilities such as house visits or sports facilities. ST will display its STHV748 high-performance pulse generator designed for ultrasound imaging applications. With embedded peripheral circuits such as a T/R switch (transmission/receiving switch) and noise blocking diodes, a maximum output of ±90V, a maximum operating frequency of 20MHz, and high-precision pulse-signal transmission control, ST’s pulse generator contributes to the accurate visualization of a person’s internal information.

ST solutions showed at MEDTEC also include the dual-interface EEPROM development kit for personal healthcare devices, ASICs for medical devices, and real-time PCR solutions for molecular diagnosis.

ST will be exhibiting at MEDTEC Japan 2013 from Wednesday, April 24, through Thursday, April 25, at the Tokyo Big Sight, Booth No.3314.

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power and automotive products and embedded processing solutions. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.

In 2012, the company’s net revenues were $8.49 billion. Further information on ST can be found at

Feedback Form
Customer Feedback