ST Life.augmented

新闻稿

Latest Cool Bypass Devices from STMicroelectronics Unlock Extra Solar Energy and Cost Savings

Cool bypass devices minimize internal energy losses to route high-quality, high-efficiency solar power

Geneva /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, has introduced its latest-generation high-efficiency cool bypass switches family for photovoltaic modules, enabling an even higher percentage of harvested energy to reach end users and further reducing the cost per Watt of renewable energy. Boasting the industry’s smallest dimensions, ST’s bypass devices can be integrated directly in the photovoltaic module, reducing both installation complexity and cost for consumers.

ST’s cool bypass devices combine efficient power switching and intelligent control in a single chip to compensate for the variable effects of hotspots and shadows on the solar panel surface. The new devices can save up to 1% of the energy produced and normally lost through conventional bypass diodes; in a 1MWp solar array farm this loss could provide the total annual electricity consumption of two average European households 1

ST’s latest cool bypass devices feature new technology and control techniques that minimize energy losses in all operating modes, by ensuring the integrated power switch has ultra-low leakage current when turned off and very low voltage drop when turned on. Thanks to the reduced power losses, a further advantage of these devices is a reduction in typical operating temperature, leading to increased reliability and longer lifetime. Solar installations can achieve a lifespan of 25 years using this device.
 
The SPV1512 and SPV1520 cool bypass switches are rated for operation up to 12 V and 20 V respectively. Other voltage options (up to 120 V) will be introduced in late 2012 and early 2013 in industry-standard D2PAK and TO-220AC packages.
 
The SPV1512 is available in an extremely small 5 x 6 x 0.75mm-high VFQFPN package, which enables the bypass circuitry to be laminated on the back of each solar panel. This simplifies design and installation by eliminating large numbers of junction boxes and interconnects, and can reduce the cost of each panel by around 5%.

Renewable Energy Efficiency and Climate Change
Electricity generation using solar panels (solar photovoltaic) is the fastest growing renewable energy technology of the past decade according to the International Energy Authority (IEA), which states that total installed capacity is now around 65 Gigawatts.

The IEA’s 2012 Energy Technology Perspectives (ETP 2012, www.iea.org/etp) calls for ongoing investment in solar photovoltaic to reduce system costs and encourage growth in capacity. This investment is needed to help cut more than 50% of energy-related CO2 emissions by 2050, compared to 2009 levels, if global temperature rise is to be kept within 2 °C. 

“As installed photovoltaic capacity continues to rise, efficient and cost-effective power solutions such as our cool bypass switches will make an increasingly significant contribution to saving energy and reducing greenhouse gas emissions,” said Matteo Lo Presti, General Manager of ST’s Industrial and Power Conversion Division. 
 
Major features of SPV15 family:

  • 100mV forward voltage drop
  • 10µA leakage current in reverse polarity
  • Very high resilience to electrical overstress
  • Low operating temperature for increased lifetime
  • High efficiency

The 12V SPV1512 in DPAK or 5x6 PQFN packages, and 20V SPV1520 in D2PAK or 5x6 PQFN, are available now for minimum orders of 1000 units, priced at $2.00 each. Alternative pricing options for higher quantities are available on request.

Click here for the high-resolution photo

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power technologies and multimedia convergence applications. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.
In 2011, the Company’s net revenues were $9.73 billion. Further information on ST can be found at www.st.com.

1 European Environment Agency figures: Final electricity consumption by sector (ENER 018) – Assessment, published Apr 2012 and available at http://www.eea.europa.eu/data-and-maps/indicators/final-electricity-consumption-by-sector/final-electricity-consumption-by-sector-3