ST Life.augmented

新闻稿

Advanced Energy-Harvesting IC from STMicroelectronics Broadens Benefits of Battery-Free Technology

Highly efficient, ultra low-power energy harvester and battery charger enhances flexibility, simplifies design, extends application reach
Geneva /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, is opening new avenues for energy-harvesting applications with its latest IC integrating all the functions needed to power electronic circuits and recharge batteries using either a solar cell or Thermo-Electric Generator (TEG).
 

Harvesting ambient light or thermal energy to power small electronic devices such as wireless sensors, smart-building and industrial equipment controls, wellness and wearable monitors, protects the environment by reducing CO2 emissions, while eliminating batteries and power cabling, so finally enabling the Internet of Things (IoT) ecosystem. In the future, hundreds of millions of these devices operating from tiny quantities of harvested ambient energy are expected to be deployed in environments such as office buildings, houses, hotels, industrial sites, transportation infrastructure and electric vehicles.

ST’s SPV1050 is ideal for applications with power requirements from a few microwatts to several milliwatts, and is equally suitable for both indoor and outdoor consumer and industrial applications using either solar or thermal energy.

The ultra low-power energy-harvesting IC also provides more functions than competing devices, which aids miniaturization and saves bill-of-materials costs. Both 1.8V and 3.3V regulators are available to power a companion microcontroller or wireless transmitter directly without requiring additional components. Maximum Power-Point Tracking (MPPT) continuously optimizes energy harvesting, or can be disabled. The battery-charging circuitry supports a wide variety of battery types including lithium-ion and lithium-polymer, lithium thin-film solid state, NiMH and NiCd, as well as supercapacitors.

“Energy harvesting delivers environmental benefits and helps reduce equipment ownership costs, and is used increasingly as energy-conversion efficiency rises and typical system power demands fall,” said Matteo Lo Presti, Group Vice President and General Manager, Industrial and Power Conversion Division, STMicroelectronics. “The tremendous operational and energy-harvesting efficiency of the SPV1050, combined with its unparalleled flexibility and feature integration, enables engineers to realize many new opportunities in industrial and consumer markets.”

Inside the SPV1050, a buck-boost converter allows the device to connect to either TEG or indoor/outdoor solar-energy harvesting modules by providing a wide input-voltage range from 180mV to 8V. Average operating efficiency of 90% allows fast battery charging even at low input power levels, while minimum MPPT accuracy of 90% maximizes energy extraction from solar or TEG sources. In addition, the integrated battery charging controller uses highly accurate under-voltage and end-of-charge thresholds, and provides safe control logic to prevent excessive discharging for longer battery life.


The SPV1050 is sampling now and scheduled for production in Q1 2014. It is available in a 20-lead QFN 3x3x1mm package or in 20-bump WLCSP tested and unsawn wafers. Budgetary pricing is $1.15 for orders of up to 1,000 pieces.

Click here for the high-resolution photo


About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power and automotive products and embedded processing solutions. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.

In 2012, the Company’s net revenues were $8.49 billion. Further information on ST can be found at www.st.com.

Feedback Form
Customer Feedback