ST Life.augmented

Lead-free Solutions

The Ecopack working group has selected 3 technologies (NiPdAu, Pure Sn and SnAgCu Ball) to match the different technical and quality requirements and cover the full spectrum of packages. The Conversion program applies both to internal and subcontractor production lines.

NiPdAu:This technology is well known on the market and several billions of parts have been already shipped by the semiconductor industry. ST already qualified it in 1996. It is also known as PPF (Pre-Plated Frame). The NiPdAu technology is the preferred choice of ST each time it is technically feasible. Beside the change of lead frame, a change in materials (glue and molding compound) may occur to meet the higher soldering temperature constraints required for lead-free soldering.



The NiPdAu technology will be used for most of Signal SMD packages: SO, TSSOP, L/TQFP with few exceptions such as SMD packages with soft solder die attach, PLCC (due to the particular shape of the leads), TSOP (alloy 42), few L/TQFP, Exposed pad packages.



Pure Tin (Sn):This technology is also a very common Lead-free solution used by semiconductor manufacturers. There are 2 sub-processes: Dipping and Post-plating (Matt Sn). This technology is selected by ST for all other leadframe-based packages which are not eligible for NiPdAu.



The Pure Tin technology will be used for: Power SMD packages, Insertion packages, PLCC, TSOP.



SnAgCu ball:This ternary alloy is an improved composition, derived from SnAgCu alloy. SAC + is the material chosen for the balls of all “Ball Grid Arrays” (BGA) and balls and bumps of Flip-Chips (currently using PbSn). Its melting point is 217°C and its composition close to the one of the most common solder pastes. It is the preferred alloy selected by the large majority of semiconductors companies and subcontractors.

 



Packages
Pb-Based
Lead-Free
Lead frame

based
SnPb

Dipping
Tin (Sn)

Dipping
SnPb

Post plating
Matte Tin

(Sn)

Post-plating
NiPdAu

Pre-plating
SnBi

 

 

 

Packages
Pb-Based
Lead-Free
Ball Grid

Array
 
SAC+
Bumps for

FlipChip
 
SnAg

Gold bumps
Die bonding in power packages
 
Exempted
Glass sealing in frit seal packages
 

 

 
Alloys and packages
 

 

 
Alloys used in
Packages
ST Production lines
Subcontractors lines
     
Power SMD
Matte Sn post plated coating
X
Signal SMD
NiPdAu pre plated coating
Sn, SnBi post plated coating
Matte Sn post plated coating
Insertion package
Matte Sn post plated coating
Sn, SnAgCu coating by dipping
BGA
SAC+ solder balls
SAC+ solder balls

 

 

(*) SnAgCu metallurgy or its derivatives

 

Feedback Form
Customer Feedback