ST Life.augmented

eSTore

Introducing the eSTore dedicated initially to offer the convenience of buying boards and development kits directly from our site. Supported by our logistics and order fulfillment partner, the eSTore makes possible a quick and simple access to our available inventory of development kits and boards.

  • STEVAL-ISB008V1
    Standalone USB Li-Ion battery charger demonstration board based on the STw4102 and STM32F103C6

    The STEVAL-ISB008V1 demonstration board is based on the STw4102 battery charger device and the STM32F103C6 microcontroller. The board is designed as a complete standalone battery charger, and includes a gas gauge to monitor battery capacity using five LEDs to represent different capacity levels. Two status LEDs indicate battery charging, discharging and some fault conditions.

    By default, the firmware programmed in the demonstration board considers a battery capacity of 1200 mAh. This maximum capacity value is used to identify the percentage of available battery capacity, which is shown using the 5 LEDs.

    The demonstration board firmware allows the user to vary the maximum capacity up to 2100 mAh, in steps of 300 mAH.

    The STM32F103C6 microcontroller is used to control and monitor the STw4102 battery charger device.

    All communication between the STw4102 and the STM32F103C6 is done through an I2C interface.

    The STEVAL- ISB008V1 is equipped with both a USB and a DC adapter connector.

    The board can supply a maximum battery charging current of 400 mA for a USB port, extending to 800 mA for a DC adapter.

    ... See More

    Price:  $60.45

    Availability:  1

    Orderable Qty:  1

    Buy Direct
  • STEVAL-PCC009V1
    Universal USB to serial communication interface demonstration board based on the STM32

    This demonstration board implements an universal USB to serial communication interface (UUSCI) based on STM32.

    This demoboard has a 10 pin interface. In this interface, there is a provision to connect a device which can communicate using I2C, SPI and UART. Thus UUSCI tool allows a user to connect a serial communication based device to a PC. At the same time it allows to control some GPIOs available in that 10 pin interface and set them in input/output modes as per the application requirements.

    In UUSCI demonstration board, the STM32 microcontroller is used as the interface between PC and the end device. Due to intelligence available in the STM32 device, I2C, SPI and UART are multiplexed in same 10 pin interface thus leading to reduced board size and the complexity of usage.

    Power to board is provided from USB Mini B-Type connector.

    DLL files of the PC GUI are provided with this tool. So a user can use these DLL files to make their own customized PC GUI as per their requirements.

    ... See More

    Price:  $37.97

    Availability:  3

    Orderable Qty:  1

    Buy Direct
  • STEVAL-SCM001V1
    RTC dongle demonstration board based on the M41T62 and ST72651AR6

    The STEVAL-SCM001V1 RTC dongle demonstrates all the features of STMicroelectronics' M41T62 serial access RTC (real-time clock), as well as the mass storage capability using the ST7 USB. The demonstration board also demonstrates the RTC operation using a capacitor or the ST7 MCU regulator as a supply.

    ... See More

    Price:  $59.17

    Availability:  2

    Lead Time:  5

    Orderable Qty:  1

    Buy Direct
  • STEVAL-SPBT3ATV3
    USB dongle for the Bluetooth® class 2 SBT2632C2A.AT2 module

    The STEVAL-SPBT3ATV3 demonstration board is a design tool to evaluate the SPBT2632C2A.AT2 module in a quick and simple way.

    The dongle includes the RF antenna and the USB connector.

    The USB connector is used to connect the dongle to a PC, to access the Bluetooth® module, and to supply the dongle.

    The STEVAL-SPBT3ATV3 includes downloaded FW, enabling the user to create a Bluetooth® link with simple AT commands. The AT command list is detailed in the User Manual UM1547.

    The AN4127 application note describes how to get started with the STEVAL-SPBT3ATV3.

    The SPBT2632C2A.AT2-based dongle is a demonstration tool only, to be used strictly for evaluation purposes. It is not a product in itself.

    ... See More

    Price:  $30.62

    Availability:  9

    Orderable Qty:  1

    Buy Direct
  • STEVAL-SPBT4ATV3
    USB dongle for the Bluetooth® class 1 SPBT2632C1A.AT2 module

    The STEVAL-SPBT4ATV3 demonstration board is a design tool to evaluate the SPBT2632C1A.AT2 module in a quick and simple way.

    The dongle includes the RF antenna and the USB connector.

    The USB connector is used to connect the dongle to a PC, to access the Bluetooth® module, and to supply the dongle.

    The STEVAL-SPBT4ATV3 includes downloaded FW, enabling the user to create a Bluetooth® link with simple AT commands. The AT command list is detailed in the user manual UM1547.

    The AN4128 application note describes how to get started with the STEVAL-SPBT4ATV3.

    The SPBT2632C1A.AT2-based dongle is a demonstration tool only, to be used strictly for evaluation purposes. It is not a product in itself.

    ... See More

    Price:  $30.62

    Availability:  16

    Lead Time:  14

    Orderable Qty:  1

    Buy Direct
Feedback Form
Customer Feedback