ST Life.augmented

Product Environmental Compliance

RoHS / ECOPACK

STMicroelectronics is fully committed to Environmental protection within its Sustainable Excellence program. It has been a pioneer in environmental protection since 1992 and kept such issues at the forefront of its management. ST has adopted the most stringent Environment, Health & Safety regulations worldwide and strictly applies these rules to all its sites / organizations. Read more into the following chapters:

Lead-free Quality and Reliability

STMicroelectronics devices are requalified to ensure their resistance to new soldering temperatures requested by PC board mounting with Tin-Silver-Copper alloys : melting temperature of 217°C instead of 183°C for SnPb eutectic alloy. 

Materials Declaration

STMicroelectronics’ banned, exempted and declarable substances list is regularly reviewed to include regulations and customer requirements and to insure that our suppliers are in line with our rules regarding the use of chemicals and hazardous substances.

Lead-free Solutions

The Ecopack working group has selected 3 technologies (NiPdAu, Pure Sn and SnAgCu Ball) to match the different technical and quality requirements and cover the full spectrum of packages. The Conversion program applies both to internal and subcontractor production lines.

 

Publications

FAQ

 

Feedback Form
Customer Feedback