ST Life.augmented

eSTore

Introducing the eSTore dedicated initially to offer the convenience of buying boards and development kits directly from our site. Supported by our logistics and order fulfillment partner, the eSTore makes possible a quick and simple access to our available inventory of development kits and boards.

  • EVALKITST7580-1
    ST7580 Power Line Networking System On Chip Demonstration kit

    Built around the ST7580 power line networking system-on-chip, this demonstration kit embeds all the functions required for a “turnkey” power line communication network: the PLC node based on the ST7580, the AC power supply (based on the ALTAIR4-900 chip) and the STM32 microcontroller, to either control the system as a standalone application or to connect the EVALKITST7580-1 to an external host.

    The typical application environment consists of two or more EVALKITST7580-1s connected to the same mains line, each being controlled by a PC running the ST7580 GUI software.

    ... See More

    Price:  $245.00

    Availability:  12

    Lead Time:  10

    Orderable Qty:  1

    Buy Direct
  • EVALST7538DUAL
    Dual channel power line transceiver board based on ST7538

    The EVALST7538DUAL board integrates the ST7538 power line transceiver along with the power supply section, the signal coupling interface section, the crystal oscillator and device protections. The coupling interface section has been realized for communication on CENELEC A-band used mainly for AMR applications, with the chance of programmable switching between 72 kHz and 86 kHz communication channels. This half-duplex “dual channel” communication feature has been implemented through optimized receiving and transmitting filters on the board.

    EVALST7538DUAL board must be connected to a PC through the EVALCOMMBOARD general purpose board. The dedicated SW running on the PC can be downloaded from “www.st.com/powerline” web page.

    The typical application environment consists of two or more EVALST7538DUAL connected to the same mains line, each connected to its own EVALCOMMBOARD controlled by a PC running the EVALCOMMBOARD GUI software.

    ... See More

    Price:  $154.35

    Availability:  1

    Orderable Qty:  1

    Buy Direct
  • EVALST7540-2

    EVALST7540-2
    ST7540 FSK powerline transceiver evaluation board

    The EVALST7540-2 board integrates the ST7540 power line transceiver along with the power supply section, the signal coupling interface section, the crystal oscillator and device protections. The coupling interface section has been realized for communication around 72 kHz carrier frequency, within the european CENELEC standard A-band specified for automatic meter reading (AMR) applications. This communication feature has been optimized through tuned receiving and transmitting filters on the board. The EVALST7540-2 board must be connected to a PC through the EVALCOMMBOARD general purpose board. The dedicated graphical user interface (GUI) running on the PC can be downloaded from “www.st.com/powerline” web page.

    The typical application environment consists of two or more EVALST7540-2 connected to the same mains line, each connected to its own EVALCOMMBOARD controlled by a PC running the EVALCOMMBOARD GUI software.

    ... See More

    Price:  $154.35

    Availability:  4

    Lead Time:  21

    Orderable Qty:  1

    Buy Direct
  • EVALST7590T-2

    EVALST7590T-2
    STarGRID ST7590T SoC PRIME-certified power line communication development kit

    Based on the ST7590 powerline communication system-on-chip, the EVALST7590T-2 development kit embeds all the functions required for a turnkey powerline communication network: the PLC node is based on the ST7590T device, the AC power supply is based on the ALTAIR4-900 SMPS controller and the STM32F103RG microcontroller, to either control the system as a standalone application or to connect the EVALST7590T-2 to an external host.

    The EVALST7590T-2 embeds ST’s full PRIME-compliant protocol stack and provides a complete reference for PRIME-based applications such as smart meters or concentrators, and is an ideal standalone tool for in-field PRIME network tests.

    The EVALST7590T-2 kit supports DLMS/COSEM libraries and has been jointly developed by ST and Fideltronik to accelerate high-volume

    industrial implementation and customization, as well as to provide ready and customizable solutions for any special, low-volume application.

    ... See More

    Price:  $110.25

    Availability:  6

    Lead Time:  26

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IDS001V2
    SPIRIT1 - Low Data Rate Transceiver - 315 MHz - USB dongle

    The STEVAL-IDS001V2 demonstration board is based on the SPIRIT1, which is a sub-GHz low power, low data-rate transceiver suitable for ISM bands. The board is equipped with an STM32L low power microcontroller to control the SPIRIT1. The board also features a USB connector for PC GUI interaction and firmware update. An optional JTAG connector (not mounted) allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $62.47

    Availability:  2

    Lead Time:  8

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IDS001V3
    SPIRIT1 - Low Data Rate Transceiver - 433 MHz - USB dongle

    The STEVAL-IDS001V4 demonstration board is based on the SPIRIT1, which is a sub-GHz low power, low data-rate transceiver suitable for ISM bands and Wireless M-BUS. The board is equipped with an STM32L low power microcontroller to control the SPIRIT1. The board also features a USB connector for PC GUI interaction and firmware update. An optional JTAG connector (not mounted) allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $62.47

    Availability:  5

    Lead Time:  10

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IDS001V4
    SPIRIT1 - Low Data Rate Transceiver - 868 MHz - USB dongle

    The STEVAL-IDS001V4 demonstration board is based on the SPIRIT1, which is a sub-GHz low power, low data-rate transceiver suitable for ISM bands and Wireless M-BUS. The board is equipped with an STM32L low power microcontroller to control the SPIRIT1. The board also features a USB connector for PC GUI interaction and firmware update. An optional JTAG connector (not mounted) allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $62.47

    Availability:  2

    Lead Time:  8

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IDS001V5
    SPIRIT1 - Low Data Rate Transceiver - 915 MHz - USB dongle

    The STEVAL-IDS001V5 demonstration board is based on the SPIRIT1, which is a sub-GHz low power, low data-rate transceiver suitable for ISM bands. The board is equipped with an STM32L low power microcontroller to control the SPIRIT1. The board also features a USB connector for PC GUI interaction and firmware update. An optional JTAG connector (not mounted) allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $62.47

    Availability:  2

    Lead Time:  8

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IDX001V11
    802.15.4/ZigBeeA? daughterboard

    The STEVAL-IDX001V11 demonstration board is based on an RF module of the SPZB32W series and is designed to be integrated together with the STEVAL-IDX001V1. When coupled with the motherboard, the STEVAL-IDX001V11 receives VCCand other system signals from the motherboard. A jumper allows the connection of the RF module via UART or SPI with the microcontroller integrated in the motherboard. Additional jumpers also allow the handling of reset and booting also from the motherboard. The use of this STEVAL-IDX001V11 demonstration board allows the evaluation of all the application partitioning modes between the host and the SPZB32W modules. A JTAG connector is integrated for debugging and reprogramming of the SPZB32W module. Configurable LEDs and pushbuttons are added in order to facilitate the user interaction at the run time.

    ... See More

    Price:  $56.35

    Availability:  4

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IDZ001V1
    ZigBee®-dual IFs EEPROM adapter for STM3221G-EVAL

    The STEVAL-IDZ001V1 demonstration board is based on SPZB32W and allows the interfacing to the STM3221G-EVAL needed to manage a smartplug network system. Furthermore, the adapter has a dual interface EEPROM (M24LR64-r) on board.

    The ZigBee module SPZB32W communicates with the STM3221G demonstration board by an adapter connected through the SPI and UART communication, while the dual interface EEPROM is connected to the STM3221G-EVAL by the I2C interface.

    ... See More

    Price:  $58.80

    Availability:  2

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IHP005V1
    General purpose power line modem module based on the ST7540 PLM and STM32 microcontroller

    The general purpose power line modem module is based on an ST7540 FSK power line modem transceiver and an STM32 microcontroller. The PLM module board is a fully functional communication module, with 8 programmable I/Os, a real-time clock and a Flash memory area for modem parameters and user data storage.

    The firmware structure is made up of several layers, each dealing with a different feature. The application layer engine is the general interface between the user program and all the parts of the module. It deals with the communication ports, the module peripherals such as SPI, SCI, RTC, I/Os, LEDs and timing management. It is also the interface between the PLM stack and the user program. The PLM stack, itself made up of several layers, implements and manages the power line communication, manages the conflicts, timing and repetitions, the addressing, and so on.

    Some features are managed directly by the application engine, and are transparent to the user, such as the RTC management or the module parameter update, as well as the module programming and configuration, which is done by particular programming or service commands managed and acknowledged directly by the application engine.

    The user layer is fully customizable by using some easy to use APIs available for user application implementation. User data can be easily addressed to the PLM or to the other communication interface by simply changing the destination channel in the user data structure.

    ... See More

    Price:  $99.22

    Availability:  4

    Lead Time:  8

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IKR001V3
    Sub-GHz transceiver development kit based on the SPIRIT1 (433 MHz band)

    The STEVAL-IKR001V3 development kit includes 2 RF daughterboards based on the SPIRIT1 low power, sub-GHz low data rate transceiver suitable for ISM bands and wireless M-BUS, and 2 motherboards based on the STM32L low power microcontroller to control the daughterboards.

    Each motherboard features a USB connector for PC GUI interaction and firmware updates. A JTAG connector allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $447.12

    Availability:  5

    Lead Time:  3

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IKR001V8D
    SPIRIT1- low data rate transceiver - 868 MHz - daughterboard - range extender

    The STEVAL-IKR001V8D demonstration board is based on the SPIRIT1, a sub GHz low power, low data rate transceiver suitable for ISM bands and wireless M-BUS systems.

    The STEVAL-IKR001V8D includes an external power amplifier from SkyWorks®, which allows the application to reach +27 dBm (500 mW) output power.

    ... See More

    Price:  $221.72

    Availability:  1

    Lead Time:  8

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IKR002V1
    SPIRIT1 - Low Data Rate Transceiver - 169 MHz - FULL KIT

    The STEVAL-IKR002V1 development kit includes 2 RF daughterboards based on the SPIRIT1 low power, sub-GHz low data rate transceiver suitable for ISM bands and wireless M-BUS, and 2 motherboards based on the STM32L low power microcontroller to control the daughterboards.

    Each motherboard features a USB connector for PC GUI interaction and firmware updates. A JTAG connector allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $398.12

    Availability:  3

    Lead Time:  3

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IKR002V3
    SPIRIT1 - Low Data Rate Transceiver - 433 MHz - FULL KIT

    The STEVAL-IKR002V3 development kit includes 2 RF daughterboards based on the SPIRIT1 low power, sub-GHz low data rate transceiver suitable for ISM bands and wireless M-BUS, and 2 motherboards based on the STM32L low power microcontroller to control the daughterboards.

    Each motherboard features a USB connector for PC GUI interaction and firmware updates. A JTAG connector allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $367.50

    Availability:  3

    Lead Time:  3

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IKR002V4
    Sub-GHz transceiver development kit based on the SPIRIT1 (868 MHz band)

    The STEVAL-IKR002V4 development kit includes 2 RF daughterboards based on the SPIRIT1 low power, sub-GHz low data rate transceiver suitable for ISM bands and wireless M-BUS, and 2 motherboards based on the STM32L low power microcontroller to control the daughterboards.

    Each motherboard features a USB connector for PC GUI interaction and firmware updates. A JTAG connector allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $367.50

    Availability:  1

    Lead Time:  8

    Orderable Qty:  1

    Buy Direct
  • STEVAL-IKR002V5
    Sub-GHz transceiver development kit based on the SPIRIT1 (915 MHz band)

    The STEVAL-IKR002V5 development kit includes 2 RF daughterboards based on the SPIRIT1 low power, sub-GHz low data rate transceiver suitable for ISM bands and wireless M-BUS, and 2 motherboards based on the STM32L low power microcontroller to control the daughterboards.

    Each motherboard features a USB connector for PC GUI interaction and firmware updates. A JTAG connector allows the development of specific firmware on the microcontroller.

    ... See More

    Price:  $367.50

    Availability:  3

    Lead Time:  3

    Orderable Qty:  1

    Buy Direct
  • STEVAL-PCC009V4
    Universal USB to serial bridge demonstration board for motor control applications

    The STEVAL-PCC009V4 demonstration board implements a universal USB on the serial isolated interface communication. It is useful in all applications which need safe connection from PC to the application boards.

    The STEVAL-PCC009V4 has a 16-pin communication interface which allows connecting a device that uses I2C, SPI or UART protocols. Thus, the board functions as a bridge between a serial communication based device and a PC.

    ... See More

    Price:  $37.97

    Availability:  3

    Lead Time:  5

    Orderable Qty:  1

    Buy Direct
  • STEVAL-PCC015V1
    Full speed USB to RS232 bridge

    The STEVAL-PCC015V1 demonstration board is an easy and compact solution in order to make a bridge between a standard USB port and a standard serial COM port. In modern PCs, USB is the standard communication port for almost all peripherals. However many industrial software applications and old equipment still use the classic COM port (UART). The STEVAL-PCC015V1 demonstration board provides a simple solution to overcome this problem.

    ... See More

    Price:  $42.87

    Availability:  4

    Orderable Qty:  1

    Buy Direct
  • STEVAL-PCC018V1
    UART to USB bridge

    Based on the Silab CP2102 USB bridge, the STEVAL-PCC018V1 is a USB to UART board that allows the integration of a USB connector with a general-purpose board which has a UART interface available.

    ... See More

    Price:  $35.52

    Availability:  3

    Lead Time:  3

    Orderable Qty:  1

    Buy Direct
  • STEVAL-SPBT2ATV2
    USB Dongle for the Bluetooth® class 2 SPBT2532C2.AT module

    The STEVAL-SPBT2ATV2 demonstration board is a design tool to evaluate the SPBT2532C2.AT module in a quick and simple way.

    The dongle includes the RF antenna and the USB connector.

    The USB connector is used to connect the dongle to a PC, to access the Bluetooth module, and to supply the dongle.

    The STEVAL-SPBT2ATV2 is a board which has downloaded FW, enabling the user to create a Bluetooth link with simple AT commands.

    The AT command list is detailed in the SPBT2532C2.AT datasheet.

    How to get started with STEVAL-SPBT2ATV2 is described in the AN3189 application note.

    ... See More

    Price:  $30.62

    Availability:  12

    Orderable Qty:  1

    Buy Direct
  • STEVAL-SPBT2ATV3
    USB dongle for the Bluetooth® class 2 SPBT2532C2.AT2 module

    The STEVAL-SPBT2ATV3 demonstration board is a design tool to evaluate the SPBT2532C2.AT2 module in a quick and simple way.

    The dongle includes the RF antenna and the USB connector.

    The USB connector is used to connect the dongle to a PC, to access the Bluetooth® module, and to supply the dongle.

    The STEVAL-SPBT2ATV3 includes downloaded FW, enabling the user to create a Bluetooth® link with simple AT commands.

    The AT command list is detailed in the user manual UM1547.

    The AN3189 application note describes how to get started with the STEVAL-SPBT2ATV3.

    The SPBT2532C2.AT2-based dongle is a demonstration tool only, to be used strictly for evaluation purposes. It is not a product in itself.

    ... See More

    Price:  $30.62

    Availability:  10

    Orderable Qty:  1

    Buy Direct
Feedback Form
Customer Feedback