ST Life.augmented


Tailored Gyroscopes from STMicroelectronics Target Shake-Free Images on Mobiles and Cameras

Geneva /

STMicroelectronics (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, the world’s top MEMS manufacturer, and the leading supplier of MEMS sensors for consumer and portable applications1, has introduced a new family of gyroscopes specifically optimized for optical image stabilization in smartphones and digital still cameras.


Optical Image Stabilization has become an essential feature in today’s smartphones and digital still cameras. By moving the lens in real time to compensate for physical movement of the camera, it can significantly improve the sharpness of the image, especially when taking photographs in low light, when hand jitter during the longer exposure time would blur images.  

In addition, to assure maximum reliability, the new 2-axis (L2G3IS) and 3-axis (L3G3IS) gyroscopes operate with a resonant frequency of the sensing mass at around 20kHz. As a result of this high resonant frequency in combination with the mechanical structure, the devices are immune to the damage that could be caused by ultrasonic cleaning equipment (typically operating at around 30kHz) that many customers use to clean devices before equipment assembly.

“In addition to revolutionizing user interfaces with intuitive gesture recognition, MEMS gyroscopes have brought enormous benefits to hand-held digital photography through optical image stabilization. With the LxG3IS family, ST’s proven MEMS manufacturing technology and supply-chain advantage are applied to gyroscopes that are uniquely tailored for image stabilization and offer increased damage protection,” said Fabio Pasolini, General Manager, Motion MEMS Division, STMicroelectronics.

Other key technical features of the new devices include ±65 dps / ±130 dps full-scale range, SPI digital interface, embedded temperature sensor, and integrated low- and high-pass filters with selectable bandwidth. The devices operate with supply voltage from 2.4V to 3.6V and are housed in an LGA-16 3x3.5x1 mm package.

According to information and analytics firm IHS, ST’s total MEMS and sensor sales grew more than 19% in 2012, reaching a total of approximately $800 million. In the largest of these markets, motion sensors in mobile handsets and tablets, ST’s MEMS sales accounted for 48% of the market, well more than twice as large as that of its closest competitor.

The one-stop MEMS supplier of choice, ST offers a comprehensive portfolio of micro-machined accelerometers, gyroscopes, pressure sensors, magnetic sensors, and microphones, and has the capability to integrate these in multi-sensor combos with on-board signal processing, control functions, sensor-fusion algorithms, and wireless connectivity. Not only the clear market leader, ST is also at the forefront of MEMS technology development with more than 800 MEMS-related patent families.  ST leads the way towards intelligent and independent sensing devices that will open new horizons in consumer electronics, healthcare, environmental sciences, and many other domains.

Samples of ST’s new 2-axis (L2G3IS) and 3-axis (L3G3IS) gyroscopes are available now and budgetary unit pricing is $2.37 (L2G3IS) and $3.38 (L3G3IS) for orders over 1,000 pieces.

For further information please go to

Click here for the high-resolution photo

About STMicroelectronics
ST is a global leader in the semiconductor market serving customers across the spectrum of sense and power and automotive products and embedded processing solutions. From energy management and savings to trust and data security, from healthcare and wellness to smart consumer devices, in the home, car and office, at work and at play, ST is found everywhere microelectronics make a positive and innovative contribution to people's life. By getting more from technology to get more from life, ST stands for life.augmented.

In 2012, the Company’s net revenues were $8.49 billion. Further information on ST can be found at

1IHS: MEMS H2 2012 Special Report
Feedback Form
Customer Feedback