ARM MCU Workshop 2016
Tokyo, JAPAN
Tokyo Convention Hall
June 17, 2016
Visit us at ST booth
Website: Click here
Embedded Technology in the IoT era
ARM MCU Workshop 2016 ~ Sensor & Wireless
ARM MCU Workshop 2016 is the 1 day event specializing for ARM MCU with several technical seminar sessions. This year, the workshop is focusing on the sensor technology and wireless? Visitors can find the embedded technologies in the IoT era, based on the ARM MCU with sensor technologies & wireless connectivity.
At the event, ST will showcase the demonstration of STM32 Open Development Environment which is an open, flexible, easy and affordable way to develop innovative devices and applications based on the STM32 32-bit microcontroller family combined with other state-of-the-art components connected via expansion boards, such as motion sensor and wireless connectivity.
![]() | 32bit microcontroller STM32 | |
![]() | STM32 ODE (Nucleo + X-Nucleo) | |
![]() | MEMS microphone MP34DT01-M | |
![]() | BLE processor BlueNRG | |
![]() | 6-axis motion sensor LSM6DSL | |
Vendor session seminar by ST | ||
![]() | Date & Time : Jun 17th (Fri), 12:50 - 13:20 | |
![]() | Title : Super Easy! STM32 Open Development Environment & mbed OS sensor node development | |
![]() | Registration : Click here |