BlueNRG-LP & LE Power Control (LEPC) for battery-powered IoT applications
![]() | Learn how to reduce power consumption and interference while improving the communication environment in battery-powered IoT applicationsWednesday, December 8th, 2021 | 2:00 pm Eastern Time |
Today's Bluetooth-enabled IoT applications are becoming increasingly more demanding, not only in terms of range capabilities and the amount of data that can be advertised, but also with regard to power consumption. This can be particularly challenging in battery-powered applications, where designers are faced with finding ways to lower the power budget to extend battery life without sacrificing communication performance.
During this 1-hour webinar, we'll show you how to address these challenges using the BlueNRG-LP, a Bluetooth Low Energy 5.2 certified system-on-chip (SoC) that combines ultra-low power consumption with best-in-class radio performance. The newest member of our BlueNRG family of devices, the BlueNRG-LP enables even further power reduction through support for the LE Power Control feature, significantly extending the battery life while also maintaining excellent RF performance.
You will learn:
- The key features of the BlueNRG-LP SoC, with emphasis on LE Power Control
- About our ecosystem of design tools, SDK, and working examples with LEPC
- How to use the BlueNRG Power Consumption Estimation Tool
- About the BlueNRG Sensor App
There will be a live Q&A session at the end of the webinar where ST’s experienced engineers will be available to answer your questions.
Registration information
To participate in this free online event, simply register on my.st.com.
Speakers
![]() | Salvo Bonina Salvo is an Application Staff Engineer for STMicroelectronics’ RF Applications team in the United States. Salvo has been with ST since 2002, where he started as an IT System & Service Engineer/Administrator. He earned both his bachelor’s and a master’s degrees in Computer Science from the Università di Catania in Italy. |
![]() | Julio Sanchez Julio is a Product Marketing Engineer for STMicroelectronics’ RF business unit in the Americas, a position he has held since 2017. Julio began his career in 2005, working for several companies as an FAE before joining ST Mexico in 2015 as a Sr. Key Account Manager. Based in Irvine, CA, Julio holds a degree in Electronics and Communications and a Master’s in Embedded Systems. |
Not sure if you can attend the live session? No problem! Register now and we'll be sure to email you the recorded webinar.