Learn the latest SiC technology and application case studies

Discover the Silicon Carbide MOSFET & Diode products & applications Webinar

 

Thursday, April 22nd 2021 | 11:30 am IST (UTC+05:30)

 

Register now

 

 

Silicon carbide (SiC) - The latest breakthrough in high-voltage switching and rectification.

ST’s portfolio of silicon carbide devices incluses STPOWER SiC MOSFETs ranging from 650 to 1700 V with the industry’s highest junction temperature rating of 200 °C for more efficient and simplified designs, and STPOWER SiC diodes ranging from 600 to 1200 V which feature negligible switching losses and 15% lower forward voltage (VF) than standard silicon diodes.

ST has over 20 years experiences in SiC and is the leader in this market through dedicated product lines. ST SiC technology innovation (Gen 2 and next Gen 3) plus the complete industrilzation of new power packages has led to a strong product range for many power systems. In this webinar, our engineering experts will explain the latest SiC technology with application case studies. Also our experts will be happy to discuss further with you in the live Q&A session.

Agenda: 

  • Benefits of using SiC
  • SiC Market
  • Application case study
  • SiC technology overview
  • ST SiC product profile

Product details

 

Register now

 

Speakers

Dondon Ifurung

Dondon holds a Bachelor of Science in Electronics & Communications Engineering from De La Salle University of Manila, Philippines. He joined ST in 2000 with background in Switch Mode Power Supply (SMPS) design. In 2003, he was expatriated to ST Catania, Italy as Worldwide Product Marketing Manager dedicated for SMPS customers. He became the Philippines Country Manager in 2007. In 2012, he moved to Sydney as Product Marketing Manager responsible for PDSA products in Australia & New Zealand region.

Satish Pawar

(Senior Manager Technical Marketing - Power Discrete & Sub Analog)

Experience in Semiconductor Industries more than 25 years, He is working with ST from last 13th year as Technical Marketer, His main filed of interest as dedicated market development in field of Motor Control & Home Appliances taking care of IGBT, IPM, Mosfet and Power Module. Satish helps motor control engineers find best solutions for their applications.

Upcoming Events

STM32 Summit 2021 08 Mar - 29 Apr, 2021
SENSOR+TEST 2021 16 Apr - 06 May, 2021
ST PCIM 2021 16 Apr - 07 May, 2021

Latest from ST