ST Accelerometers: How to pick the perfect fit for any application
![]() | Find the right sensor for your application with one of the industry's most extensive portfolios of MEMS accelerometersThursday, December 2nd, 2021 | 2:00 pm Eastern Time |
The use cases for accelerometers are rapidly growing every year, and the products that use them must be more power efficient, higher performing, and lower cost while also meeting the reliability and longevity standards that customers expect. With the vast range of accelerometers available on the market today, it is more important than ever that designers understand how to choose the most appropriate sensor for their application.
During this one-hour webinar, we will take a detailed look at the key features, performance parameters, and use-case examples needed to help designers make the most informed decision when selecting an accelerometer.
By the end of the session, you will have the knowledge required to select the ideal accelerometer for your application.
You will learn:
- The fundamentals of MEMS accelerometer technology
- Which parameters are most relevant for accelerometer selection
- About ST's complete range of accelerometers serving all major market segments
- The demonstrated system-level power consumption of an accelerometer
There will be a live Q&A session at the end of the webinar where ST’s experienced engineers will be available to answer your questions.
Registration information
To participate in this free online event, simply register on my.st.com.
Speakers
![]() | Alexandra Gogonea Alexandra is a Product Marketing Engineer for Sensors at STMicroelectronics, a position she has held since 2018. Alexandra started her career in 2009 as a consultant for ST in Italy, then worked as a product marketing engineer focusing on product and business management. In 2013, she transferred to the ST Americas region where she has managed several product families. Alexandra Gogonea holds a master’s degree in biomedical engineering from the University of Pavia (Italy). |
![]() | Kirby Atwater Kirby is a Product Marketing Staff Engineer with STMicroelectronics, supporting ST's MEMS sensors portfolio and low-power RF products in North America. Currently located in the Schaumburg, IL office, he joined ST in 2005 and has supported a wide variety of products to ST customers in the USA and Canada. Prior to joining ST, he was a Field Applications Engineer with ST’s distribution partners, and a project design engineer. Kirby graduated from Purdue University with a BSEE. |
Not sure if you can attend the live session? No problem! Register now and we'll be sure to email you the recorded webinar.
About ST's MEMS accelerometers
Accelerometers measure linear acceleration. ST’s MEMS accelerometers embed several useful features for motion and acceleration detection including free-fall, wakeup, single/double-tap recognition, activity/inactivity detection and 6D/4D orientation, and can also be used to measure inclination or vibration. ST's state-of-the-art 3-axis MEMS accelerometers include analog and digital sensors featuring up to ±400 g acceleration full scale and from 1.71 to 3.6 V supply voltage.